EmberAfGbzMessageData Struct Reference
#include <
af-types.h
>
Data Fields | |
bool | encryption |
uint8_t * | plainPayload |
uint16_t | plainPayloadLength |
uint8_t * | encryptedPayload |
uint16_t | encryptedPayloadLength |
Field Documentation
uint8_t* EmberAfGbzMessageData::encryptedPayload |
uint16_t EmberAfGbzMessageData::encryptedPayloadLength |
bool EmberAfGbzMessageData::encryption |
uint8_t* EmberAfGbzMessageData::plainPayload |
uint16_t EmberAfGbzMessageData::plainPayloadLength |
The documentation for this struct was generated from the following file:
af-types.h