EmberAfGpfMessage Struct Reference
#include <
af-types.h
>
Data Fields | |
uint8_t * | gbzCommands |
uint16_t | gbzCommandsLength |
uint8_t * | gbzCommandsResponse |
uint16_t | gbzCommandsResponseLength |
uint16_t | messageCode |
Field Documentation
uint8_t* EmberAfGpfMessage::gbzCommands |
uint16_t EmberAfGpfMessage::gbzCommandsLength |
uint8_t* EmberAfGpfMessage::gbzCommandsResponse |
uint16_t EmberAfGpfMessage::gbzCommandsResponseLength |
uint16_t EmberAfGpfMessage::messageCode |
The documentation for this struct was generated from the following file:
af-types.h