#include <af-types.h
>
bool EmberAfPluginPriceClientPrice::active |
uint32_t EmberAfPluginPriceClientPrice::alternateCostDelivered |
uint8_t EmberAfPluginPriceClientPrice::alternateCostTrailingDigit |
uint8_t EmberAfPluginPriceClientPrice::alternateCostUnit |
uint8_t EmberAfPluginPriceClientPrice::clientEndpoint |
uint16_t EmberAfPluginPriceClientPrice::currency |
uint32_t EmberAfPluginPriceClientPrice::currentTime |
uint16_t EmberAfPluginPriceClientPrice::durationInMinutes |
uint32_t EmberAfPluginPriceClientPrice::endTime |
uint32_t EmberAfPluginPriceClientPrice::generationPrice |
uint8_t EmberAfPluginPriceClientPrice::generationPriceRatio |
uint32_t EmberAfPluginPriceClientPrice::issuerEventId |
uint8_t EmberAfPluginPriceClientPrice::numberOfBlockThresholds |
uint8_t EmberAfPluginPriceClientPrice::numberOfPriceTiersAndRegisterTier |
uint32_t EmberAfPluginPriceClientPrice::price |
uint8_t EmberAfPluginPriceClientPrice::priceControl |
uint8_t EmberAfPluginPriceClientPrice::priceRatio |
uint8_t EmberAfPluginPriceClientPrice::priceTrailingDigitAndPriceTier |
uint32_t EmberAfPluginPriceClientPrice::providerId |
uint32_t EmberAfPluginPriceClientPrice::startTime |
uint8_t EmberAfPluginPriceClientPrice::unitOfMeasure |
bool EmberAfPluginPriceClientPrice::valid |
The documentation for this struct was generated from the following file: