EmberAfSecurityProfileData Struct Reference
#include <
af-types.h
>
Field Documentation
EmberAfAppLinkKeyRequestPolicy EmberAfSecurityProfileData::appLinkKeyRequestPolicy |
uint16_t EmberAfSecurityProfileData::nodeBitmask |
EmberExtendedSecurityBitmask EmberAfSecurityProfileData::nodeExtendedBitmask |
EmberKeyData EmberAfSecurityProfileData::preconfiguredKey |
EmberAfSecurityProfile EmberAfSecurityProfileData::securityProfile |
uint16_t EmberAfSecurityProfileData::tcBitmask |
EmberExtendedSecurityBitmask EmberAfSecurityProfileData::tcExtendedBitmask |
EmberAfTcLinkKeyRequestPolicy EmberAfSecurityProfileData::tcLinkKeyRequestPolicy |
The documentation for this struct was generated from the following file:
af-types.h