EmberAfTagData Struct Reference
This structure contains information about a tag that resides within an Over-the-air bootload file.
#include <
af-types.h
>
Data Fields | |
uint16_t | id |
uint32_t | length |
This structure contains information about a tag that resides within an Over-the-air bootload file.
Field Documentation
uint16_t EmberAfTagData::id |
uint32_t EmberAfTagData::length |
The documentation for this struct was generated from the following file:
af-types.h