EmberApsFrame Struct Reference
An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.
#include <
ember-types.h
>
Data Fields | |
uint16_t | profileId |
uint16_t | clusterId |
uint8_t | sourceEndpoint |
uint8_t | destinationEndpoint |
EmberApsOption | options |
uint16_t | groupId |
uint8_t | sequence |
uint8_t | radius |
An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.
Field Documentation
uint16_t EmberApsFrame::clusterId |
The cluster ID for this message.
Referenced by cliBufferPrint()
, emAfApsFrameClusterIdSetup()
, emAfCliBsendCommand()
, interpanCommand()
, and interpanLongCommand()
.
uint8_t EmberApsFrame::destinationEndpoint |
The destination endpoint.
Referenced by emAfApsFrameEndpointSetup()
.
uint16_t EmberApsFrame::groupId |
The group ID for this message, if it is multicast mode.
EmberApsOption EmberApsFrame::options |
A bitmask of options from the enumeration above.
Referenced by emAfApsFrameClusterIdSetup()
, emAfCliBsendCommand()
, emAfCliSendCommand()
, zclDrlcLoadControlEventCommand()
, and zclGroupsGetCommand()
.
uint16_t EmberApsFrame::profileId |
The application profile ID that describes the format of the message.
uint8_t EmberApsFrame::radius |
uint8_t EmberApsFrame::sequence |
The sequence number.
uint8_t EmberApsFrame::sourceEndpoint |
The source endpoint.
Referenced by emAfApsFrameEndpointSetup()
, and emAfCliBsendCommand()
.
The documentation for this struct was generated from the following file:
ember-types.h