EmberTransientKeyData Struct Reference
This data structure contains the transient key data that is used during Zigbee 3.0 joining.
#include <
ember-types.h
>
Data Fields | |
EmberEUI64 | eui64 |
EmberKeyData | keyData |
uint32_t | incomingFrameCounter |
EmberKeyStructBitmask | bitmask |
uint16_t | remainingTimeSeconds |
This data structure contains the transient key data that is used during Zigbee 3.0 joining.
Field Documentation
EmberKeyStructBitmask EmberTransientKeyData::bitmask |
Referenced by printTransientKeyTable()
.
EmberEUI64 EmberTransientKeyData::eui64 |
Referenced by printTransientKeyTable()
.
uint32_t EmberTransientKeyData::incomingFrameCounter |
Referenced by printTransientKeyTable()
.
EmberKeyData EmberTransientKeyData::keyData |
Referenced by printTransientKeyTable()
.
uint16_t EmberTransientKeyData::remainingTimeSeconds |
Referenced by printTransientKeyTable()
.
The documentation for this struct was generated from the following file:
ember-types.h