EmberAfDefaultAttributeValue Union Reference
Type for default values.
#include <
af-types.h
>
Data Fields | |
uint8_t * | ptrToDefaultValue |
uint16_t | defaultValue |
Type for default values.
Default value is either a value itself, if it is 2 bytes or less, or a pointer to the value itself, if attribute type is longer than 2 bytes.
Field Documentation
uint16_t EmberAfDefaultAttributeValue::defaultValue |
Actual default value if the attribute size is 2 bytes or less.
uint8_t* EmberAfDefaultAttributeValue::ptrToDefaultValue |
Points to data if size is more than 2 bytes. If size is more than 2 bytes, and this value is NULL, then the default value is all zeroes.
The documentation for this union was generated from the following file:
af-types.h