Silicon Labs
zigbee/6.7/functions-i
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
      Results 1-5 of 5 for zigbee/6.7/functions-i in 0.03 seconds
      BGAPI | BGAPI headers | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 5.0 //API Reference //BGAPI Headers You are viewing documentation for version: 5.0 BGAPI# ... BGAPI commands cannot be called from interrupt context.
      Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
      https://docs.silabs.com/.../sl-bt-adverti...
      // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
      sl_bt_evt_scanner_scan_reportScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../a00...
      // Bluetooth LE//Version 5.0 //API Reference //Commands & Events ... Bits 3.4 : Reserved for future Bits 5.6 : data completeness* 00: Complete ... Value 0 indicates no periodic advertising.
      Adaptive Frequency Hopping | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../adaptive-frequency-hopp...
      Bluetooth functions in the 2.4 GHz frequency range. ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... Bluetooth Low Energy has two channel selection algorithms.
      TX Power Limitations for Regulatory Compliance (ETSI, FCC) | System & Performance | Bluetooth LE | v3.1 | Silicon Labs
      https://docs.silabs.com/.../tx-power-limitations-for-regulatory-compliance-etsi-...
      // Bluetooth LE//Version 3.1 //General ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled (or AFH is enabled but ...
        Results 1-5 of 5 for zigbee/6.7/functions-i