Bluetooth cannot be used on this hardware. ... SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT ((sl_status_t)0x1008) ... Connection was terminated because the Message Integrity Check (MIC) failed on a ...
connection-oriented channel by sending disconnection request. ... Errors from Attribute Protocol Bluetooth Mesh errors Bluetooth Mesh foundation errors Filesystem errors
The Bluetooth SDK comes with a number of example application that you can then modify to create your ... can register at https://siliconlabs.force.com/apex/SL_CommunitiesSelfReg?form=short.
Training ... Register // Bluetooth LE//Version 9.0.0 //Developer's Guide ... 9.0.0 Bluetooth LE Developers Guide# The Developer's Guide content is organized in the following groups: