Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
... while EFR32xG22 and later platforms require 4-byte alignment; applications can use ... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks).
Example Example usage. Alphabetical List of Commands ... <index> - the index obtained from the scan command output ... os pins can only use the strong drive strength. ... > gges Example > gges
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for zigbee/6.7/structSourceRouteTableEntry