CLI commands for sending various messages.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_ZCL_CLI_H
#define SILABS_ZCL_CLI_H
#if !defined(EMBER_AF_GENERATE_CLI)
void emAfCliSendCommand(void);
void emAfCliSendUsingMulticastBindingCommand(void);
void emAfCliBsendCommand(void);
void emAfCliReadCommand(void);
void emAfCliWriteCommand(void);
void emAfCliTimesyncCommand(void);
void emAfCliRawCommand(void);
void emAfCliAddReportEntryCommand(void);
#endif
void zclSimpleCommand(uint8_t frameControl,
uint16_t clusterId,
uint8_t commandId);
extern EmberCommandEntry keysCommands[];
extern EmberCommandEntry interpanCommands[];
extern EmberCommandEntry printCommands[];
extern EmberCommandEntry zclCommands[];
extern EmberCommandEntry certificationCommands[];
#define zclSimpleClientCommand(clusterId, commandId) \
zclSimpleCommand(ZCL_CLUSTER_SPECIFIC_COMMAND | ZCL_FRAME_CONTROL_CLIENT_TO_SERVER, \
(clusterId), \
(commandId))
#define zclSimpleServerCommand(clusterId, commandId) \
zclSimpleCommand(ZCL_CLUSTER_SPECIFIC_COMMAND | ZCL_FRAME_CONTROL_SERVER_TO_CLIENT, \
(clusterId), \
(commandId))
#endif // SILABS_ZCL_CLI_H
Macros#
#define
zclSimpleClientCommand (clusterId, commandId)
#define
zclSimpleServerCommand (clusterId, commandId)
Functions#
void
emAfCliSendCommand(void)
void
void
emAfCliBsendCommand(void)
void
emAfCliReadCommand(void)
void
emAfCliWriteCommand(void)
void
emAfCliTimesyncCommand(void)
void
emAfCliRawCommand(void)
void
void
zclSimpleCommand(uint8_t frameControl, uint16_t clusterId, uint8_t commandId)
Macro Definition Documentation#
zclSimpleClientCommand#
#define zclSimpleClientCommandValue:
zclSimpleCommand(ZCL_CLUSTER_SPECIFIC_COMMAND | ZCL_FRAME_CONTROL_CLIENT_TO_SERVER, \
(clusterId), \
(commandId))
zclSimpleServerCommand#
#define zclSimpleServerCommandValue:
zclSimpleCommand(ZCL_CLUSTER_SPECIFIC_COMMAND | ZCL_FRAME_CONTROL_SERVER_TO_CLIENT, \
(clusterId), \
(commandId))
Variable Documentation#
Function Documentation#
emAfCliSendCommand#
void emAfCliSendCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
References appZclBuffer , appZclBufferLen , disableDefaultResponse , emAfApsFrameEndpointSetup , EMBER_AF_NULL_MANUFACTURER_CODE , EMBER_APS_OPTION_ENCRYPTION , EMBER_BROADCAST_ADDRESS , EMBER_OUTGOING_DIRECT , EMBER_SUCCESS , emberAfDebugPrintln , emberAfGetNodeId , emberAfPreCliSendCallback , emberAfSendBroadcast , emberAfSendMulticast , emberAfSendUnicast , globalApsFrame , mfgSpecificId , EmberApsFrame::options , and zclCmdIsBuilt
emAfCliSendUsingMulticastBindingCommand#
void emAfCliSendUsingMulticastBindingCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emAfCliBsendCommand#
void emAfCliBsendCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emAfCliReadCommand#
void emAfCliReadCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emAfCliWriteCommand#
void emAfCliWriteCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emAfCliTimesyncCommand#
void emAfCliTimesyncCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
References cliBufferPrint , emAfCliSendCommand , emAfSyncingTime , ZCL_FRAME_CONTROL_CLIENT_TO_SERVER , ZCL_GLOBAL_COMMAND , zclBufferAddWord , and zclBufferSetup
emAfCliRawCommand#
void emAfCliRawCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
References APP_ZCL_BUFFER_SIZE_CLI , appZclBuffer , emAfApsFrameClusterIdSetup , and ZCL_MANUFACTURER_SPECIFIC_MASK
emAfCliAddReportEntryCommand#
void emAfCliAddReportEntryCommand (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
zclSimpleCommand#
void zclSimpleCommand (uint8_t frameControl, uint16_t clusterId, uint8_t commandId)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | frameControl | |
| uint16_t | N/A | clusterId | |
| uint8_t | N/A | commandId |