See Bootloader for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_BOOTLOAD_H
#define SILABS_BOOTLOAD_H
EmberStatus emberSendBootloadMessage(bool broadcast,
EmberEUI64 destEui64,
EmberMessageBuffer message);
void emberIncomingBootloadMessageHandler(EmberEUI64 longId,
EmberMessageBuffer message);
void emberBootloadTransmitCompleteHandler(EmberMessageBuffer message,
EmberStatus status);
#endif // SILABS_BOOTLOAD_H
Functions#
Transmits the given bootload message to a neighboring node using a specific 802.15.4 header that allows the EmberZNet stack and the Ember bootloader to recognize the message; but will not interfere with other Zigbee stacks.
A callback invoked by the EmberZNet stack when a bootload message is received. If the application includes emberIncomingBootloadMessageHandler(), it must define EMBER_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
A callback invoked by the EmberZNet stack when the MAC has finished transmitting a bootload message. If the application includes this callback, it must define EMBER_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
Function Documentation#
emberSendBootloadMessage#
EmberStatus emberSendBootloadMessage (bool broadcast, EmberEUI64 destEui64, EmberMessageBuffer message)
Transmits the given bootload message to a neighboring node using a specific 802.15.4 header that allows the EmberZNet stack and the Ember bootloader to recognize the message; but will not interfere with other Zigbee stacks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | broadcast | If true, the destination address and PAN ID are both set to the broadcast address. |
| EmberEUI64 | N/A | destEui64 | The EUI64 of the target node. Ignored if the broadcast field is set to true. |
| EmberMessageBuffer | N/A | message | The bootloader message to send. |
Returns
EMBER_SUCCESS if the message was successfully submitted to the transmit queue, and EMBER_ERR_FATAL otherwise.
emberIncomingBootloadMessageHandler#
void emberIncomingBootloadMessageHandler (EmberEUI64 longId, EmberMessageBuffer message)
A callback invoked by the EmberZNet stack when a bootload message is received. If the application includes emberIncomingBootloadMessageHandler(), it must define EMBER_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | longId | The EUI64 of the sending node. |
| EmberMessageBuffer | N/A | message | The bootload message that was sent. |
emberBootloadTransmitCompleteHandler#
void emberBootloadTransmitCompleteHandler (EmberMessageBuffer message, EmberStatus status)
A callback invoked by the EmberZNet stack when the MAC has finished transmitting a bootload message. If the application includes this callback, it must define EMBER_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMessageBuffer | N/A | message | The message that was sent. |
| EmberStatus | N/A | status | EMBER_SUCCESS if the transmission was successful, or EMBER_DELIVERY_FAILED if not. |