Bootloader GPIO definitions. See GPIO for detailed documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef __BOOTLOADER_GPIO_H__
#define __BOOTLOADER_GPIO_H__
//
#define BL_STATE_UP() do { bootloadStateIndicator(BL_ST_UP); } while (0)
#define BL_STATE_DOWN() do { bootloadStateIndicator(BL_ST_DOWN); } while (0)
#define BL_STATE_POLLING_LOOP() do { bootloadStateIndicator(BL_ST_POLLING_LOOP); } while (0)
#define BL_STATE_DOWNLOAD_LOOP() do { bootloadStateIndicator(BL_ST_DOWNLOAD_LOOP); } while (0)
#define BL_STATE_DOWNLOAD_SUCCESS() do { bootloadStateIndicator(BL_ST_DOWNLOAD_SUCCESS); } while (0)
#define BL_STATE_DOWNLOAD_FAILURE() do { bootloadStateIndicator(BL_ST_DOWNLOAD_FAILURE); } while (0)
enum blState_e {
BL_ST_UP,
BL_ST_DOWN,
BL_ST_POLLING_LOOP,
BL_ST_DOWNLOAD_LOOP,
BL_ST_DOWNLOAD_FAILURE,
BL_ST_DOWNLOAD_SUCCESS
};
void bootloadGpioInit(void);
void bootloadStateIndicator(enum blState_e state);
bool bootloadForceActivation(void);
#endif // __BOOTLOADER_GPIO_H__
State Indicator Macros#
The bootloader indicates which state it is in by calling these // macros. Map them to the ::halBootloadStateIndicator function // (in bootloder-gpio.c) if you want to display that bootloader state. // Used to blink the LED's or otherwise signal bootloader activity.
Finished init sequence, ready for bootload.
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary.
Standalone bootloader polling serial/radio interface.
Processing download image.
Download process was a success.
Download process failed.
Enumerations#
Defines various bootloader states. Use in LED code to signal bootload activity.
Functions#
Initialize GPIO.
Helper function used for displaying bootloader state (for example: with LEDs).
Force activation of bootloader.
State Indicator Macros Documentation#
BL_STATE_DOWN#
#define BL_STATE_DOWNValue:
()
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary.
BL_STATE_POLLING_LOOP#
#define BL_STATE_POLLING_LOOPValue:
()
Standalone bootloader polling serial/radio interface.
Enumeration Documentation#
blState_e#
blState_e
Defines various bootloader states. Use in LED code to signal bootload activity.
| Enumerator | |
|---|---|
| BL_ST_UP | bootloader up |
| BL_ST_DOWN | bootloader going down |
| BL_ST_POLLING_LOOP | polling interfaces |
| BL_ST_DOWNLOAD_LOOP | downloading |
| BL_ST_DOWNLOAD_FAILURE | download failure |
| BL_ST_DOWNLOAD_SUCCESS | download success |
Function Documentation#
bootloadGpioInit#
void bootloadGpioInit (void )
Initialize GPIO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
bootloadStateIndicator#
void bootloadStateIndicator (enum blState_e state)
Helper function used for displaying bootloader state (for example: with LEDs).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| enum blState_e | N/A | state |
bootloadForceActivation#
bool bootloadForceActivation (void )
Force activation of bootloader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |