See Buzzer Control for documentation.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#define NOTE_C3 119
#define NOTE_Db3  112
#define NOTE_D3 106
#define NOTE_Eb3  100
#define NOTE_E3 94
#define NOTE_F3 89
#define NOTE_Gb3  84
#define NOTE_G3 79
#define NOTE_Ab3  74
#define NOTE_A3 70
#define NOTE_Bb3  66
#define NOTE_B3 63
#define NOTE_C4 59
#define NOTE_Db4  55
#define NOTE_D4 52
#define NOTE_Eb4  49
#define NOTE_E4 46
#define NOTE_F4 44
#define NOTE_Gb4  41
#define NOTE_G4 39
#define NOTE_Ab4  37
#define NOTE_A4 35
#define NOTE_Bb4  33
#define NOTE_B4 31
#define NOTE_C5 29
#define NOTE_Db5  27
#define NOTE_D5 26
#define NOTE_Eb5  24
#define NOTE_E5 23
#define NOTE_F5 21
#define NOTE_Gb5  20
#define NOTE_G5 19
#define NOTE_Ab5  18
#define NOTE_A5 17
#define NOTE_Bb5  16
#define NOTE_B5 15

void halPlayTune_P(uint8_t PGM *tune, bool bkg);

void halStackIndicatePresence(void);

Note Definitions#

Flats are used instead of sharps because # is a special character.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

#define

A note which can be used in tune structure definitions.

Functions#

void
halPlayTune_P(uint8_t PGM *tune, bool bkg)

Plays a tune on the piezo buzzer.

void

Causes something to happen on a node (such as playing a tune on the buzzer) that can be used to indicate where it physically is.

Note Definitions Documentation#

NOTE_C3#

#define NOTE_C3
Value:
119

A note which can be used in tune structure definitions.


NOTE_Db3#

#define NOTE_Db3
Value:
112

A note which can be used in tune structure definitions.


NOTE_D3#

#define NOTE_D3
Value:
106

A note which can be used in tune structure definitions.


NOTE_Eb3#

#define NOTE_Eb3
Value:
100

A note which can be used in tune structure definitions.


NOTE_E3#

#define NOTE_E3
Value:
94

A note which can be used in tune structure definitions.


NOTE_F3#

#define NOTE_F3
Value:
89

A note which can be used in tune structure definitions.


NOTE_Gb3#

#define NOTE_Gb3
Value:
84

A note which can be used in tune structure definitions.


NOTE_G3#

#define NOTE_G3
Value:
79

A note which can be used in tune structure definitions.


NOTE_Ab3#

#define NOTE_Ab3
Value:
74

A note which can be used in tune structure definitions.


NOTE_A3#

#define NOTE_A3
Value:
70

A note which can be used in tune structure definitions.


NOTE_Bb3#

#define NOTE_Bb3
Value:
66

A note which can be used in tune structure definitions.


NOTE_B3#

#define NOTE_B3
Value:
63

A note which can be used in tune structure definitions.


NOTE_C4#

#define NOTE_C4
Value:
59

A note which can be used in tune structure definitions.


NOTE_Db4#

#define NOTE_Db4
Value:
55

A note which can be used in tune structure definitions.


NOTE_D4#

#define NOTE_D4
Value:
52

A note which can be used in tune structure definitions.


NOTE_Eb4#

#define NOTE_Eb4
Value:
49

A note which can be used in tune structure definitions.


NOTE_E4#

#define NOTE_E4
Value:
46

A note which can be used in tune structure definitions.


NOTE_F4#

#define NOTE_F4
Value:
44

A note which can be used in tune structure definitions.


NOTE_Gb4#

#define NOTE_Gb4
Value:
41

A note which can be used in tune structure definitions.


NOTE_G4#

#define NOTE_G4
Value:
39

A note which can be used in tune structure definitions.


NOTE_Ab4#

#define NOTE_Ab4
Value:
37

A note which can be used in tune structure definitions.


NOTE_A4#

#define NOTE_A4
Value:
35

A note which can be used in tune structure definitions.


NOTE_Bb4#

#define NOTE_Bb4
Value:
33

A note which can be used in tune structure definitions.


NOTE_B4#

#define NOTE_B4
Value:
31

A note which can be used in tune structure definitions.


NOTE_C5#

#define NOTE_C5
Value:
29

A note which can be used in tune structure definitions.


NOTE_Db5#

#define NOTE_Db5
Value:
27

A note which can be used in tune structure definitions.


NOTE_D5#

#define NOTE_D5
Value:
26

A note which can be used in tune structure definitions.


NOTE_Eb5#

#define NOTE_Eb5
Value:
24

A note which can be used in tune structure definitions.


NOTE_E5#

#define NOTE_E5
Value:
23

A note which can be used in tune structure definitions.


NOTE_F5#

#define NOTE_F5
Value:
21

A note which can be used in tune structure definitions.


NOTE_Gb5#

#define NOTE_Gb5
Value:
20

A note which can be used in tune structure definitions.


NOTE_G5#

#define NOTE_G5
Value:
19

A note which can be used in tune structure definitions.


NOTE_Ab5#

#define NOTE_Ab5
Value:
18

A note which can be used in tune structure definitions.


NOTE_A5#

#define NOTE_A5
Value:
17

A note which can be used in tune structure definitions.


NOTE_Bb5#

#define NOTE_Bb5
Value:
16

A note which can be used in tune structure definitions.


NOTE_B5#

#define NOTE_B5
Value:
15

A note which can be used in tune structure definitions.


Function Documentation#

halPlayTune_P#

void halPlayTune_P (uint8_t PGM * tune, bool bkg)

Plays a tune on the piezo buzzer.

Parameters
TypeDirectionArgument NameDescription
uint8_t PGM *N/Atune

A pointer to tune to play.

boolN/Abkg

Determines whether the tune plays in the background. If true, tune plays in background; if false, tune plays in foreground.

The tune is played in the background if ::bkg is true. Otherwise, the API blocks until the playback of the tune is complete. halPlayTune_P() is not meant to be called back-to-back.

A tune is implemented as follows:

uint8_t PGM hereIamTune[] = {  //All tunes are stored in flash.
   NOTE_B4,  1,                //Plays the note B4 for 100 milliseconds.
   0,        1,                //Pause for 100 milliseconds.
   NOTE_B5,  5,                //Plays the note B5 for 500 milliseconds.
   0,        0                 //NULL terminates the tune.
 };

halStackIndicatePresence#

void halStackIndicatePresence (void )

Causes something to happen on a node (such as playing a tune on the buzzer) that can be used to indicate where it physically is.

Parameters
TypeDirectionArgument NameDescription
voidN/A