Generic set of HAL includes for all platforms.

See also Hardware Abstraction Layer (HAL) API Reference for more documentation.

Some HAL includes are not used or present in builds intended for the Host processor connected to the Ember Network Coprocessor.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef __HAL_H__
#define __HAL_H__

#ifdef HAL_HOST

#include "host/button-common.h"
#include "host/crc.h"
#include "host/led-common.h"
#include "host/micro-common.h"
#include "host/serial.h"
#include "host/system-timer.h"
#include "host/bootloader-eeprom.h"
//Pull in the micro specific ADC, buzzer, and clocks headers.  The
//specific header is chosen by the build include path pointing at
//the appropriate directory.
#include "plugin/adc/adc-stm32f103ret.h"

#ifdef STM32F10X_HD
#include "plugin/buzzer/buzzer-stm32f103ret.h"
#else
#include "plugin/buzzer/buzzer.h"
#endif

#else //HAL_MICRO

// Keep micro and board first for specifics used by other headers
#include "micro/micro.h"
#if !defined(STACK)
#ifdef BOARD_HEADER
  #include BOARD_HEADER
#endif
#ifdef HAL_CONFIG
  #include "hal-config.h"
  #include "ember-hal-config.h"
  #ifndef HAL_GPIO_MAX
  #define HAL_GPIO_MAX 0
  #endif
// if no serial port defined or vuart is used, define dummy value for HAL_SERIAL_APP_PORT
  #if !defined(HAL_SERIAL_APP_BAUD_RATE) || (BSP_SERIAL_APP_PORT == HAL_SERIAL_PORT_VUART)
  #define HAL_SERIAL_APP_BAUD_RATE 0
  #ifndef APP_SERIAL
  #define APP_SERIAL 0
  #endif
  #endif
  #ifdef RF_USARTRF_CS_PORT
  #define BSP_EXTDEV_CS_PORT  RF_USARTRF_CS_PORT
  #define BSP_EXTDEV_CS_PIN   RF_USARTRF_CS_PIN
  #define BSP_EXTDEV_INT_PORT RF_INT_PORT
  #define BSP_EXTDEV_INT_PIN  RF_INT_PIN
  #define BSP_EXTDEV_SDN_PORT RF_SDN_PORT
  #define BSP_EXTDEV_SDN_PIN  RF_SDN_PIN
  #endif
void halConfigPowerDownGpio(void);
void halConfigPowerUpGpio(void);
#elif defined(BOARD_HEADER) //HAL_CONFIG
#define BSP_SERIAL_APP_PORT APP_SERIAL
#ifdef COM_RETARGET_SERIAL
  #define BSP_BUTTON0_PIN   BUTTON0
  #define BSP_BUTTON0_PORT  BUTTON0_PORT
  #define BSP_BUTTON1_PIN   BUTTON1
  #define BSP_BUTTON1_PORT  BUTTON1_PORT
  #include "retargetserialconfig.h"
  #ifdef _USART_ROUTELOC0_MASK
    #define BSP_USART0_TX_LOC RETARGET_TX_LOCATION
    #define BSP_USART0_RX_LOC RETARGET_RX_LOCATION
  #else
    #define BSP_USART0_ROUTE_LOC RETARGET_LOCATION
  #endif

  #define BSP_USART0_TX_PORT RETARGET_TXPORT
  #define BSP_USART0_TX_PIN  RETARGET_TXPIN
  #define BSP_USART0_RX_PORT RETARGET_RXPORT
  #define BSP_USART0_RX_PIN  RETARGET_RXPIN

  #define halConfigInit()
  #define halConfigPowerDownGpio()
  #define halConfigPowerUpGpio()
#endif /*COM_RETARGET_SERIAL*/
#endif
#endif
#include "plugin/antenna/antenna.h"

#if defined(EMBER_STACK_CONNECT)
  #if defined(UNIX_HOST) && !defined(EMBER_TEST)
    #include "plugin/adc/adc.h"
    #include "micro/button.h"
    #include "plugin/buzzer/buzzer.h"
    #include "micro/crc.h"
    #include "micro/endian.h"
    #include "micro/led.h"
    #include "micro/random.h"
    #include "micro/serial.h"
    #include "micro/spi.h"
    #include "micro/system-timer.h"
  #else
// TODO: here we include only the functionalities that we will have on mustang
    #if defined(CORTEXM3)
      #include "plugin/adc/adc.h"
      #include "micro/bootloader-eeprom.h"
      #if defined (_EFR_DEVICE) || defined(CORTEXM3_EMBER_MICRO)
      #include "micro/bootloader-interface.h"
      #endif
      #include "micro/button.h"
      #include "micro/led.h"
      #include "plugin/buzzer/buzzer.h"
      #include "micro/crc.h"
      #include "micro/diagnostic.h"
      #include "micro/endian.h"
    #endif //CORTEXM3
    #include "plugin/sim-eeprom/sim-eeprom.h"
    #include "micro/system-timer.h"
    #include "micro/symbol-timer.h"
    #include "micro/spi.h"
    #if defined(CORTEXM3) || defined(EMBER_TEST)
      #include "micro/serial.h"
    #else
      #include "micro/serial-minimal.h"
    #endif
    #include "micro/random.h"
    #include "micro/token.h"
    #ifdef EMBER_TEST
      #include "plugin/adc/adc.h"
      #include "micro/bootloader-interface.h"
      #include "micro/button.h"
      #include "micro/led.h"
    #endif
  #endif // UNIX_HOST && !EMBER_TEST
#elif defined(EMBER_STACK_OWL_RX)
// TODO: here we include only the functionalities that we will have on OWL-RX
  #include "micro/button.h"
  #include "micro/flash.h"
  #include "micro/led.h"
  #include "micro/dog_glcd.h"
  #include "micro/system-timer.h"
  #include "micro/symbol-timer.h"
  #include "micro/spi.h"
  #include "micro/serial-minimal.h"
  #include "micro/endian.h"
//  #include "micro/random.h"
//  #include "micro/token.h"
//  #ifdef EMBER_TEST
//    #include "plugin/adc/adc.h"
//    #include "micro/bootloader-interface.h"
//    #include "micro/button.h"
//    #include "micro/led.h"
//  #endif
#elif defined(EMBER_STACK_OWL_TX)
// TODO: here we include only the functionalities that we will have on OWL-TX
//  #include "micro/button.h"
//  #include "micro/flash.h"
//  #include "micro/led.h"
//  #include "micro/dog_glcd.h"
//  #include "micro/system-timer.h"
//  #include "micro/symbol-timer.h"
//  #include "micro/spi.h"
//  #include "micro/serial-minimal.h"
//  #include "micro/random.h"
//  #include "micro/token.h"
//  #ifdef EMBER_TEST
//    #include "plugin/adc/adc.h"
//    #include "micro/bootloader-interface.h"
//    #include "micro/button.h"
//    #include "micro/led.h"
//  #endif
#elif defined(EMBER_STACK_WASP)
// TODO: here we include only the functionalities that we will have on mustang
  #if defined(CORTEXM3)
//    #include "plugin/adc/adc.h"
//    #include "micro/bootloader-eeprom.h"
    #include "micro/button.h"
    #include "plugin/buzzer/buzzer.h"
    #include "micro/led.h"
    #include "micro/diagnostic.h"
  #endif //CORTEXM3
  #include "micro/flash.h"
  #include "micro/system-timer.h"
  #include "micro/symbol-timer.h"
  #include "micro/spi.h"
  #if defined(CORTEXM3)
    #include "micro/serial.h"
  #else
    #include "micro/serial-minimal.h"
  #endif
  #include "micro/random.h"
  #include "micro/token.h"
  #ifdef EMBER_TEST
    #include "plugin/adc/adc.h"
    #include "micro/bootloader-interface.h"
    #include "micro/button.h"
    #include "micro/led.h"
  #endif
#elif !defined(EMBER_STACK_IP)
// Pro Stack
  #include "plugin/adc/adc.h"
  #include "micro/button.h"
  #include "plugin/buzzer/buzzer.h"
  #include "micro/crc.h"
  #include "micro/endian.h"
  #include "micro/led.h"
  #include "micro/random.h"
  #include "micro/serial.h"
  #include "micro/spi.h"
  #include "micro/system-timer.h"
  #include "micro/bootloader-eeprom.h"

//Host processors sometimes use the token module.
  #if !defined(EZSP_HOST) || defined(EMBER_AF_API_TOKEN)
    #include "micro/token.h"
  #endif

//Host processors do not use the following modules, therefore the header
//files should be ignored.
  #ifndef EZSP_HOST
    #include "micro/bootloader-interface.h"
    #include "micro/diagnostic.h"
//No public HAL code in release 4.0 uses the symbol timer,
//therefore it should not be in doxygen.
    #ifndef DOXYGEN_SHOULD_SKIP_THIS
      #include "micro/symbol-timer.h"
    #endif // DOXYGEN_SHOULD_SKIP_THIS
  #endif //EZSP_HOST

#else
// IP Stack
  #include "plugin/adc/adc.h"
  #include "micro/button.h"
  #include "plugin/buzzer/buzzer.h"
  #include "micro/crc.h"
  #include "micro/endian.h"
  #include "micro/led.h"
  #include "micro/random.h"
  #include "micro/serial.h"
  #include "micro/spi.h"
  #include "micro/system-timer.h"

//Host processors sometimes use the token module.
  #if !defined(UNIX_HOST) || defined(EMBER_AF_API_TOKEN)
    #include "micro/token.h"
  #endif

//Host processors do not use the following modules, therefore the header
//files should be ignored.
  #ifndef UNIX_HOST
    #include "micro/bootloader-interface.h"
    #include "micro/diagnostic.h"
//No public HAL code in release 4.0 uses the symbol timer,
//therefore it should not be in doxygen.
    #ifndef DOXYGEN_SHOULD_SKIP_THIS
      #include "micro/symbol-timer.h"
    #endif // DOXYGEN_SHOULD_SKIP_THIS
  #endif //UNIX_HOST

#endif // !EMBER_STACK_IP

#endif // !HAL_HOST

#if ((defined(RTOS) && !defined(IP_MODEM_LIBRARY)) \
  || (defined(UNIX_HOST)                           \
  || defined(UNIX_HOST_SIM)))
  #define EMBER_HOST
  #define emAmHost() true
#else
  #define emAmHost() false
#endif

#endif //__HAL_H__

Macros#

#define

Macro Definition Documentation#

emAmHost#

#define emAmHost
Value:
()