Definitions for all the reset cause types.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef DOXYGEN_SHOULD_SKIP_THIS
// *******************
// This file is specifically kept wider than 80 columns in order to keep the information
//   well organized and easy to read by glancing down the columns
// *******************
// The reset types of the EM300 series have both a base type and an
//  extended type.  The extended type is a 16-bit value which has the base
//  type in the upper 8-bits, and the extended classification in the
//  lower 8-bits
// For backwards compatibility with other platforms, only the base type is
//  returned by the halGetResetInfo() API.  For the full extended type, the
//  halGetExtendedResetInfo() API should be called.
// RESET_BASE_DEF macros take the following parameters:
//    RESET_BASE_DEF(basename, value, string)  // description
//        basename - the name used in the enum definition, expanded as RESET_basename
//        value - the value of the enum definition
//        string - the reset string, must be 3 characters
//        description - a comment describing the cause
// RESET_EXT_DEF macros take the following parameters:
//    RESET_EXT_DEF(basename, extname, extvalue, string)  // description
//        basename - the base name used in the enum definition
//        extname - the extended name used in the enum definition, expanded as RESET_basename_extname
//        extvalue - the LSB value of the enum definition, combined with the value of the base value in the MSB
//        string - the reset string, must be 3 characters
//        description - a comment describing the cause
// *******************
// This file is specifically kept wider than 80 columns in order to keep the information
//   well organized and easy to read by glancing down the columns
// (Yes, this comment is mentioned multiple times in the file)
// *******************
// This file wants to use the bareword BOOTLOADER, which is sometimes a symbol.
// To allow this we will undefine the symbol here and restore it at the end of
// this file.
#ifdef BOOTLOADER
  #define SAVED_BOOTLOADER BOOTLOADER
  #undef BOOTLOADER
#endif
//[[
//   The first 3 (unknown, fib, and bootloader) reset base types and their
//     extended values should never be changed, as they are used by
//     bootloaders in the field which can never be changed.
//   The later reset base and extended types may be changed over time
//]]
RESET_BASE_DEF(UNKNOWN, 0x00U, "UNK")                    // Underterminable cause
RESET_EXT_DEF(UNKNOWN, UNKNOWN, 0x00U, "UNK")               // Undeterminable cause
RESET_BASE_DEF(FIB, 0x01U, "FIB")                          // Reset originated from the FIB bootloader
RESET_EXT_DEF(FIB, GO, 0x00U, "GO ")                          // FIB bootloader caused a reset to main flash
RESET_EXT_DEF(FIB, BOOTLOADER, 0x01U, "BTL")                  // FIB bootloader is instructing ember bootloader to run
RESET_EXT_DEF(FIB, GO2, 0x02U, "GO2")                         // GO2 (unused)
RESET_EXT_DEF(FIB, GO3, 0x03U, "GO3")                         // GO3 (unused)
RESET_EXT_DEF(FIB, GO4, 0x04U, "GO4")                         // GO4 (unused)
RESET_EXT_DEF(FIB, GO5, 0x05U, "GO5")                         // GO5 (unused)
RESET_EXT_DEF(FIB, GO6, 0x06U, "GO6")                         // GO6 (unused)
RESET_EXT_DEF(FIB, GO7, 0x07U, "GO7")                         // GO7 (unused)
RESET_EXT_DEF(FIB, GO8, 0x08U, "GO8")                         // GO8 (unused)
RESET_EXT_DEF(FIB, GO9, 0x09U, "GO9")                         // GO9 (unused)
RESET_EXT_DEF(FIB, GOA, 0x0AU, "GOA")                         // GOA (unused)
RESET_EXT_DEF(FIB, GOB, 0x0BU, "GOB")                         // GOB (unused)
RESET_EXT_DEF(FIB, GOC, 0x0CU, "GOC")                         // GOC (unused)
RESET_EXT_DEF(FIB, GOD, 0x0DU, "GOD")                         // GOD (unused)
RESET_EXT_DEF(FIB, GOE, 0x0EU, "GOE")                         // GOE (unused)
RESET_EXT_DEF(FIB, GOF, 0x0FU, "GOF")                         // GOF (unused)
RESET_EXT_DEF(FIB, JUMP, 0x10U, "JMP")                        // FIB bootloader is jumping to a specific flash address
RESET_EXT_DEF(FIB, BAUDRATE, 0x11U, "BDR")                    // FIB bootloader detected a high baud rate, causes ember bootloader to run
RESET_EXT_DEF(FIB, UNPROTECT, 0x12U, "UPR")                   // Read protection disabled, flash should be erased
RESET_EXT_DEF(FIB, BOOTMODE, 0x13U, "BTM")                    // BOOTMODE was not held long enough
RESET_EXT_DEF(FIB, MISMATCH, 0x14U, "MSM")                    // MISMATCHED FIB Bootloader & Part Data
RESET_EXT_DEF(FIB, FATAL, 0x15U, "FTL")                       // FIB Fatal Error
RESET_BASE_DEF(BOOTLOADER, 0x02U, "BTL")                   // Reset relates to an Ember bootloader
RESET_EXT_DEF(BOOTLOADER, UNKNOWN, 0x00U, "UNK")               // Unknown bootloader cause (should never occur)
RESET_EXT_DEF(BOOTLOADER, GO, 0x01U, "GO ")                    // Bootloader caused reset telling app to run
RESET_EXT_DEF(BOOTLOADER, BOOTLOAD, 0x02U, "BTL")              // Application requested that bootloader runs
RESET_EXT_DEF(BOOTLOADER, BADIMAGE, 0x03U, "BAD")              // Application bootloader detect bad external upgrade image
RESET_EXT_DEF(BOOTLOADER, FATAL, 0x04U, "FTL")                 // Fatal Error or assert in bootloader
RESET_EXT_DEF(BOOTLOADER, FORCE, 0x05U, "FRC")                 // Forced bootloader activation
RESET_EXT_DEF(BOOTLOADER, OTAVALID, 0x06U, "OTA")              // OTA Bootloader mode activation
RESET_EXT_DEF(BOOTLOADER, DEEPSLEEP, 0x07U, "DSL")             // Bootloader initiated deep sleep
//[[ -- Reset types below here may be changed in the future if absolutely necessary -- ]]
RESET_BASE_DEF(EXTERNAL, 0x03U, "EXT")                     // External reset trigger
RESET_EXT_DEF(EXTERNAL, UNKNOWN, 0x00U, "UNK")                // Unknown external cause (should never occur)
RESET_EXT_DEF(EXTERNAL, PIN, 0x01U, "PIN")                    // External pin reset
RESET_BASE_DEF(POWERON, 0x04U, "PWR")                      // Poweron reset type, supply voltage < power-on threshold
RESET_EXT_DEF(POWERON, UNKNOWN, 0x00U, "UNK")                 // Unknown poweron reset (should never occur)
RESET_EXT_DEF(POWERON, HV, 0x01U, "HV ")                      // High voltage poweron
RESET_EXT_DEF(POWERON, LV, 0x02U, "LV ")                      // Low voltage poweron
RESET_BASE_DEF(WATCHDOG, 0x05U, "WDG")                     // Watchdog reset occurred
RESET_EXT_DEF(WATCHDOG, UNKNWON, 0x00U, "UNK")                // Unknown watchdog reset (should never occur)
RESET_EXT_DEF(WATCHDOG, EXPIRED, 0x01U, "EXP")                // Watchdog timer expired
RESET_EXT_DEF(WATCHDOG, CAUGHT, 0x02U, "LWM")                 // Watchdog low watermark expired and caught extended info
RESET_BASE_DEF(SOFTWARE, 0x06U, " SW")                     // Software triggered reset
RESET_EXT_DEF(SOFTWARE, UNKNOWN, 0x00U, "UNK")                // Unknown software cause
RESET_EXT_DEF(SOFTWARE, REBOOT, 0x01U, "RBT")                 // General software reboot
RESET_EXT_DEF(SOFTWARE, DEEPSLEEP, 0x02U, "DSL")              // App initiated deep sleep
RESET_BASE_DEF(CRASH, 0x07U, "CRS")                        // Software crash
RESET_EXT_DEF(CRASH, UNKNOWN, 0x00U, "UNK")                   // Unknown crash
RESET_EXT_DEF(CRASH, ASSERT, 0x01U, "AST")                    // a self-check assert in the code failed
RESET_BASE_DEF(FLASH, 0x08U, "FSH")                        // Flash failure cause reset
RESET_EXT_DEF(FLASH, UNKNWON, 0x00U, "UNK")                   // Unknown flash failure
RESET_EXT_DEF(FLASH, VERIFY, 0x01U, "VFY")                    // Flash write verify failure
RESET_EXT_DEF(FLASH, INHIBIT, 0x02U, "INH")                   // Flash write inhibited: already written
RESET_BASE_DEF(FATAL, 0x09U, "BAD")                        // A non-recoverable fatal error occurred
RESET_EXT_DEF(FATAL, UNKNOWN, 0x00U, "UNK")                   // Unknown fatal error (should never occur)
RESET_EXT_DEF(FATAL, LOCKUP, 0x01U, "LCK")                    // CPU Core locked up
RESET_EXT_DEF(FATAL, CRYSTAL, 0x02U, "XTL")                   // 24MHz crystal failure
RESET_EXT_DEF(FATAL, OPTIONBYTE, 0x03U, "OBF")                // option byte complement error
RESET_BASE_DEF(FAULT, 0x0AU, "FLT")                        // A access fault occurred
RESET_EXT_DEF(FAULT, UNKNOWN, 0x00U, "UNK")                   // An unknown fault occurred
RESET_EXT_DEF(FAULT, HARD, 0x01U, "HRD")                      // Hard fault
RESET_EXT_DEF(FAULT, MEM, 0x02U, "MEM")                       // Memory protection violation
RESET_EXT_DEF(FAULT, BUS, 0x03U, "BUS")                       // Bus fault
RESET_EXT_DEF(FAULT, USAGE, 0x04U, "USG")                     // Usage fault
RESET_EXT_DEF(FAULT, DBGMON, 0x05U, "DBG")                    // Debug monitor fault
RESET_EXT_DEF(FAULT, PROTDMA, 0x06U, "DMA")                   // DMA RAM protection violation
RESET_EXT_DEF(FAULT, BADVECTOR, 0x07U, "VCT")                 // Uninitialized interrupt vector
// Restore the value of the BOOTLOADER symbol if we had to save it off in this
// file so that the word BOOTLOADER could be used.
#ifdef SAVED_BOOTLOADER
  #define BOOTLOADER SAVED_BOOTLOADER
  #undef SAVED_BOOTLOADER
#endif
#endif //DOXYGEN_SHOULD_SKIP_THIS