Modules#
EmberZNet API for accessing and setting stack information. See Stack Information for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_STACK_INFO_H
#define SILABS_STACK_INFO_H
void emberStackStatusHandler(EmberStatus status);
EmberNetworkStatus emberNetworkState(void);
bool emberStackIsUp(void);
EmberStatus emberWriteNodeData(bool erase);
#ifdef DOXYGEN_SHOULD_SKIP_THIS
EmberEUI64 emberGetEui64(void);
bool emberIsLocalEui64(EmberEUI64 eui64);
EmberNodeId emberGetNodeId(void);
EmberNodeId emberRadioGetNodeId(void);
void emberSetManufacturerCode(uint16_t code);
void emberSetPowerDescriptor(uint16_t descriptor);
void emberSetMaximumIncomingTransferSize(uint16_t size);
void emberSetMaximumOutgoingTransferSize(uint16_t size);
void emberSetDescriptorCapability(uint8_t capability);
#else // Doxygen ignores the following
extern EmberEUI64 emLocalEui64;
#define emberGetEui64() (emLocalEui64)
#define emberIsLocalEui64(eui64) \
(MEMCOMPARE((eui64), emLocalEui64, EUI64_SIZE) == 0)
EmberNodeId emberGetNodeId(void);
EmberNodeId emberRadioGetNodeId(void);
extern uint16_t emManufacturerCode;
extern uint16_t emPowerDescriptor;
extern uint16_t emMaximumIncomingTransferSize;
extern uint16_t emMaximumOutgoingTransferSize;
extern uint8_t emDescriptorCapability;
enum {
EMBER_ROUTE_ERROR_NO_ROUTE_AVAILABLE = 0x00,
EMBER_ROUTE_ERROR_TREE_LINK_FAILURE = 0x01,
EMBER_ROUTE_ERROR_NON_TREE_LINK_FAILURE = 0x02,
EMBER_ROUTE_ERROR_LOW_BATTERY_LEVEL = 0x03,
EMBER_ROUTE_ERROR_NO_ROUTING_CAPACITY = 0x04,
EMBER_ROUTE_ERROR_NO_INDIRECT_CAPACITY = 0x05,
EMBER_ROUTE_ERROR_INDIRECT_TRANSACTION_EXPIRY = 0x06,
EMBER_ROUTE_ERROR_TARGET_DEVICE_UNAVAILABLE = 0x07,
EMBER_ROUTE_ERROR_TARGET_ADDRESS_UNALLOCATED = 0x08,
EMBER_ROUTE_ERROR_PARENT_LINK_FAILURE = 0x09,
EMBER_ROUTE_ERROR_VALIDATE_ROUTE = 0x0A,
EMBER_ROUTE_ERROR_SOURCE_ROUTE_FAILURE = 0x0B,
EMBER_ROUTE_ERROR_MANY_TO_ONE_ROUTE_FAILURE = 0x0C,
EMBER_ROUTE_ERROR_ADDRESS_CONFLICT = 0x0D,
EMBER_ROUTE_ERROR_VERIFY_ADDRESSES = 0x0E,
EMBER_ROUTE_ERROR_PAN_IDENTIFIER_UPDATE = 0x0F,
ZIGBEE_NETWORK_STATUS_NETWORK_ADDRESS_UPDATE = 0x10,
ZIGBEE_NETWORK_STATUS_BAD_FRAME_COUNTER = 0x11,
ZIGBEE_NETWORK_STATUS_BAD_KEY_SEQUENCE_NUMBER = 0x12,
ZIGBEE_NETWORK_STATUS_UNKNOWN_COMMAND = 0x13
};
EmberStatus emberSetBrokenRouteErrorCode(uint8_t errorCode);
#define emberSetManufacturerCode(code) \
(emManufacturerCode = (code))
#define emberSetPowerDescriptor(descriptor) \
(emPowerDescriptor = (descriptor))
#define emberSetMaximumIncomingTransferSize(size) \
(emMaximumIncomingTransferSize = (size))
#define emberSetMaximumOutgoingTransferSize(size) \
(emMaximumOutgoingTransferSize = (size))
#define emberSetDescriptorCapability(capability) \
(emDescriptorCapability = (capability))
#endif
EmberStatus emberGetNetworkParameters(EmberNetworkParameters *parameters);
EmberStatus emberGetRadioParameters(uint8_t phyIndex, EmberMultiPhyRadioParameters *parameters);
EmberStatus emberGetNodeType(EmberNodeType *resultLocation);
EmberStatus emberSetRadioChannel(uint8_t channel);
EmberStatus emberSetLogicalAndRadioChannel(uint8_t channel);
uint8_t emberGetRadioChannel(void);
EmberStatus emberSetRadioPower(int8_t power);
int8_t emberGetRadioPower(void);
void *emberGetRailHandle(void);
EmberPanId emberGetPanId(void);
EmberPanId emberRadioGetPanId(void);
void emberGetExtendedPanId(uint8_t *resultLocation);
extern const uint8_t emberStackProfileId[];
typedef struct {
uint16_t profileId;
uint16_t deviceId;
uint8_t deviceVersion;
uint8_t inputClusterCount;
uint8_t outputClusterCount;
} EmberEndpointDescription;
typedef struct {
uint8_t endpoint;
EmberEndpointDescription const * description;
uint16_t const * inputClusterList;
uint16_t const * outputClusterList;
} EmberEndpoint;
extern uint8_t emberEndpointCount;
extern EmberEndpoint emberEndpoints[];
uint8_t emberGetEndpoint(uint8_t index);
bool emberGetEndpointDescription(uint8_t endpoint,
EmberEndpointDescription *result);
uint16_t emberGetEndpointCluster(uint8_t endpoint,
EmberClusterListId listId,
uint8_t listIndex);
#ifdef DOXYGEN_SHOULD_SKIP_THIS
bool emberIsNodeIdValid(EmberNodeId nodeId);
#else
#define emberIsNodeIdValid(nodeId) ((nodeId) < EMBER_DISCOVERY_ACTIVE_NODE_ID)
#endif
EmberNodeId emberLookupNodeIdByEui64(EmberEUI64 eui64);
EmberStatus emberLookupEui64ByNodeId(EmberNodeId nodeId,
EmberEUI64 eui64Return);
void emberCounterHandler(EmberCounterType type, EmberCounterInfo info);
bool emberCounterRequiresPhyIndex(EmberCounterType type);
bool emberCounterRequiresDestinationNodeId(EmberCounterType type);
void emberStackTokenChangedHandler(uint16_t tokenAddress);
bool emberRtosIdleHandler(uint32_t *idleTimeMs);
void emberRtosStackWakeupIsrHandler(void);
EmberStatus emberGetNeighbor(uint8_t index, EmberNeighborTableEntry *result);
EmberStatus emberSetRoutingShortcutThreshold(uint8_t costThresh);
uint8_t emberGetRoutingShortcutThreshold(void);
EmberStatus emberSetInitialNeighborOutgoingCost(uint8_t cost);
uint8_t emberGetInitialNeighborOutgoingCost(void);
void emberResetRejoiningNeighborsFC(bool reset);
bool emberIsResetRejoiningNeighborsFCEnabled(void);
EmberStatus emberGetNeighborFrameCounter(EmberEUI64 nodeEui64,
uint32_t *returnFrameCounter);
EmberStatus emberGetRouteTableEntry(uint8_t index, EmberRouteTableEntry *result);
uint8_t emberStackProfile(void);
uint8_t emberSecurityLevel(void);
#ifdef DOXYGEN_SHOULD_SKIP_THIS
uint8_t emberTreeDepth(void);
#endif
uint8_t emberNeighborCount(void);
#ifdef DOXYGEN_SHOULD_SKIP_THIS
uint8_t emberRouteTableSize(void);
#else // Doxgyen ignores the following
// The '+ 0' prevents anyone from accidentally assigning to these.
#define emberTreeDepth() (emTreeDepth + 0)
#define emberMaxDepth() (emMaxDepth + 0)
#define emberRouteTableSize() (emRouteTableSize + 0)
extern uint8_t emDefaultSecurityLevel;
extern uint8_t emMaxHops;
extern uint8_t emRouteTableSize;
extern uint8_t emSourceRouteTableSize;
extern uint8_t emMaxDepth; // The maximum tree depth.
extern uint8_t emTreeDepth; // The current depth.
extern uint8_t emEndDeviceConfiguration;
void emberSetStackProfile(uint8_t stackProfile);
void emberSetSecurityLevel(uint8_t securityLevel);
#endif
uint8_t emberNextZigbeeSequenceNumber(void);
uint8_t emberGetMaxNwkRetries(void);
EmberStatus emberSetTxPowerMode(uint16_t txPowerMode);
uint16_t emberGetTxPowerMode(void);
EmberStatus emberSetNodeId(EmberNodeId nodeId);
uint8_t emberGetPhyInterfaceCount(void);
void emberRadioNeedsCalibratingHandler(void);
void sl_mac_calibrate_current_channel(void);
//General connectivity status APIs
void emberSetLongUpTime(bool hasLongUpTime);
void emberSetHubConnectivity(bool connected);
bool emberIsUpTimeLong(void);
bool emberIsHubConnected(void);
EmberStatus emberRadioGetSchedulerPriorities(EmberMultiprotocolPriorities *priorities);
EmberStatus emberRadioSetSchedulerPriorities(const EmberMultiprotocolPriorities *priorities);
EmberStatus emberRadioSetSchedulerSliptime(uint32_t slipTime);
EmberStatus emberRadioGetSchedulerSliptime(uint32_t *slipTime);
EmberStatus emberGetBeaconClassificationParams(EmberBeaconClassificationParams* param);
EmberStatus emberSetBeaconClassificationParams(EmberBeaconClassificationParams* param);
EmberStatus slx_zigbee_routing_set_route_record_policy(sl_zigbee_route_record_policy_type_t policy);
uint8_t slx_zigbee_routing_get_route_record_policy(void);
#endif // SILABS_STACK_INFO_H
Radio-specific Functions#
Enables boost power mode and/or the alternate transmit path.
Returns the current configuration of boost power mode and alternate transmitter output.
Sets the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
Returns the number of PHY interfaces present.
The radio calibration callback function.
Calibrates the current channel. The stack will notify the application of the need for channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
sets the device uptime to be long or short the uptime is then advertised in the beacons
sets the hub connectivity to be true or false the hub connectivity is then advertised in the beacons
API used to get the current scheduler priorities used for Zigbee multiprotocol operations.
API used to set the current scheduler priorities used for Zigbee multiprotocol operations.
Set the multiprotocol slip time.
Get the multiprotocol slip time.
API used to get current beacon classification parameter settings.
API used to set current beacon classification parameters.
Set the route record policy.
Get the route record policy.
Variables#
The application must provide a definition for this variable.
The application must provide a definition for this variable.
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
Functions#
A callback invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the emberGetNetworkParameters() function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
Returns the current join status.
Indicates whether the stack is currently up.
Writes node data to stack token.
Returns the EUI64 ID of the local node.
Determines whether eui64 is the local node's EUI64 ID.
Returns the 16-bit node ID of local node on the current logical network.
Returns the 16-bit node ID of local node on the network it is currently tuned on.
Sets the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
Sets the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
Sets the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
Sets the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
Sets the descriptor capability field of the node.
Copies the current network parameters into the structure provided by the caller.
Copies the current radio parameters into the structure provided by the caller.
Copies the current node type into the location provided by the caller.
Sets the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
Sets the current logical and physical channel.
Gets the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
Sets the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
Gets the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
Returns the RAIL level handle required to make RAIL API calls. Will return NULL if RAIL is not in use.
Returns the local node's PAN ID of the current logical network.
Returns the local node's PAN ID of the current radio network.
Fetches a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see emberNetworkState), the Extended PAN ID returned will be an invalid value.
Retrieves the endpoint number for the index'th endpoint. index must be less than the value of emberEndpointCount.
Retrieves the endpoint description for the given endpoint.
Retrieves a cluster ID from one of the cluster lists associated with the given endpoint.
Determines whether nodeId is valid.
Returns the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
Returns the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
A callback invoked to inform the application that a stack token has changed.
A callback to allow the application to manage idling the MCU.
A callback to request the application to wake up the stack task.
Copies a neighbor table entry to the structure that result points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using emberNeighborCount().
Sets the routing shortcut threshold to directly use a neighbor instead of performing routing.
Gets the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
Sets neighbor's initial outgoing link cost.
Gets neighbor's initial outgoing link cost.
Indicates whether a rejoining neighbor's incoming FC should be reset.
Checks if resetting the incoming FC for a rejoining neighbor is enabled.
This function gets the last received frame counter as found in the Network Auxiliary header for the specified neighbor or child.
Copies a route table entry to the structure that the result points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via emberRouteTableSize().
Returns the stack profile of the network which the node has joined.
Returns the security level of the network which the node has joined.
Returns the depth of the node in the network.
Returns the number of active entries in the neighbor table.
Returns the size of the route table.
Increments and returns the Zigbee sequence number.
Get max number of NWK retries.
Radio-specific Functions Documentation#
emberSetTxPowerMode#
EmberStatus emberSetTxPowerMode (uint16_t txPowerMode)
Enables boost power mode and/or the alternate transmit path.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | txPowerMode | Specifies which transmit power mode options should be activated. This parameter should be set to one of the literal values described in stack/include/ember-types.h. Any power option not specified in the txPowerMode parameter will be deactivated. |
Boost power mode is a high-performance radio mode, which offers increased transmit power and receive sensitivity at the cost of an increase in power consumption. emberInit() calls this function using the power mode and transmitter output settings as specified in the MFG_PHY_CONFIG token (with each bit inverted so that the default token value of 0xffff corresponds to normal power mode and bi-directional RF transmitter output). The application only needs to call emberSetTxPowerMode() to use a power mode or transmitter output setting different than specified in the MFG_PHY_CONFIG token. After the initial call to emberSetTxPowerMode(), the stack will automatically maintain the specified power mode configuration across sleep/wake cycles.
Returns
EMBER_SUCCESS if successful; an error code otherwise.
emberGetTxPowerMode#
uint16_t emberGetTxPowerMode (void )
Returns the current configuration of boost power mode and alternate transmitter output.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current TX power mode.
emberSetNodeId#
EmberStatus emberSetNodeId (EmberNodeId nodeId)
Sets the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | Specifies the short ID to be assigned to the node. |
Returns
EMBER_SUCCESS if successful; an error code otherwise.
emberGetPhyInterfaceCount#
uint8_t emberGetPhyInterfaceCount (void )
Returns the number of PHY interfaces present.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The number of PHY interface(s).
emberRadioNeedsCalibratingHandler#
void emberRadioNeedsCalibratingHandler (void )
The radio calibration callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The Voltage Controlled Oscillator (VCO) can drift with temperature changes. During every call to emberTick(), the stack will check to see if the VCO has drifted. If the VCO has drifted, the stack will call emberRadioNeedsCalibratingHandler() to inform the application that it should perform calibration of the current channel as soon as possible. Calibration can take up to 150 ms. The default callback function implementation provided here performs the calibration immediately. The application can define its own callback by defining ::EMBER_APPLICATION_HAS_CUSTOM_RADIO_CALIBRATION_CALLBACK in its CONFIGURATION_HEADER. It can then failsafe any critical processes or peripherals before calling ::emberCalibrateCurrentChannel(). The application must call ::emberCalibrateCurrentChannel() in response to this callback to maintain expected radio performance.
sl_mac_calibrate_current_channel#
void sl_mac_calibrate_current_channel (void )
Calibrates the current channel. The stack will notify the application of the need for channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberSetLongUpTime#
void emberSetLongUpTime (bool hasLongUpTime)
sets the device uptime to be long or short the uptime is then advertised in the beacons
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | hasLongUpTime |
emberSetHubConnectivity#
void emberSetHubConnectivity (bool connected)
sets the hub connectivity to be true or false the hub connectivity is then advertised in the beacons
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | connected |
emberIsUpTimeLong#
bool emberIsUpTimeLong (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if device uptime is long, false otherwise
emberIsHubConnected#
bool emberIsHubConnected (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if there is hub connectivity, false otherwise
emberRadioGetSchedulerPriorities#
EmberStatus emberRadioGetSchedulerPriorities (EmberMultiprotocolPriorities * priorities)
API used to get the current scheduler priorities used for Zigbee multiprotocol operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMultiprotocolPriorities * | N/A | priorities | A pointer to a structure to store the current priorities in. This must not be NULL. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
For more details on what these priorities are and how to use them see UG305, the Dynamic Multiprotocol User Guide.
emberRadioSetSchedulerPriorities#
EmberStatus emberRadioSetSchedulerPriorities (const EmberMultiprotocolPriorities * priorities)
API used to set the current scheduler priorities used for Zigbee multiprotocol operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberMultiprotocolPriorities * | N/A | priorities | A pointer to a structure of the new priorities to use. This must not be NULL. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
For more details on what these priorities are and how to use them see UG305, the Dynamic Multiprotocol User Guide.
emberRadioSetSchedulerSliptime#
EmberStatus emberRadioSetSchedulerSliptime (uint32_t slipTime)
Set the multiprotocol slip time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | slipTime | The value to set the slip time to for each transmit. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
Use this to update the slip time passed to the radio scheduler for each transmit from the PHY layer. The smaller this is set the lower the potential multi-protocol induced latency is, but it makes packets more likely to fail to be transmitted. For more details on slip time see UG305.
emberRadioGetSchedulerSliptime#
EmberStatus emberRadioGetSchedulerSliptime (uint32_t * slipTime)
Get the multiprotocol slip time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | N/A | slipTime | A pointer to the place to store the current slip time |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
Use this to get the current value of the multiprotocol slip time used for each transmit at the PHY layer. For more details on slip time see UG305.
emberGetBeaconClassificationParams#
EmberStatus emberGetBeaconClassificationParams (EmberBeaconClassificationParams * param)
API used to get current beacon classification parameter settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberBeaconClassificationParams * | N/A | param |
emberSetBeaconClassificationParams#
EmberStatus emberSetBeaconClassificationParams (EmberBeaconClassificationParams * param)
API used to set current beacon classification parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberBeaconClassificationParams * | N/A | param |
slx_zigbee_routing_set_route_record_policy#
EmberStatus slx_zigbee_routing_set_route_record_policy (sl_zigbee_route_record_policy_type_t policy)
Set the route record policy.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_route_record_policy_type_t | N/A | policy | A pointer to the place to store the current slip time |
Returns
EMBER_SUCCESS if route record policy was sucessfully set EMBER_BAD_ARGUMENT otherwise.
Use this to set the policy for senidng a route record message to a concentrator Note that policies other than the default ROUTE_RECORD_POLICY_ACK_BY_SOURCE_ROUTED_MESSAGE may result in behaviour not compliant with the Zigbee specification
slx_zigbee_routing_get_route_record_policy#
uint8_t slx_zigbee_routing_get_route_record_policy (void )
Get the route record policy.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The route record policy
Use this to get the current value of the route record policy
Variable Documentation#
emberStackProfileId#
const uint8_t emberStackProfileId[]
The application must provide a definition for this variable.
emberEndpointCount#
uint8_t emberEndpointCount
The application must provide a definition for this variable.
emberEndpoints#
EmberEndpoint emberEndpoints[]
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
This can be done either by providing a definition of emberEndpoints or by providing definitions of emberGetEndpoint(), emberGetEndpointDescription() and emberGetEndpointCluster(). Using the array is often simpler, but consumes large amounts of memory if emberEndpointCount is large.
If the application provides definitions for the three functions, it must define EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Function Documentation#
emberStackStatusHandler#
void emberStackStatusHandler (EmberStatus status)
A callback invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the emberGetNetworkParameters() function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberStatus | N/A | status | Stack status. One of the following: |
The application is free to begin messaging after it receives the EMBER_NETWORK_UP status. However, routes discovered immediately after the stack comes up may be suboptimal because the routes are based on the neighbor table's information about two-way links with neighboring nodes, which is obtained from periodic ZigBee Link Status messages. It can take two or three link status exchange periods (of 16 seconds each) before the neighbor table has a good estimate of link quality to neighboring nodes. Therefore, the application may improve the quality of initially discovered routes by waiting after startup to give the neighbor table time to be populated.
emberNetworkState#
EmberNetworkStatus emberNetworkState (void )
Returns the current join status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns a value indicating whether the node is joining, joined to, or leaving a network.
Returns
An EmberNetworkStatus value indicating the current join status.
emberStackIsUp#
bool emberStackIsUp (void )
Indicates whether the stack is currently up.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns true if the stack is joined to a network and ready to send and receive messages. This reflects only the state of the local node; it does not indicate whether other nodes are able to communicate with this node.
Returns
True if the stack is up, false otherwise.
emberWriteNodeData#
EmberStatus emberWriteNodeData (bool erase)
Writes node data to stack token.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | erase | Indicates whether the node type should be erased. |
Returns
The status of the operation and an error code if unsuccessful.
emberGetEui64#
EmberEUI64 emberGetEui64 (void )
Returns the EUI64 ID of the local node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 64-bit ID.
emberIsLocalEui64#
bool emberIsLocalEui64 (EmberEUI64 eui64)
Determines whether eui64 is the local node's EUI64 ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | eui64 | An EUI64 ID. |
Returns
True if
eui64is the local node's ID, otherwise false.
emberGetNodeId#
EmberNodeId emberGetNodeId (void )
Returns the 16-bit node ID of local node on the current logical network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 16-bit ID.
emberRadioGetNodeId#
EmberNodeId emberRadioGetNodeId (void )
Returns the 16-bit node ID of local node on the network it is currently tuned on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 16-bit ID.
emberSetManufacturerCode#
void emberSetManufacturerCode (uint16_t code)
Sets the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | code | The manufacturer code for the local node. |
emberSetPowerDescriptor#
void emberSetPowerDescriptor (uint16_t descriptor)
Sets the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | descriptor | The new power descriptor for the local node. |
emberSetMaximumIncomingTransferSize#
void emberSetMaximumIncomingTransferSize (uint16_t size)
Sets the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | size | The maximum incoming transfer size for the local node. |
emberSetMaximumOutgoingTransferSize#
void emberSetMaximumOutgoingTransferSize (uint16_t size)
Sets the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | size | The maximum outgoing transfer size for the local node. |
emberSetDescriptorCapability#
void emberSetDescriptorCapability (uint8_t capability)
Sets the descriptor capability field of the node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | capability | The descriptor capability of the local node. |
emberGetNetworkParameters#
EmberStatus emberGetNetworkParameters (EmberNetworkParameters * parameters)
Copies the current network parameters into the structure provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNetworkParameters * | N/A | parameters | A pointer to an EmberNetworkParameters value into which the current network parameters will be copied. |
Returns
An EmberStatus value indicating the success or failure of the command.
emberGetRadioParameters#
EmberStatus emberGetRadioParameters (uint8_t phyIndex, EmberMultiPhyRadioParameters * parameters)
Copies the current radio parameters into the structure provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | phyIndex | The index of the PHY interface for radio parameters.
|
| EmberMultiPhyRadioParameters * | N/A | parameters |
Returns
An EmberStatus value indicating the success or failure of the command.
emberGetNodeType#
EmberStatus emberGetNodeType (EmberNodeType * resultLocation)
Copies the current node type into the location provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeType * | N/A | resultLocation | A pointer to an EmberNodeType value into which the current node type will be copied. |
Returns
An EmberStatus value that indicates the success or failure of the command.
emberSetRadioChannel#
EmberStatus emberSetRadioChannel (uint8_t channel)
Sets the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | channel | The desired radio channel. |
Note: When using this API, all devices on a network must use the same channel.
Returns
An EmberStatus value indicating the success or failure of the command.
emberSetLogicalAndRadioChannel#
EmberStatus emberSetLogicalAndRadioChannel (uint8_t channel)
Sets the current logical and physical channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | channel |
emberGetRadioChannel#
uint8_t emberGetRadioChannel (void )
Gets the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current radio channel.
emberSetRadioPower#
EmberStatus emberSetRadioPower (int8_t power)
Sets the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int8_t | N/A | power | A desired radio output power, in dBm. |
Returns
An EmberStatus value indicating the success or failure of the command. Failure indicates that the requested power level is out of range.
emberGetRadioPower#
int8_t emberGetRadioPower (void )
Gets the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current radio output power, in dBm.
emberGetRailHandle#
void* emberGetRailHandle (void )
Returns the RAIL level handle required to make RAIL API calls. Will return NULL if RAIL is not in use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A RAIL handle
emberGetPanId#
EmberPanId emberGetPanId (void )
Returns the local node's PAN ID of the current logical network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A PAN ID.
emberRadioGetPanId#
EmberPanId emberRadioGetPanId (void )
Returns the local node's PAN ID of the current radio network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A PAN ID.
emberGetExtendedPanId#
void emberGetExtendedPanId (uint8_t * resultLocation)
Fetches a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see emberNetworkState), the Extended PAN ID returned will be an invalid value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | resultLocation |
emberGetEndpoint#
uint8_t emberGetEndpoint (uint8_t index)
Retrieves the endpoint number for the index'th endpoint. index must be less than the value of emberEndpointCount.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of an endpoint (as distinct from its endpoint number). This must be less than the value of emberEndpointCount. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Returns
The endpoint number for the index'th endpoint.
emberGetEndpointDescription#
bool emberGetEndpointDescription (uint8_t endpoint, EmberEndpointDescription * result)
Retrieves the endpoint description for the given endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | The endpoint whose description is to be returned. |
| EmberEndpointDescription * | N/A | result | A pointer to the location to which to copy the endpoint description. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its ::CONFIGURATION_HEADER.
Returns
True if the description was copied to result, or false if the endpoint is not active.
emberGetEndpointCluster#
uint16_t emberGetEndpointCluster (uint8_t endpoint, EmberClusterListId listId, uint8_t listIndex)
Retrieves a cluster ID from one of the cluster lists associated with the given endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | The endpoint from which the cluster ID is to be read. |
| EmberClusterListId | N/A | listId | The list from which the cluster ID is to be read. |
| uint8_t | N/A | listIndex | The index of the desired cluster ID in the list. This value must be less than the length of the list. The length can be found in the EmberEndpointDescription for this endpoint. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Returns
The cluster ID at position listIndex in the specified endpoint cluster list.
emberIsNodeIdValid#
bool emberIsNodeIdValid (EmberNodeId nodeId)
Determines whether nodeId is valid.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | A node ID. |
Returns
True if
nodeIdis valid, false otherwise.
emberLookupNodeIdByEui64#
EmberNodeId emberLookupNodeIdByEui64 (EmberEUI64 eui64)
Returns the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | eui64 | The EUI64 of the node to look up. |
Returns
The short ID of the node or EMBER_NULL_NODE_ID if the short ID is not known.
emberLookupEui64ByNodeId#
EmberStatus emberLookupEui64ByNodeId (EmberNodeId nodeId, EmberEUI64 eui64Return)
Returns the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | The short ID of the node to look up. |
| EmberEUI64 | N/A | eui64Return | The EUI64 of the node is copied here if it is known. |
Returns
An EmberStatus value:
EMBER_SUCCESS - eui64Return has been set to the EUI64 of the node.
EMBER_ERR_FATAL - The EUI64 of the node is not known.
emberCounterHandler#
void emberCounterHandler (EmberCounterType type, EmberCounterInfo info)
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type | Type of the event. |
| EmberCounterInfo | N/A | info | could map to:
|
The application must define ::EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
emberCounterRequiresPhyIndex#
bool emberCounterRequiresPhyIndex (EmberCounterType type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type |
emberCounterRequiresDestinationNodeId#
bool emberCounterRequiresDestinationNodeId (EmberCounterType type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type |
emberStackTokenChangedHandler#
void emberStackTokenChangedHandler (uint16_t tokenAddress)
A callback invoked to inform the application that a stack token has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | tokenAddress | The address of the stack token that has changed. |
emberRtosIdleHandler#
bool emberRtosIdleHandler (uint32_t * idleTimeMs)
A callback to allow the application to manage idling the MCU.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | N/A | idleTimeMs | The time in millisecond the stack is allowed to idle. |
Returns
True if the application is managing idling the MCU, false otherwise. If this function returns false, the stack will manage idling the MCU.
emberRtosStackWakeupIsrHandler#
void emberRtosStackWakeupIsrHandler (void )
A callback to request the application to wake up the stack task.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberGetNeighbor#
EmberStatus emberGetNeighbor (uint8_t index, EmberNeighborTableEntry * result)
Copies a neighbor table entry to the structure that result points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using emberNeighborCount().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of a neighbor table entry. |
| EmberNeighborTableEntry * | N/A | result | A pointer to the location to which to copy the neighbor table entry. |
Returns
EMBER_ERR_FATAL if the index is greater or equal to the number of active neighbors, or if the device is an end device. Returns EMBER_SUCCESS otherwise.
emberSetRoutingShortcutThreshold#
EmberStatus emberSetRoutingShortcutThreshold (uint8_t costThresh)
Sets the routing shortcut threshold to directly use a neighbor instead of performing routing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | costThresh | the routing shortcut value that should be used to directly use a neighbor instead of performing routing. |
Returns
::return EMBER_BAD_ARGUMENT if the costThresh is not 1, 3, 5, 7 Returns EMBER_SUCCESS otherwise.
emberGetRoutingShortcutThreshold#
uint8_t emberGetRoutingShortcutThreshold (void )
Gets the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
the routingShortcutThresh which takes one of the following values: 1, 3, 5, or 7.
emberSetInitialNeighborOutgoingCost#
EmberStatus emberSetInitialNeighborOutgoingCost (uint8_t cost)
Sets neighbor's initial outgoing link cost.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | cost | The new default cost. |
Returns
EMBER_BAD_ARGUMENT if the cost is not any of 0, 1, 3, 5, or 7. Returns EMBER_SUCCESS otherwise NOTE: There is no EZSP version of this function yet.
emberGetInitialNeighborOutgoingCost#
uint8_t emberGetInitialNeighborOutgoingCost (void )
Gets neighbor's initial outgoing link cost.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The default cost associated with new neighbor's outgoing links. NOTE: There is no EZSP version of this function yet.
emberResetRejoiningNeighborsFC#
void emberResetRejoiningNeighborsFC (bool reset)
Indicates whether a rejoining neighbor's incoming FC should be reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | reset | True or False. |
Returns
::void NOTE: There is no EZSP version of this function yet.
emberIsResetRejoiningNeighborsFCEnabled#
bool emberIsResetRejoiningNeighborsFCEnabled (void )
Checks if resetting the incoming FC for a rejoining neighbor is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
::True or False. NOTE: There is no EZSP version of this function yet.
emberGetNeighborFrameCounter#
EmberStatus emberGetNeighborFrameCounter (EmberEUI64 nodeEui64, uint32_t * returnFrameCounter)
This function gets the last received frame counter as found in the Network Auxiliary header for the specified neighbor or child.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | nodeEui64 | The neighbor or child EUI to search. |
| uint32_t * | N/A | returnFrameCounter | The frame counter variable to fill in. |
Returns
EmberStatus depending on whether the frame counter is found in the neighbor or child table.
emberGetRouteTableEntry#
EmberStatus emberGetRouteTableEntry (uint8_t index, EmberRouteTableEntry * result)
Copies a route table entry to the structure that the result points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via emberRouteTableSize().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of a route table entry. |
| EmberRouteTableEntry * | N/A | result | A pointer to the location to which to copy the route table entry. |
Returns
EMBER_ERR_FATAL if the index is out of range or the device is an end device, and EMBER_SUCCESS otherwise.
emberStackProfile#
uint8_t emberStackProfile (void )
Returns the stack profile of the network which the node has joined.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The stack profile.
emberSecurityLevel#
uint8_t emberSecurityLevel (void )
Returns the security level of the network which the node has joined.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The security level.
emberTreeDepth#
uint8_t emberTreeDepth (void )
Returns the depth of the node in the network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current depth.
emberNeighborCount#
uint8_t emberNeighborCount (void )
Returns the number of active entries in the neighbor table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The number of active entries in the neighbor table.
emberRouteTableSize#
uint8_t emberRouteTableSize (void )
Returns the size of the route table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The size of the route table.
emberNextZigbeeSequenceNumber#
uint8_t emberNextZigbeeSequenceNumber (void )
Increments and returns the Zigbee sequence number.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The next Zigbee sequence number.
emberGetMaxNwkRetries#
uint8_t emberGetMaxNwkRetries (void )
Get max number of NWK retries.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns the maximum number of NWK retries that will be attempted
Returns
uint8_t Max NWK retries