The master include file for the EmberZNet API.
See EmberZNet Stack API Reference for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_EMBER_H
#define SILABS_EMBER_H
#if (!defined(EZSP_HOST) && !defined(EMBER_TEST))
#include "em_device.h"  // To get _SILICON_LABS macros
#endif  // !EZSP_HOST && !EMBER_TEST
#ifndef EMBER_TEST
#define EVENT_NAME(x) ""
#else
#define EVENT_NAME(x) x
#endif
// We define EMBER_MULTI_NETWORK_STRIPPED before including header files
// so that the EMBER_MULTI_NETWORK_STRIPPED can be well aware.
#if defined(SMART_ENERGY_STACK_TOKENS) && !defined(EMBER_MULTI_NETWORK_STRIPPED)
#define EMBER_MULTI_NETWORK_STRIPPED
#endif
// EMBER_MULTI_NETWORK_STRIPPED is an optional #define
// that is used to conditionally compile out multi-network
// related source code. The following flash-space constrained chips
// have EMBER_MULTI_NETWORK_STRIPPED by default.
#ifndef EMBER_MULTI_NETWORK_STRIPPED
#if defined(CORTEXM3_EM351) || defined(CORTEXM3_EM357) || defined(_SILICON_LABS_32B_SERIES_1_CONFIG_1) || defined(_SILICON_LABS_32B_SERIES_1_CONFIG_4)
#ifndef EMBER_MULTI_NETWORK_REENABLE
#define EMBER_MULTI_NETWORK_STRIPPED
#endif
#endif
#endif // EMBER_MULTI_NETWORK_STRIPPED
#include "ember-types.h"
#include "byte-utilities.h"
#include "stack-info.h"
#include "network-formation.h"
#include "buffer_manager/buffer-management.h"
#include "buffer_manager/buffer-queue.h"
#include "buffer_manager/legacy-packet-buffer.h"
#include "message.h"
#include "child.h"
#include "security.h"
#include "aes-mmo.h"
#include "binding-table.h"
#include "bootload.h"
#include "zigbee-device-stack.h"
#ifndef UC_BUILD
#include "event_control/event.h"
#endif
#include "event_queue/event-queue.h"
#include "ember-debug.h"
#include "library.h"
#include "zll-api.h"
#include "multi-phy.h"
#include "ember-duty-cycle.h"
#include "mac-layer.h"
#include "ember-random-api.h"
#include "ember-alternate-mac.h"
#include "raw-message.h"
#include "multi-network.h"
#ifndef DOXYGEN_SHOULD_SKIP_THIS
#define RADIO_BANDS_SUPPORTED_868   BIT(0)
#define RADIO_BANDS_SUPPORTED_915   BIT(1)
#define RADIO_BANDS_SUPPORTED_433   BIT(2)
#endif // DOXYGEN_SHOULD_SKIP_THIS
#define RADIO_BANDS_SUPPORTED_2400  BIT(3)
#ifndef DOXYGEN_SHOULD_SKIP_THIS
#define RADIO_BANDS_SUPPORTED_408   BIT(4)
#endif // DOXYGEN_SHOULD_SKIP_THIS
#ifndef DOXYGEN_SHOULD_SKIP_THIS
#include "config/config.h"
#ifdef DEBUG_ASSERT
extern bool enableFailure;
extern uint8_t rateOfFailure;
extern uint8_t failuresInARow;
static uint8_t bufferFailure;
bool generateFailure(void);
void dumpFailure(void);
#endif
#endif //DOXYGEN_SHOULD_SKIP_THIS
#endif // SILABS_EMBER_H
PHY Information#
Bit masks for TOKEN_MFG_RADIO_BANDS_SUPPORTED.
#define
RADIO_BANDS_SUPPORTED_2400 BIT(3)
2.4 GHz band
Macros#
#define
EVENT_NAME (x)