Fragmented message support for EZSP Hosts. Splits long messages into smaller blocks for transmission and reassembles received blocks. See Message Fragmentation for documentation.
DeprecatedThe fragment library is deprecated and will be removed in a future release. Similar functionality is available in the Fragmentation plugin in Application Framework.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
void ezspFragmentInit(uint16_t receiveBufferLength, uint8_t *receiveBuffer);
EmberStatus ezspFragmentSendUnicast(EmberOutgoingMessageType type,
                                    uint16_t indexOrDestination,
                                    EmberApsFrame *apsFrame,
                                    uint8_t maxFragmentSize,
                                    uint16_t messageLength,
                                    uint8_t *messageContents);
EmberStatus ezspFragmentSourceRouteHandler(void);
bool ezspFragmentMessageSent(EmberApsFrame *apsFrame, EmberStatus status);
void ezspFragmentMessageSentHandler(EmberStatus status);
bool ezspFragmentIncomingMessage(EmberApsFrame *apsFrame,
                                 EmberNodeId sender,
                                 uint16_t *messageLength,
                                 uint8_t **messageContents);
void ezspFragmentTick(void);
Initialization#
Initialize variables and buffers used for sending and receiving long messages. This functions reads the values of ::EZSP_CONFIG_MAX_HOPS and ::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE. The application must set these values before calling this function.
Transmitting#
Send a long message by splitting it into blocks. Only one long message can be sent at a time. Calling this function a second time aborts the first message.
DEPRECATED A callback invoked just before each block of the current long message is sent. Previously, if the message had to be source routed, the application needed this callback and call ezspSetSourceRoute() in it. Since Zigbee 6.7 has removed the host side source route table, this callback deems to be unnecessary, and will be deprecated later.
The application must call this function at the start of its ezspMessageSentHandler(). If it returns true, the fragmentation code has handled the event and the application must not process it further.
The fragmentation code calls this application-defined handler when it finishes sending a long message.
Receiving#
The application must call this function at the start of its ezspIncomingMessageHandler(). If it returns true, the fragmentation code has handled the message and the application must not process it further. When the final block of a long message is received, this function replaces the message with the reassembled long message and returns false so that the application processes it.
Used by the fragmentation code to time incoming blocks. The application must call this function regularly.
Initialization Documentation#
ezspFragmentInit#
void ezspFragmentInit (uint16_t receiveBufferLength, uint8_t * receiveBuffer)
Initialize variables and buffers used for sending and receiving long messages. This functions reads the values of ::EZSP_CONFIG_MAX_HOPS and ::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE. The application must set these values before calling this function.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | N/A | receiveBufferLength | The length of receiveBuffer. Incoming messages longer than this will be dropped. | 
| uint8_t * | N/A | receiveBuffer | The buffer used to reassemble incoming long messages. Once the message is complete, this buffer will be passed back to the application by ezspFragmentIncomingMessage(). | 
Transmitting Documentation#
ezspFragmentSendUnicast#
EmberStatus ezspFragmentSendUnicast (EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame * apsFrame, uint8_t maxFragmentSize, uint16_t messageLength, uint8_t * messageContents)
Send a long message by splitting it into blocks. Only one long message can be sent at a time. Calling this function a second time aborts the first message.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberOutgoingMessageType | N/A | type | Specifies the outgoing message type. Must be one of EMBER_OUTGOING_DIRECT, EMBER_OUTGOING_VIA_ADDRESS_TABLE, or EMBER_OUTGOING_VIA_BINDING. | 
| uint16_t | N/A | indexOrDestination | Depending on the type of addressing used, this is either the EmberNodeId of the destination, an index into the address table, or an index into the binding table. | 
| EmberApsFrame * | N/A | apsFrame | The APS frame for the message. | 
| uint8_t | N/A | maxFragmentSize | The message will be broken into blocks no larger than this. | 
| uint16_t | N/A | messageLength | The length of the messageContents parameter in bytes. | 
| uint8_t * | N/A | messageContents | The long message to be sent. | 
Returns
- An EmberStatus value. - EMBER_INVALID_CALL is returned if messageLength is zero or if the window size (::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE) is zero. 
 
ezspFragmentSourceRouteHandler#
EmberStatus ezspFragmentSourceRouteHandler (void )
DEPRECATED A callback invoked just before each block of the current long message is sent. Previously, if the message had to be source routed, the application needed this callback and call ezspSetSourceRoute() in it. Since Zigbee 6.7 has removed the host side source route table, this callback deems to be unnecessary, and will be deprecated later.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
The application must define EZSP_APPLICATION_HAS_FRAGMENT_SOURCE_ROUTE_HANDLER in its configuration header if it defines this callback.
Returns
- EMBER_SUCCESS if the source route has been set. Any other value will abort transmission of the current long message. 
ezspFragmentMessageSent#
bool ezspFragmentMessageSent (EmberApsFrame * apsFrame, EmberStatus status)
The application must call this function at the start of its ezspMessageSentHandler(). If it returns true, the fragmentation code has handled the event and the application must not process it further.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberApsFrame * | N/A | apsFrame | The APS frame passed to ezspMessageSentHandler(). | 
| EmberStatus | N/A | status | The status passed to ezspMessageSentHandler(). | 
Returns
- true if the sent message was a block of a long message. The fragmentation code has handled the event so the application must return immediately from its ezspMessageSentHandler(). Returns false otherwise. The fragmentation code has not handled the event so the application must continue to process it. 
ezspFragmentMessageSentHandler#
void ezspFragmentMessageSentHandler (EmberStatus status)
The fragmentation code calls this application-defined handler when it finishes sending a long message.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberStatus | N/A | status | EMBER_SUCCESS if all the blocks of the long message were delivered to the destination, otherwise EMBER_DELIVERY_FAILED, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY. | 
Receiving Documentation#
ezspFragmentIncomingMessage#
bool ezspFragmentIncomingMessage (EmberApsFrame * apsFrame, EmberNodeId sender, uint16_t * messageLength, uint8_t ** messageContents)
The application must call this function at the start of its ezspIncomingMessageHandler(). If it returns true, the fragmentation code has handled the message and the application must not process it further. When the final block of a long message is received, this function replaces the message with the reassembled long message and returns false so that the application processes it.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberApsFrame * | N/A | apsFrame | The APS frame passed to ezspIncomingMessageHandler(). | 
| EmberNodeId | N/A | sender | The sender passed to ezspIncomingMessageHandler(). | 
| uint16_t * | N/A | messageLength | A pointer to the message length passed to ezspIncomingMessageHandler(). | 
| uint8_t ** | N/A | messageContents | A pointer to the message contents passed to ezspIncomingMessageHandler(). | 
Returns
- true if the incoming message was a block of an incomplete long message. The fragmentation code has handled the message so the application must return immediately from its ezspIncomingMessageHandler(). Returns false if the incoming message was not part of a long message. The fragmentation code has not handled the message so the application must continue to process it. Returns false if the incoming message was a block that completed a long message. The fragmentation code replaces the message with the reassembled long message so the application must continue to process it. 
ezspFragmentTick#
void ezspFragmentTick (void )
Used by the fragmentation code to time incoming blocks. The application must call this function regularly.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A |