Defines for the Zigbee Event Logger component, which describes various events that can be recorded and retrieved for user inspection.
License#
Copyright 2021 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
//
// *** Generated file. Do not edit! ***
// Generated by: generate-zigbee-logger-files.py -y zigbee_logger.yaml
#ifndef _ZIGBEE_EVENT_LOGGER_GEN_H_
#define ZIGBEE_EVENT_LOGGER_VERSION 1
#define LOGGER_AREA_BIT_SHIFT 12
#define EMBER_ZIGBEE_LOGGER_AREA (0 << LOGGER_AREA_BIT_SHIFT)
typedef enum {
  EMBER_LOGGER_ZIGBEE_BOOT_EVENT_ID = 0,
  EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_ID = 1,
  EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_ID = 2,
  EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_ID = 3,
  EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_ID = 4,
  EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_ID = 5,
  EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_ID = 6,
  EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_ID = 7,
  EMBER_LOGGER_ZIGBEE_RESET_ID = 8,
  EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_ID = 9,
  EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_ID = 10,
  EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_ID = 11,
  EMBER_LOGGER_ZIGBEE_CHILD_ADDED_ID = 12,
  EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_ID = 13,
  EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_ID = 14,
  EMBER_LOGGER_ZIGBEE_STACK_STATUS_ID = 15,
  EMBER_LOGGER_ZIGBEE_TIME_SYNC_ID = 16,
  EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_ID = 17,
  // Last value. All event IDs should be less than this
  EMBER_LOGGER_ZIGBEE_NULL_ID = 0xFFFF,
} EmberZigbeeLoggerEventTypes;
typedef enum {
  EMBER_LOGGER_ZIGBEE_FACILITY_BASE = 0,
  EMBER_LOGGER_ZIGBEE_FACILITY_MAC = 1,
  EMBER_LOGGER_ZIGBEE_FACILITY_NETWORK = 2,
  EMBER_LOGGER_ZIGBEE_FACILITY_APS = 3,
  EMBER_LOGGER_ZIGBEE_FACILITY_SECURITY = 4,
  EMBER_LOGGER_ZIGBEE_FACILITY_ZDO = 5,
  EMBER_LOGGER_ZIGBEE_FACILITY_ZCL = 6,
  EMBER_LOGGER_ZIGBEE_FACILITY_BDB = 7,
  EMBER_LOGGER_ZIGBEE_FACILITY_SMART_ENERGY = 8,
} EmberZigbeeLoggerFacilityTypes;
#define EMBER_LOGGER_ZIGBEE_BOOT_EVENT_LENGTH 6
#define EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_LENGTH 12
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_LENGTH 5
#define EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_LENGTH 5
#define EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_LENGTH 3
#define EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_LENGTH 3
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_LENGTH 0
#define EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_LENGTH 1
#define EMBER_LOGGER_ZIGBEE_RESET_LENGTH 2
#define EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_LENGTH 2
#define EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_LENGTH 10
#define EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_LENGTH 7
#define EMBER_LOGGER_ZIGBEE_CHILD_ADDED_LENGTH 10
#define EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_LENGTH 10
#define EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_LENGTH 10
#define EMBER_LOGGER_ZIGBEE_STACK_STATUS_LENGTH 1
#define EMBER_LOGGER_ZIGBEE_TIME_SYNC_LENGTH 8
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_LENGTH 3
void emberAfPluginZigBeeEventLoggerAddBootEvent(uint32_t bootCount, uint16_t resetType)
;
void emberAfPluginZigBeeEventLoggerAddJoinNetwork(EmberPanId panId, uint8_t channelNumber, uint8_t page, uint8_t *extendedPanId)
;
void emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin(uint32_t channelMask, EmberRejoinReason reason)
;
void emberAfPluginZigBeeEventLoggerAddSecureRejoin(uint32_t channelMask, EmberRejoinReason reason)
;
void emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin(EmberNodeId sourceNode, EmberLeaveReason reason)
;
void emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin(EmberNodeId sourceNode, EmberLeaveReason reason)
;
void emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange(void)
;
void emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange(uint8_t sequence)
;
void emberAfPluginZigBeeEventLoggerAddReset(uint8_t resetCode, uint8_t extendedReason)
;
void emberAfPluginZigBeeEventLoggerAddChannelChange(uint8_t page, uint8_t channel)
;
void emberAfPluginZigBeeEventLoggerAddParentChange(EmberNodeId parentNodeId, EmberEUI64 parentEui64)
;
void emberAfPluginZigBeeEventLoggerAddDutyCycleChange(EmberDutyCycleState state, EmberDutyCycleHectoPct limitThreshold, EmberDutyCycleHectoPct criticalThreshold, EmberDutyCycleHectoPct suspendedLimit)
;
void emberAfPluginZigBeeEventLoggerAddChildAdded(EmberNodeId childNodeId, EmberEUI64 childEui64)
;
void emberAfPluginZigBeeEventLoggerAddChildRemoved(EmberNodeId childNodeId, EmberEUI64 childEui64)
;
void emberAfPluginZigBeeEventLoggerAddChildTimedOut(EmberNodeId childNodeId, EmberEUI64 childEui64)
;
void emberAfPluginZigBeeEventLoggerAddStackStatus(EmberStatus status)
;
void emberAfPluginZigBeeEventLoggerAddTimeSync(uint32_t utcTime, uint32_t secondsSinceBoot)
;
void emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision(EmberNodeId nodeId, uint8_t decision)
;
#endif  // #ifndef _ZIGBEE_EVENT_LOGGER_GEN_H_
Macros#
The version of this feature.
The length of the Boot Event event data.
The length of the Join Network event data.
The length of the Trust Center Rejoin event data.
The length of the Secure Rejoin event data.
The length of the Leave Without Rejoin event data.
The length of the Leave With Rejoin event data.
The length of the Trust Center Link Key Change event data.
The length of the Network Key Sequence Number Change event data.
The length of the Reset event data.
The length of the Channel Change event data.
The length of the Parent Change event data.
The length of the Duty Cycle Change event data.
The length of the Child Added event data.
The length of the Child Removed event data.
The length of the Child Timed Out event data.
The length of the Stack Status event data.
The length of the Time Sync event data.
The length of the Trust Center Join Decision event data.
Enumerations#
A list of identifiers for system events.
A list of facilities for system events, identifying which layer they occurred in.
Functions#
Records an event indicating that the device has booted.
Records an event indicating that a network was successfully joined.
Records an event indicating that a trust center rejoin was attempted.
Records an event indicating that a secure rejoin was attempted.
Records an event indicating that a device has left-without-rejoin.
Records an event indicating that a device has left-with-rejoin.
Records an event indicating that an attempt was made to update the trust center link key.
Records an event indicating that the network key sequence number has changed.
Records an event indicating that the local device has reset.
Records an event indicating that the network's channel has changed.
Records an event indicating that the local device's parent has changed.
Records an event indicating that the duty cycle has changed.
Records an event indicating that a child device has joined the local device.
Records an event indicating that a child device has been removed from the local device.
Records an event indicating that a child device has been timed out by the local device.
Records an event indicating that the stack status has changed.
Records an event indicating that the clock time has been synchronized.
Records an event indicating that a device has attempted to join or rejoin the network.
Enumeration Documentation#
EmberZigbeeLoggerEventTypes#
EmberZigbeeLoggerEventTypes
A list of identifiers for system events.
| Enumerator | |
|---|---|
| EMBER_LOGGER_ZIGBEE_BOOT_EVENT_ID | |
| EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_RESET_ID | |
| EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_ADDED_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_ID | |
| EMBER_LOGGER_ZIGBEE_STACK_STATUS_ID | |
| EMBER_LOGGER_ZIGBEE_TIME_SYNC_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_ID | |
| EMBER_LOGGER_ZIGBEE_NULL_ID | |
EmberZigbeeLoggerFacilityTypes#
EmberZigbeeLoggerFacilityTypes
A list of facilities for system events, identifying which layer they occurred in.
| Enumerator | |
|---|---|
| EMBER_LOGGER_ZIGBEE_FACILITY_BASE | |
| EMBER_LOGGER_ZIGBEE_FACILITY_MAC | |
| EMBER_LOGGER_ZIGBEE_FACILITY_NETWORK | |
| EMBER_LOGGER_ZIGBEE_FACILITY_APS | |
| EMBER_LOGGER_ZIGBEE_FACILITY_SECURITY | |
| EMBER_LOGGER_ZIGBEE_FACILITY_ZDO | |
| EMBER_LOGGER_ZIGBEE_FACILITY_ZCL | |
| EMBER_LOGGER_ZIGBEE_FACILITY_BDB | |
| EMBER_LOGGER_ZIGBEE_FACILITY_SMART_ENERGY | |
Function Documentation#
emberAfPluginZigBeeEventLoggerAddBootEvent#
void emberAfPluginZigBeeEventLoggerAddBootEvent (uint32_t bootCount, uint16_t resetType)
Records an event indicating that the device has booted.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | bootCount | The number of times the device has booted. | 
| uint16_t | N/A | resetType | A reset cause. See micro.h and reset-def.h. | 
Note
- This API only works on SoC. It does not work on host or NCP. 
emberAfPluginZigBeeEventLoggerAddJoinNetwork#
void emberAfPluginZigBeeEventLoggerAddJoinNetwork (EmberPanId panId, uint8_t channelNumber, uint8_t page, uint8_t * extendedPanId)
Records an event indicating that a network was successfully joined.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberPanId | N/A | panId | The PAN ID of the network. | 
| uint8_t | N/A | channelNumber | The channel of the network. | 
| uint8_t | N/A | page | The page of the network joined. | 
| uint8_t * | N/A | extendedPanId | The extended PAN ID of the network. | 
emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin#
void emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin (uint32_t channelMask, EmberRejoinReason reason)
Records an event indicating that a trust center rejoin was attempted.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | channelMask | The channel mask used when searching for the network. | 
| EmberRejoinReason | N/A | reason | An EmberRejoinReason enumeration, indicating why the rejoin was initiated. | 
Note
- This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success. 
emberAfPluginZigBeeEventLoggerAddSecureRejoin#
void emberAfPluginZigBeeEventLoggerAddSecureRejoin (uint32_t channelMask, EmberRejoinReason reason)
Records an event indicating that a secure rejoin was attempted.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | channelMask | The channel mask used when searching for the network. | 
| EmberRejoinReason | N/A | reason | An EmberRejoinReason enumeration, indicating why the rejoin was initiated. | 
Note
- This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success. 
emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin#
void emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)
Records an event indicating that a device has left-without-rejoin.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | sourceNode | The node ID of the device leaving. | 
| EmberLeaveReason | N/A | reason | An EmberLeaveReason enumeration, indicating why the device left. | 
emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin#
void emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)
Records an event indicating that a device has left-with-rejoin.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | sourceNode | The node ID of the device leaving-and-rejoining. | 
| EmberLeaveReason | N/A | reason | An EmberLeaveReason enumeration, indicating why the device left. | 
emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange#
void emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange (void )
Records an event indicating that an attempt was made to update the trust center link key.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange#
void emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange (uint8_t sequence)
Records an event indicating that the network key sequence number has changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | sequence | The new network key sequence number. | 
emberAfPluginZigBeeEventLoggerAddReset#
void emberAfPluginZigBeeEventLoggerAddReset (uint8_t resetCode, uint8_t extendedReason)
Records an event indicating that the local device has reset.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | resetCode | The reset code. See reset-def.h. | 
| uint8_t | N/A | extendedReason | The extended reset reason. See reset-def.h. | 
emberAfPluginZigBeeEventLoggerAddChannelChange#
void emberAfPluginZigBeeEventLoggerAddChannelChange (uint8_t page, uint8_t channel)
Records an event indicating that the network's channel has changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | page | The new page number. | 
| uint8_t | N/A | channel | The new channel number. | 
emberAfPluginZigBeeEventLoggerAddParentChange#
void emberAfPluginZigBeeEventLoggerAddParentChange (EmberNodeId parentNodeId, EmberEUI64 parentEui64)
Records an event indicating that the local device's parent has changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | parentNodeId | The new parent's short address. | 
| EmberEUI64 | N/A | parentEui64 | The new parent's long address. | 
emberAfPluginZigBeeEventLoggerAddDutyCycleChange#
void emberAfPluginZigBeeEventLoggerAddDutyCycleChange (EmberDutyCycleState state, EmberDutyCycleHectoPct limitThreshold, EmberDutyCycleHectoPct criticalThreshold, EmberDutyCycleHectoPct suspendedLimit)
Records an event indicating that the duty cycle has changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberDutyCycleState | N/A | state | An EmberDutyCycleState state. | 
| EmberDutyCycleHectoPct | N/A | limitThreshold | An EmberDutyCycleHectoPct limit. | 
| EmberDutyCycleHectoPct | N/A | criticalThreshold | An EmberDutyCycleHectoPct critical threshold. | 
| EmberDutyCycleHectoPct | N/A | suspendedLimit | An EmberDutyCycleHectoPct suspend limit. | 
emberAfPluginZigBeeEventLoggerAddChildAdded#
void emberAfPluginZigBeeEventLoggerAddChildAdded (EmberNodeId childNodeId, EmberEUI64 childEui64)
Records an event indicating that a child device has joined the local device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. | 
| EmberEUI64 | N/A | childEui64 | The child's long address. | 
emberAfPluginZigBeeEventLoggerAddChildRemoved#
void emberAfPluginZigBeeEventLoggerAddChildRemoved (EmberNodeId childNodeId, EmberEUI64 childEui64)
Records an event indicating that a child device has been removed from the local device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. | 
| EmberEUI64 | N/A | childEui64 | The child's long address. | 
emberAfPluginZigBeeEventLoggerAddChildTimedOut#
void emberAfPluginZigBeeEventLoggerAddChildTimedOut (EmberNodeId childNodeId, EmberEUI64 childEui64)
Records an event indicating that a child device has been timed out by the local device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. | 
| EmberEUI64 | N/A | childEui64 | The child's long address. | 
emberAfPluginZigBeeEventLoggerAddStackStatus#
void emberAfPluginZigBeeEventLoggerAddStackStatus (EmberStatus status)
Records an event indicating that the stack status has changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberStatus | N/A | status | An EmberStatus value indicating the change. | 
emberAfPluginZigBeeEventLoggerAddTimeSync#
void emberAfPluginZigBeeEventLoggerAddTimeSync (uint32_t utcTime, uint32_t secondsSinceBoot)
Records an event indicating that the clock time has been synchronized.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | utcTime | The updated UTC time. | 
| uint32_t | N/A | secondsSinceBoot | The number of seconds that have elapsed since boot. | 
emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision#
void emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision (EmberNodeId nodeId, uint8_t decision)
Records an event indicating that a device has attempted to join or rejoin the network.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EmberNodeId | N/A | nodeId | The short address of the device attempting to join or rejoin. | 
| uint8_t | N/A | decision | The join or rejoin decision taken by the local device. | 
Note
- This event is only recorded on a trust center device.