See Debugging Utilities for documentation.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef SILABS_EMBER_DEBUG_H
#define SILABS_EMBER_DEBUG_H

#ifndef UC_BUILD
// Define the values for DEBUG_LEVEL
#define NO_DEBUG    0
#define BASIC_DEBUG 1
#define FULL_DEBUG  2
#endif // UC_BUILD

#define emberDebugInit(port) do {} while (false)

#if (DEBUG_LEVEL >= BASIC_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS) || defined(UC_BUILD)

#define DEBUG_ROUTINES_PRESENT

void emberDebugAssert(const char * filename, int linenumber);

void emberDebugMemoryDump(uint8_t *start, uint8_t *end);

void emberDebugBinaryPrintf(const char * formatString, ...);

void emDebugSendVuartMessage(uint8_t *buff, uint8_t len);

//#if (DEBUG_LEVEL == FULL_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS)
void emberDebugError(EmberStatus code);

bool emberDebugReportOff(void);

void emberDebugReportRestore(bool state);

// Format: Same as emberSerialPrintf
// emberDebugPrintf("format string"[, parameters ...])
void emberDebugPrintf(const char * formatString, ...);

#else // (DEBUG_LEVEL >= BASIC_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS) || defined(UC_BUILD)
  #define emberDebugAssert(filename, linenumber) do {} while (false)
  #define emberDebugMemoryDump(start, end) do {} while (false)
  #define emberDebugBinaryPrintf(formatstring, ...) do {} while (false)
  #define emDebugSendVuartMessage(buff, len) do {} while (false)
  #define emberDebugError(code) do {} while (false)
// Note the following doesn't have a do{}while(false)
//   because it has a return value
  #define emberDebugReportOff() (false)
  #define emberDebugReportRestore(state) do {} while (false)
  #define emberDebugPrintf(...) do {} while (false)
#endif // (DEBUG_LEVEL >= BASIC_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS) || defined(UC_BUILD)

#endif // SILABS_EMBER_DEBUG_H

Macros#

#define

This function is obsolete and no longer required to initialize the debug system.

Functions#

void
emberDebugAssert(const char *filename, int linenumber)

Print the filename and line number to the debug serial port.

void
emberDebugMemoryDump(uint8_t *start, uint8_t *end)

Print the contents of RAM to the debug serial port.

void
emberDebugBinaryPrintf(const char *formatString,...)

Print binary data to the debug channel.

void
emDebugSendVuartMessage(uint8_t *buff, uint8_t len)

Send VUART data out the debug channel.

void
emberDebugError(EmberStatus code)

Print an EmberStatus return code to the serial port.

bool

Turn off all debug output.

void

Restore the state of the debug output.

void
emberDebugPrintf(const char *formatString,...)

Prints text debug messages.

Macro Definition Documentation#

emberDebugInit#

#define emberDebugInit
Value:
(port)

This function is obsolete and no longer required to initialize the debug system.


DEBUG_ROUTINES_PRESENT#

#define DEBUG_ROUTINES_PRESENT

Function Documentation#

emberDebugAssert#

void emberDebugAssert (const char * filename, int linenumber)

Print the filename and line number to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
const char *N/Afilename

The name of the file where the assert occurred.

intN/Alinenumber

The line number in the file where the assert occurred.


emberDebugMemoryDump#

void emberDebugMemoryDump (uint8_t * start, uint8_t * end)

Print the contents of RAM to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Astart

The start address of the block of RAM to dump.

uint8_t *N/Aend

The end address of the block of RAM to dump (address of the last byte).


emberDebugBinaryPrintf#

void emberDebugBinaryPrintf (const char * formatString, ... )

Print binary data to the debug channel.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

A string of conversion specification characters describing the arguments to be printed.

...N/A

The arguments to be printed.

This function does not use the normal printf format conventions. To print text debug messages, use emberDebugPrintf(). The format string must contain only these conversion specification characters:

  • B - uint8_t value.

  • W - uint16_t value, printed least significant byte first.

  • D - uint32_t value, printed least significant byte first.

  • F - pointer to null terminated string in Flash (const char *).

  • xxxp - pointer to RAM, length is xxx (max 255).

  • lp - pointer to RAM, length is uint8_t argument.

  • xxxf - pointer to Flash (const char *), length is xxx (max 255).

  • lf - pointer to Flash (const char *), length is uint8_t argument.

  • b - EmberMessageBuffer.

Examples:

emberDebugBinaryPrintf("BWD", status, panId, channelMask);
emberDebugBinaryPrintf("F8p", "string example", eui64);
emberDebugBinaryPrintf("lp64fb", length, bytes, dataTable, buffer);

emDebugSendVuartMessage#

void emDebugSendVuartMessage (uint8_t * buff, uint8_t len)

Send VUART data out the debug channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Abuff

A pointer to the data to send.

uint8_tN/Alen

The length of the data to send.


emberDebugError#

void emberDebugError (EmberStatus code)

Print an EmberStatus return code to the serial port.

Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Acode

The EmberStatus code to print.


emberDebugReportOff#

bool emberDebugReportOff (void )

Turn off all debug output.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The current state (true for on, false for off).


emberDebugReportRestore#

void emberDebugReportRestore (bool state)

Restore the state of the debug output.

Parameters
TypeDirectionArgument NameDescription
boolN/Astate

The state returned from emberDebugReportOff(). This is done so that debug output is not blindly turned on.


emberDebugPrintf#

void emberDebugPrintf (const char * formatString, ... )

Prints text debug messages.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

Takes the following:

...N/A

%%

Percent sign

%c

Single-byte char

%s

RAM string

%p

Flash string (does not follow the printf standard)

%u

Two-byte unsigned decimal

%d

Two-byte signed decimal

%x, %%2x, %%4x

1-, 2-, 4-byte hex value (always 0 padded; does not follow the printf standard)