Modules#

emberClusterFunctionStructure

EmberAfDefaultAttributeValue

EmberAfAttributeMinMaxValue

EmberAfDefaultOrMinMaxAttributeValue

EmberAfAttributeMetadata

EmberAfCluster

EmberAfAttributeSearchRecord

EmberAfManufacturerCodeEntry

EmberAfIncomingMessage

EmberAfInterpanHeader

EmberAfAllowedInterPanMessage

EmberAfClusterCommand

EmberAfEndpointType

EmberAfSecurityProfileData

EmberAfDefinedEndpoint

EmberAfLoadControlEvent

EmberAfServiceDiscoveryResult

EmberAfEndpointList

EmberAfClusterList

EmberAfEventContext

sl_zigbee_event_context_t

EmberAfGroupTableEntry

EmberAfSceneTableEntry

EmberAfPluginMessagingClientMessage

EmberAfPluginPriceClientPrice

EmberAfPluginReportingEntry

EmberAfPluginZllCommissioningGroupInformationRecord

EmberAfPluginZllCommissioningEndpointInformationRecord

EmberAfOtaImageId

EmberAfImageBlockRequestCallbackStruct

EmberAfOtaHeader

EmberAfTagData

EmberAfMessageStruct

EmberAfLinkKeyBackupData

EmberAfTrustCenterBackupData

EmberAfStandaloneBootloaderQueryResponseData

EmberAfCommandMetadata

EmberAfTimeStruct

EmberAfDate

EmberAfDeviceManagementTenancy

EmberAfDeviceManagementSupplier

EmberAfDeviceManagementSupply

EmberAfDeviceManagementSiteId

EmberAfDeviceManagementCIN

EmberAfDeviceManagementSupplyStatusFlags

EmberAfDeviceManagementUncontrolledFlowThreshold

EmberAfDeviceManagementSupplyStatus

EmberAfDeviceManagementPassword

EmberAfDeviceManagementInfo

EmberAfDeviceManagementAttributeRange

EmberAfDeviceManagementAttributeTable

EmberAfGbzMessageData

EmberAfGpfMessage

EmberAfRemoteClusterStruct

EmberAfRemoteBindingStruct

EmberAfClusterInfo

EmberAfEndpointInfoStruct

EmberAfDeviceInfo

EmberAfDeviceDatabaseIterator

EmberAfJoiningDevice

The include file for all the types for Ember ApplicationFramework.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef SILABS_AF_API_TYPES
#define SILABS_AF_API_TYPES

#ifdef UC_BUILD
#include "sl_component_catalog.h"
#include "zap-type.h"
#include "zigbee_app_framework_common.h"
#ifdef SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT
#include "messaging-client-config.h"
#endif  // SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT
#else
#include "enums.h"
#endif

#ifdef EZSP_HOST
#include "app/util/ezsp/ezsp-enum.h"
#endif

typedef uint16_t EmberAfProfileId;

typedef uint16_t EmberAfAttributeId;

typedef uint16_t EmberAfClusterId;

typedef uint8_t EmberAfAttributeType;

typedef uint8_t EmberAfClusterMask;

typedef uint8_t EmberAfAttributeMask;

typedef void (*EmberAfGenericClusterFunction)(void);

typedef struct {
  EmberAfClusterId                    clusterId;
  EmberAfClusterMask                  functionMask;
  const EmberAfGenericClusterFunction functionPtr;
} emberClusterFunctionStructure;

#define EMBER_AF_NULL_MANUFACTURER_CODE 0x0000u

 #define EMBER_AF_INVALID_PROFILE_ID 0xFFFFu

typedef union {
  uint8_t *ptrToDefaultValue;
  uint16_t defaultValue;
} EmberAfDefaultAttributeValue;

typedef struct {
  EmberAfDefaultAttributeValue defaultValue;
  EmberAfDefaultAttributeValue minValue;
  EmberAfDefaultAttributeValue maxValue;
} EmberAfAttributeMinMaxValue;

typedef union {
  uint8_t *ptrToDefaultValue;
  uint16_t defaultValue;
  EmberAfAttributeMinMaxValue *ptrToMinMaxValue;
} EmberAfDefaultOrMinMaxAttributeValue;

typedef struct {
  EmberAfAttributeId attributeId;
  EmberAfAttributeType attributeType;
  uint8_t size;
  EmberAfAttributeMask mask;
  EmberAfDefaultOrMinMaxAttributeValue  defaultValue;
} EmberAfAttributeMetadata;

typedef struct {
  EmberAfClusterId clusterId;
  EmberAfAttributeMetadata *attributes;
  uint16_t attributeCount;
  uint16_t clusterSize;
  EmberAfClusterMask mask;

  const EmberAfGenericClusterFunction *functions;
} EmberAfCluster;

typedef struct {
  uint8_t endpoint;

  EmberAfClusterId clusterId;

  EmberAfClusterMask clusterMask;

  EmberAfAttributeId attributeId;

  uint16_t manufacturerCode;
} EmberAfAttributeSearchRecord;

typedef struct {
  uint16_t index;
  uint16_t manufacturerCode;
} EmberAfManufacturerCodeEntry;

typedef uint64_t EmberAfDifferenceType;

typedef struct {
  EmberIncomingMessageType type;
  EmberApsFrame* apsFrame;
  uint8_t* message;
  uint16_t msgLen;
  uint16_t source;
  uint8_t lastHopLqi;
  int8_t lastHopRssi;
  uint8_t bindingTableIndex;
  uint8_t addressTableIndex;
  uint8_t networkIndex;
} EmberAfIncomingMessage;

typedef uint8_t EmberAfInterpanMessageType;
#define EMBER_AF_INTER_PAN_UNICAST   0x00u
#define EMBER_AF_INTER_PAN_BROADCAST 0x08u
#define EMBER_AF_INTER_PAN_MULTICAST 0x0Cu

// Legacy names
#define INTER_PAN_UNICAST   EMBER_AF_INTER_PAN_UNICAST
#define INTER_PAN_BROADCAST EMBER_AF_INTER_PAN_BROADCAST
#define INTER_PAN_MULTICAST EMBER_AF_INTER_PAN_MULTICAST

#define EMBER_AF_INTERPAN_OPTION_NONE                 0x0000u
#define EMBER_AF_INTERPAN_OPTION_APS_ENCRYPT          0x0001u
#define EMBER_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESS 0x0002u

typedef uint16_t EmberAfInterpanOptions;

typedef struct {
  EmberAfInterpanMessageType messageType;

  EmberEUI64 longAddress;
  EmberNodeId shortAddress;
  EmberPanId panId;

  EmberAfProfileId profileId;
  EmberAfClusterId clusterId;
  EmberMulticastId groupId;
  EmberAfInterpanOptions options;
} EmberAfInterpanHeader;

// Legacy Name
#define InterPanHeader EmberAfInterpanHeader

typedef uint8_t EmberAfAllowedInterpanOptions;

#define EMBER_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVER 0x01u
#define EMBER_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENT 0x02u
#define EMBER_AF_INTERPAN_DIRECTION_BOTH             0x03u
#define EMBER_AF_INTERPAN_GLOBAL_COMMAND             0x04u
#define EMBER_AF_INTERPAN_MANUFACTURER_SPECIFIC      0x08u

typedef struct {
  EmberAfProfileId profileId;
  EmberAfClusterId clusterId;
  uint8_t commandId;
  EmberAfAllowedInterpanOptions options;
} EmberAfAllowedInterPanMessage;

typedef struct {
  EmberApsFrame            *apsFrame;
  EmberIncomingMessageType  type;
  EmberNodeId               source;
  uint8_t                    *buffer;
  uint16_t                    bufLen;
  bool                   clusterSpecific;
  bool                   mfgSpecific;
  uint16_t                    mfgCode;
  uint8_t                     seqNum;
  uint8_t                     commandId;
  uint8_t                     payloadStartIndex;
  uint8_t                     direction;
  EmberAfInterpanHeader    *interPanHeader;
  uint8_t                     networkIndex;
} EmberAfClusterCommand;

typedef struct {
  EmberAfCluster *cluster;
  uint8_t  clusterCount;
  uint16_t endpointSize;
} EmberAfEndpointType;

#ifdef EZSP_HOST
typedef EzspDecisionId EmberAfTcLinkKeyRequestPolicy;
typedef EzspDecisionId EmberAfAppLinkKeyRequestPolicy;
  #define EMBER_AF_ALLOW_TC_KEY_REQUESTS                       EZSP_ALLOW_TC_KEY_REQUESTS_AND_SEND_CURRENT_KEY
  #define EMBER_AF_DENY_TC_KEY_REQUESTS                        EZSP_DENY_TC_KEY_REQUESTS
  #define EMBER_AF_ALLOW_APP_KEY_REQUESTS                      EZSP_ALLOW_APP_KEY_REQUESTS
  #define EMBER_AF_DENY_APP_KEY_REQUESTS                       EZSP_DENY_APP_KEY_REQUESTS
#else
typedef EmberTcLinkKeyRequestPolicy EmberAfTcLinkKeyRequestPolicy;
typedef EmberAppLinkKeyRequestPolicy EmberAfAppLinkKeyRequestPolicy;
  #define EMBER_AF_ALLOW_TC_KEY_REQUESTS                       EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY
  #define EMBER_AF_DENY_TC_KEY_REQUESTS                        EMBER_DENY_TC_LINK_KEY_REQUESTS
  #define EMBER_AF_ALLOW_APP_KEY_REQUESTS                      EMBER_ALLOW_APP_LINK_KEY_REQUEST
  #define EMBER_AF_DENY_APP_KEY_REQUESTS                       EMBER_DENY_APP_LINK_KEY_REQUESTS
#endif

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfSecurityProfile
#else
typedef uint8_t EmberAfSecurityProfile;
enum
#endif
{
  EMBER_AF_SECURITY_PROFILE_NONE    = 0x00,
  EMBER_AF_SECURITY_PROFILE_HA      = 0x01,
  EMBER_AF_SECURITY_PROFILE_HA12    = 0x02,
  EMBER_AF_SECURITY_PROFILE_SE_TEST = 0x03,
  EMBER_AF_SECURITY_PROFILE_SE_FULL = 0x04,
  EMBER_AF_SECURITY_PROFILE_Z3      = 0x05,
  EMBER_AF_SECURITY_PROFILE_CUSTOM  = 0xFF,
};

typedef struct {
  EmberAfSecurityProfile       securityProfile;
  uint16_t                       tcBitmask;
  EmberExtendedSecurityBitmask tcExtendedBitmask;
  uint16_t                       nodeBitmask;
  EmberExtendedSecurityBitmask nodeExtendedBitmask;
  EmberAfTcLinkKeyRequestPolicy  tcLinkKeyRequestPolicy;
  EmberAfAppLinkKeyRequestPolicy  appLinkKeyRequestPolicy;
  EmberKeyData                 preconfiguredKey;
} EmberAfSecurityProfileData;

#ifndef DOXYGEN_SHOULD_SKIP_THIS
typedef struct {
  EmberNodeType nodeType;
  EmberAfSecurityProfile securityProfile;
} EmAfZigbeeProNetwork;

#endif

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfEndpointBitmask;
#else
typedef uint8_t EmberAfEndpointBitmask;
enum
#endif
{
  EMBER_AF_ENDPOINT_DISABLED = 0x00,
  EMBER_AF_ENDPOINT_ENABLED  = 0x01,
};

typedef struct {
  uint8_t endpoint;
  EmberAfProfileId profileId;
  uint16_t deviceId;
  uint8_t deviceVersion;
  EmberAfEndpointType *endpointType;
  uint8_t networkIndex;
  EmberAfEndpointBitmask bitmask;
} EmberAfDefinedEndpoint;

// Cluster-specific types

#if (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 8)
typedef uint8_t EmberAfPluginEsiManagementBitmask;
#elif (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 16)
typedef uint16_t EmberAfPluginEsiManagementBitmask;
#elif (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 32)
typedef uint32_t EmberAfPluginEsiManagementBitmask;
#else
  #error "EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE cannot exceed 32"
#endif

typedef struct {
  uint32_t     eventId;
#if defined(EMBER_AF_PLUGIN_DRLC_SERVER) || defined(SL_CATALOG_ZIGBEE_DRLC_SERVER_PRESENT)
  EmberEUI64 source;
  uint8_t      sourceEndpoint;
#endif //EMBER_AF_PLUGIN_DRLC_SERVER || SL_CATALOG_ZIGBEE_DRLC_SERVER_PRESENT

#if defined(EMBER_AF_PLUGIN_DRLC) || defined(SL_CATALOG_ZIGBEE_DRLC_PRESENT)
  EmberAfPluginEsiManagementBitmask esiBitmask;
#endif //EMBER_AF_PLUGIN_DRLC || SL_CATALOG_ZIGBEE_DRLC_PRESENT

  uint8_t      destinationEndpoint;
  uint16_t     deviceClass;
  uint8_t      utilityEnrollmentGroup;
  uint32_t     startTime;
  uint16_t     duration;
  uint8_t      criticalityLevel;
  uint8_t      coolingTempOffset;
  uint8_t      heatingTempOffset;
  int16_t     coolingTempSetPoint;
  int16_t     heatingTempSetPoint;
  int8_t      avgLoadPercentage;
  uint8_t      dutyCycle;
  uint8_t      eventControl;
  uint32_t     startRand;
  uint32_t     durationRand;
  uint8_t      optionControl;
} EmberAfLoadControlEvent;

typedef enum {
  EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE               = 0x00,
  EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED      = 0x01,
  EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT                  = 0x02,
  EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE   = 0x03,
  EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x04,
  EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE   = 0x05,
  EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x06,
} EmberAfServiceDiscoveryStatus;

#define EM_AF_DISCOVERY_RESPONSE_MASK (0x05u)

#define emberAfHaveDiscoveryResponseStatus(status)  ((status) & EM_AF_DISCOVERY_RESPONSE_MASK)

typedef struct {
  EmberAfServiceDiscoveryStatus status;

  uint16_t zdoRequestClusterId;

  EmberNodeId matchAddress;

  const void* responseData;
} EmberAfServiceDiscoveryResult;

typedef struct {
  uint8_t count;
  const uint8_t* list;
} EmberAfEndpointList;

typedef struct {
  uint8_t inClusterCount;
  const uint16_t* inClusterList;
  uint8_t outClusterCount;
  const uint16_t* outClusterList;
  EmberAfProfileId profileId;
  uint16_t deviceId;
  uint8_t endpoint;
} EmberAfClusterList;

typedef void (EmberAfServiceDiscoveryCallback)(const EmberAfServiceDiscoveryResult* result);

typedef void (EmberAfPartnerLinkKeyExchangeCallback)(bool success);

typedef enum {
  EMBER_AF_LONG_POLL,
  EMBER_AF_SHORT_POLL,
} EmberAfEventPollControl;

typedef enum {
  EMBER_AF_OK_TO_SLEEP,
  EMBER_AF_OK_TO_HIBERNATE = EMBER_AF_OK_TO_SLEEP,
  EMBER_AF_OK_TO_NAP,
  EMBER_AF_STAY_AWAKE,
} EmberAfEventSleepControl;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfApplicationTask
#else
typedef uint32_t EmberAfApplicationTask;
enum
#endif
{
  // we may be able to remove these top two since they are
  // handled by the stack on the SOC.
  EMBER_AF_WAITING_FOR_DATA_ACK                     = 0x00000001, //not needed?
  EMBER_AF_LAST_POLL_GOT_DATA                       = 0x00000002, //not needed?
  EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY            = 0x00000004,
  EMBER_AF_WAITING_FOR_ZDO_RESPONSE                 = 0x00000008,
  EMBER_AF_WAITING_FOR_ZCL_RESPONSE                 = 0x00000010,
  EMBER_AF_WAITING_FOR_REGISTRATION                 = 0x00000020,
  EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE    = 0x00000040,
  EMBER_AF_FORCE_SHORT_POLL                         = 0x00000080,
  EMBER_AF_FRAGMENTATION_IN_PROGRESS                = 0x00000100,
  EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY = 0x00000200,
  EMBER_AF_WAITING_FOR_TC_KEY_UPDATE                = 0x00000400,
};

typedef struct {
  uint8_t endpoint;
  EmberAfClusterId clusterId;
  bool isClient;
  EmberAfEventPollControl pollControl;
  EmberAfEventSleepControl sleepControl;
  EmberEventControl *eventControl;
} EmberAfEventContext;

#ifdef UC_BUILD
// TODO: update doxygen
typedef struct {
  uint8_t endpoint;
  EmberAfClusterId clusterId;
  bool isClient;
  EmberAfEventPollControl pollControl;
  EmberAfEventSleepControl sleepControl;
  sl_zigbee_event_t *event;
} sl_zigbee_event_context_t;
#endif

typedef void (*EmberAfNetworkEventHandler)(void);

typedef void (*EmberAfEndpointEventHandler)(uint8_t endpoint);

#define EMBER_AF_GROUP_TABLE_NULL_INDEX 0xFFu

#define EMBER_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID 0x00u

#define ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH 16u

typedef struct {
  uint8_t  endpoint; // 0x00 when not in use
  uint16_t groupId;
  uint8_t  bindingIndex;
#ifdef EMBER_AF_PLUGIN_GROUPS_SERVER_NAME_SUPPORT
  uint8_t  name[ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
} EmberAfGroupTableEntry;

#define EMBER_AF_SCENE_TABLE_NULL_INDEX 0xFFu

#define EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID 0x00u

#define ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH 16u

#define ZCL_SCENES_GLOBAL_SCENE_GROUP_ID 0x0000u

#define ZCL_SCENES_GLOBAL_SCENE_SCENE_ID 0x00u

// EMZIGBEE-6833: EmberAfSceneTableEntry declaration should be moved to the scenes component.
#ifdef UC_BUILD
#include "sl_component_catalog.h"
#ifdef SL_CATALOG_ZIGBEE_SCENES_PRESENT
#include "scenes-config.h"
#if (EMBER_AF_PLUGIN_SCENES_NAME_SUPPORT == 1)
#define SCENES_NAME_SUPPORT
#endif
#endif // SL_CATALOG_ZIGBEE_SCENES_PRESENT
#else // !UC_BUILD
#ifdef EMBER_AF_PLUGIN_SCENES_NAME_SUPPORT
#define SCENES_NAME_SUPPORT
#endif
#endif // UC_BUILD

typedef struct {
  uint8_t   endpoint;                // 0x00 when this record is not in use
  uint16_t  groupId;                 // 0x0000 if not associated with a group
  uint8_t   sceneId;
#ifdef SCENES_NAME_SUPPORT
  uint8_t   name[ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
  uint16_t  transitionTime;          // in seconds
  uint8_t   transitionTime100ms;     // in tenths of a seconds
#ifdef ZCL_USING_ON_OFF_CLUSTER_SERVER
  bool hasOnOffValue;
  bool onOffValue;
#endif
#ifdef ZCL_USING_LEVEL_CONTROL_CLUSTER_SERVER
  bool hasCurrentLevelValue;
  uint8_t   currentLevelValue;
#endif
#ifdef ZCL_USING_THERMOSTAT_CLUSTER_SERVER
  bool hasOccupiedCoolingSetpointValue;
  int16_t  occupiedCoolingSetpointValue;
  bool hasOccupiedHeatingSetpointValue;
  int16_t  occupiedHeatingSetpointValue;
  bool hasSystemModeValue;
  uint8_t   systemModeValue;
#endif
#ifdef ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
  bool hasCurrentXValue;
  uint16_t  currentXValue;
  bool hasCurrentYValue;
  uint16_t  currentYValue;
  bool hasEnhancedCurrentHueValue;
  uint16_t  enhancedCurrentHueValue;
  bool hasCurrentSaturationValue;
  uint8_t   currentSaturationValue;
  bool hasColorLoopActiveValue;
  uint8_t   colorLoopActiveValue;
  bool hasColorLoopDirectionValue;
  uint8_t   colorLoopDirectionValue;
  bool hasColorLoopTimeValue;
  uint16_t  colorLoopTimeValue;
  bool hasColorTemperatureMiredsValue;
  uint16_t  colorTemperatureMiredsValue;
#endif //ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
#ifdef ZCL_USING_DOOR_LOCK_CLUSTER_SERVER
  bool hasLockStateValue;
  uint8_t   lockStateValue;
#endif
#ifdef ZCL_USING_WINDOW_COVERING_CLUSTER_SERVER
  bool hasCurrentPositionLiftPercentageValue;
  uint8_t   currentPositionLiftPercentageValue;
  bool hasCurrentPositionTiltPercentageValue;
  uint8_t   currentPositionTiltPercentageValue;
#endif
} EmberAfSceneTableEntry;

#if !defined(EMBER_AF_PLUGIN_MESSAGING_CLIENT) && !defined(SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT)
// To forward declare callbacks regardless of whether the plugin
// is enabled,  define all data structures. To define
// the messaging client data struct, declare this variable.
  #define EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE 0
#endif

typedef struct {
  bool    valid;
  bool    active;
  EmberAfPluginEsiManagementBitmask esiBitmask;
  uint8_t      clientEndpoint;
  uint32_t     messageId;
  uint8_t      messageControl;
  uint32_t     startTime;
  uint32_t     endTime;
  uint16_t     durationInMinutes;
  uint8_t      message[EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE + 1];
} EmberAfPluginMessagingClientMessage;

#define ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH 11u
typedef struct {
  bool valid;
  bool active;
  uint8_t   clientEndpoint;
  uint32_t  providerId;
  uint8_t   rateLabel[ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH + 1];
  uint32_t  issuerEventId;
  uint32_t  currentTime;
  uint8_t   unitOfMeasure;
  uint16_t  currency;
  uint8_t   priceTrailingDigitAndPriceTier;
  uint8_t   numberOfPriceTiersAndRegisterTier;
  uint32_t  startTime;
  uint32_t  endTime;
  uint16_t  durationInMinutes;
  uint32_t  price;
  uint8_t   priceRatio;
  uint32_t  generationPrice;
  uint8_t   generationPriceRatio;
  uint32_t  alternateCostDelivered;
  uint8_t   alternateCostUnit;
  uint8_t   alternateCostTrailingDigit;
  uint8_t   numberOfBlockThresholds;
  uint8_t   priceControl;
} EmberAfPluginPriceClientPrice;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfPluginPriceCppAuth
#else
typedef uint8_t EmberAfPluginPriceCppAuth;
enum
#endif
{
  EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING  = 0,
  EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED = 1,
  EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED = 2,
  EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED   = 3,
  EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED = 4
};

#define EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID 0x00u

typedef struct {
  EmberAfReportingDirection direction;
  uint8_t endpoint;
  EmberAfClusterId clusterId;
  EmberAfAttributeId attributeId;
  uint8_t mask;
  uint16_t manufacturerCode;
  union {
    struct {
      uint16_t minInterval;
      uint16_t maxInterval;
      uint32_t reportableChange;
    } reported;
    struct {
      EmberNodeId source;
      uint8_t endpoint;
      uint16_t timeout;
    } received;
  } data;
} EmberAfPluginReportingEntry;

typedef enum {
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS                          = 0x00,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY                             = 0x01,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS               = 0x02,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED           = 0x03,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED       = 0x04,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED      = 0xF9,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND           = 0xFA,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL               = 0xFB,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED = 0xFC,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED         = 0xFD,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED            = 0xFE,
  EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT           = 0xFF,
} EmberAfPluginTunnelingClientStatus;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfZllCommissioningStatus
#else
typedef uint8_t EmberAfZllCommissioningStatus;
enum
#endif
{
  EMBER_AF_ZLL_ABORTED_BY_APPLICATION                      = 0x00,
  EMBER_AF_ZLL_CHANNEL_CHANGE_FAILED                       = 0x01,
  EMBER_AF_ZLL_JOINING_FAILED                              = 0x02,
  EMBER_AF_ZLL_NO_NETWORKS_FOUND                           = 0x03,
  EMBER_AF_ZLL_PREEMPTED_BY_STACK                          = 0x04,
  EMBER_AF_ZLL_SENDING_START_JOIN_FAILED                   = 0x05,
  EMBER_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED   = 0x06,
  EMBER_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED             = 0x07,
  EMBER_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED = 0x08,
  EMBER_AF_ZLL_NETWORK_FORMATION_FAILED                    = 0x09,
  EMBER_AF_ZLL_NETWORK_UPDATE_OPERATION                    = 0x0A,
};

typedef struct {
  EmberMulticastId groupId;
  uint8_t            groupType;
} EmberAfPluginZllCommissioningGroupInformationRecord;

typedef struct {
  EmberNodeId networkAddress;
  uint8_t       endpointId;
  uint16_t      profileId;
  uint16_t      deviceId;
  uint8_t       version;
} EmberAfPluginZllCommissioningEndpointInformationRecord;

typedef struct {
  uint16_t manufacturerId;
  uint16_t imageTypeId;
  uint32_t firmwareVersion;

  uint8_t deviceSpecificFileEui64[EUI64_SIZE];
} EmberAfOtaImageId;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfImageBlockRequestOptions
#else
typedef uint8_t EmberAfImageBlockRequestOptions;
enum
#endif
{
  EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE                          = 0x00,
  // Client supports Min Block Request field
  EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT = 0x01,
  // Server supports Min Block Request field
  EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER = 0x02,
  // The Image Block Request is actually simulated in place of an actually
  // received Image Page Request
  EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST           = 0x04
};

typedef struct {
  const EmberAfOtaImageId* id;
  uint32_t offset;
  uint32_t waitTimeSecondsResponse;
  EmberNodeId source;
  EmberEUI64 sourceEui;           // optionally present in messages
  // The minBlockRequestPeriod can be treated as milliseconds or seconds on the
  // client. The OTA server plugin has optional support to probe clients and
  // treat this field with appropriate units (ms or sec)
  uint16_t minBlockRequestPeriod; // optionally present in messages
  uint8_t maxDataSize;
  uint8_t clientEndpoint;
  EmberAfImageBlockRequestOptions bitmask;
} EmberAfImageBlockRequestCallbackStruct;

typedef enum {
  EMBER_AF_OTA_STORAGE_SUCCESS               = 0,
  EMBER_AF_OTA_STORAGE_ERROR                 = 1,
  EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG  = 2,
  EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND    = 3,
  EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS = 4,
} EmberAfOtaStorageStatus;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfOtaDownloadResult
#else
typedef uint8_t EmberAfOtaDownloadResult;
enum
#endif
{
  EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS = 0,
  EMBER_AF_OTA_DOWNLOAD_TIME_OUT           = 1,
  EMBER_AF_OTA_VERIFY_FAILED               = 2,
  EMBER_AF_OTA_SERVER_ABORTED              = 3,
  EMBER_AF_OTA_CLIENT_ABORTED              = 4,
  EMBER_AF_OTA_ERASE_FAILED                = 5,
};

#define EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH 32u

#define UID_SIZE 32u

typedef struct {
  // Magic Number omitted since it is always the same.
  uint16_t headerVersion;
  uint16_t headerLength;
  uint16_t fieldControl;
  uint16_t manufacturerId;
  uint16_t imageTypeId;           // a.k.a. Device ID
  uint32_t firmwareVersion;
  uint16_t zigbeeStackVersion;

  uint8_t headerString[EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH + 1];

  uint32_t imageSize;

  uint8_t securityCredentials;
  union {
    uint8_t EUI64[EUI64_SIZE];
    uint8_t UID[UID_SIZE];
  } upgradeFileDestination;
  uint16_t minimumHardwareVersion;
  uint16_t maximumHardwareVersion;
} EmberAfOtaHeader;

typedef struct {
  uint16_t id;
  uint32_t length;
} EmberAfTagData;

typedef enum {
  NO_APP_MESSAGE               = 0,
  RECEIVED_PARTNER_CERTIFICATE = 1,
  GENERATING_EPHEMERAL_KEYS    = 2,
  GENERATING_SHARED_SECRET     = 3,
  KEY_GENERATION_DONE          = 4,
  GENERATE_SHARED_SECRET_DONE  = 5,
  LINK_KEY_ESTABLISHED         = 6,

  NO_LOCAL_RESOURCES          = 7,
  PARTNER_NO_RESOURCES        = 8,
  TIMEOUT_OCCURRED            = 9,
  INVALID_APP_COMMAND         = 10,
  MESSAGE_SEND_FAILURE        = 11,
  PARTNER_SENT_TERMINATE      = 12,
  INVALID_PARTNER_MESSAGE     = 13,
  PARTNER_SENT_DEFAULT_RESPONSE_ERROR = 14,

  BAD_CERTIFICATE_ISSUER      = 15,
  KEY_CONFIRM_FAILURE         = 16,
  BAD_KEY_ESTABLISHMENT_SUITE = 17,

  KEY_TABLE_FULL              = 18,

  NO_ESTABLISHMENT_ALLOWED    = 19,

  /* 283k1 certificates need to have valid key usage.
   */
  INVALID_CERTIFICATE_KEY_USAGE = 20,
} EmberAfKeyEstablishmentNotifyMessage;

#define APP_NOTIFY_ERROR_CODE_START NO_LOCAL_RESOURCES
#define APP_NOTIFY_MESSAGE_TEXT { \
    "None",                       \
    "Received Cert",              \
    "Generate keys",              \
    "Generate secret",            \
    "Key generate done",          \
    "Generate secret done",       \
    "Link key verified",          \
                                  \
    /* Transient Error codes */   \
    "No local resources",         \
    "Partner no resources",       \
    "Timeout",                    \
    "Invalid app. command",       \
    "Message send failure",       \
    "Partner sent terminate",     \
    "Bad message",                \
    "Partner sent Default Rsp",   \
                                  \
    /* Fatal errors */            \
    "Bad cert issuer",            \
    "Key confirm failure",        \
    "Bad key est. suite",         \
    "Key table full",             \
    "Not allowed",                \
    "Invalid Key Usage",          \
}

typedef enum {
  EMBER_AF_IMAGE_GOOD                 = 0,
  EMBER_AF_IMAGE_BAD                  = 1,
  EMBER_AF_IMAGE_VERIFY_IN_PROGRESS   = 2,

#ifndef DOXYGEN_SHOULD_SKIP_THIS
  // Internal use only.
  EMBER_AF_IMAGE_VERIFY_WAIT          = 3,
  EMBER_AF_IMAGE_VERIFY_ERROR         = 4,
  EMBER_AF_IMAGE_UNKNOWN              = 5,
  EMBER_AF_NO_IMAGE_VERIFY_SUPPORT    = 6,
#endif
} EmberAfImageVerifyStatus;

typedef void (*EmberAfTickFunction)(uint8_t endpoint);

typedef void (*EmberAfInitFunction)(uint8_t endpoint);

typedef void (*EmberAfClusterAttributeChangedCallback)(uint8_t endpoint,
                                                       EmberAfAttributeId attributeId);

typedef void (*EmberAfManufacturerSpecificClusterAttributeChangedCallback)(uint8_t endpoint,
                                                                           EmberAfAttributeId attributeId,
                                                                           uint16_t manufacturerCode);

typedef EmberAfStatus (*EmberAfClusterPreAttributeChangedCallback)(uint8_t endpoint,
                                                                   EmberAfAttributeId attributeId,
                                                                   EmberAfAttributeType attributeType,
                                                                   uint8_t size,
                                                                   uint8_t *value);

typedef void (*EmberAfDefaultResponseFunction)(uint8_t endpoint,
                                               uint8_t commandId,
                                               EmberAfStatus status);

typedef void (*EmberAfMessageSentFunction)(EmberOutgoingMessageType type,
                                           uint16_t indexOrDestination,
                                           EmberApsFrame *apsFrame,
                                           uint16_t msgLen,
                                           uint8_t *message,
                                           EmberStatus status);

typedef struct {
  EmberAfMessageSentFunction callback;
  EmberApsFrame* apsFrame;
  uint8_t* message;
  uint16_t indexOrDestination;
  uint16_t messageLength;
  EmberOutgoingMessageType type;
  bool broadcast;
} EmberAfMessageStruct;

typedef struct {
  EmberEUI64 deviceId;
  EmberKeyData key;
} EmberAfLinkKeyBackupData;

typedef struct {
  EmberEUI64 extendedPanId;
  uint8_t keyListLength;
  uint8_t maxKeyListLength;
  EmberAfLinkKeyBackupData* keyList;
} EmberAfTrustCenterBackupData;

#define EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH 16u

typedef struct {
  uint8_t hardwareTag[EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH];
  uint8_t eui64[EUI64_SIZE];
  uint16_t mfgId;
  uint16_t bootloaderVersion;
  uint8_t capabilities;
  uint8_t platform;
  uint8_t micro;
  uint8_t phy;
  bool bootloaderActive;
} EmberAfStandaloneBootloaderQueryResponseData;

typedef struct {
  uint16_t clusterId;
  uint8_t commandId;
  uint8_t mask;
} EmberAfCommandMetadata;

typedef struct {
  uint16_t year;
  uint8_t month;
  uint8_t day;
  uint8_t hours;
  uint8_t minutes;
  uint8_t seconds;
} EmberAfTimeStruct;

typedef struct {
  uint8_t year;
  uint8_t month;
  uint8_t dayOfMonth;
  uint8_t dayOfWeek;
} EmberAfDate;

/* Simple Metering Server Test Code */
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METER 0
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METER 1

// Functional Notification Flags
// Also #defined in enums.h under slightly different names
#define EMBER_AF_METERING_FNF_NEW_OTA_FIRMWARE                               0x00000001
#define EMBER_AF_METERING_FNF_CBKE_UPDATE_REQUEST                            0x00000002
#define EMBER_AF_METERING_FNF_TIME_SYNC                                      0x00000004
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_HAN                         0x00000010
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_WAN                         0x00000020
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SET    0x000001C0
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SET  0x00000E00
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTER             0x00001000
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTER          0x00002000
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTER        0x00004000
#define EMBER_AF_METERING_FNF_NETWORK_KEY_ACTIVE                             0x00008000
#define EMBER_AF_METERING_FNF_DISPLAY_MESSAGE                                0x00010000
#define EMBER_AF_METERING_FNF_CANCEL_ALL_MESSAGES                            0x00020000
#define EMBER_AF_METERING_FNF_CHANGE_SUPPLY                                  0x00040000
#define EMBER_AF_METERING_FNF_LOCAL_CHANGE_SUPPLY                            0x00080000
#define EMBER_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLD                0x00100000
#define EMBER_AF_METERING_FNF_TUNNEL_MESSAGE_PENDING                         0x00200000
#define EMBER_AF_METERING_FNF_GET_SNAPSHOT                                   0x00400000
#define EMBER_AF_METERING_FNF_GET_SAMPLED_DATA                               0x00800000
#define EMBER_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLE            0x01000000
#define EMBER_AF_METERING_FNF_ENERGY_SCAN_PENDING                            0x02000000
#define EMBER_AF_METERING_FNF_CHANNEL_CHANGE_PENDING                         0x04000000

// Notification Flags 2
#define EMBER_AF_METERING_NF2_PUBLISH_PRICE                                  0x00000001
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_PERIOD                           0x00000002
#define EMBER_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATION                     0x00000004
#define EMBER_AF_METERING_NF2_PUBLISH_CONVERSION_FACTOR                      0x00000008
#define EMBER_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUE                        0x00000010
#define EMBER_AF_METERING_NF2_PUBLISH_CO2_VALUE                              0x00000020
#define EMBER_AF_METERING_NF2_PUBLISH_BILLING_PERIOD                         0x00000040
#define EMBER_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILL                      0x00000080
#define EMBER_AF_METERING_NF2_PUBLISH_PRICE_MATRIX                           0x00000100
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDS                       0x00000200
#define EMBER_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSION                    0x00000400
#define EMBER_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFO                    0x00001000
#define EMBER_AF_METERING_NF2_PUBLISH_CPP_EVENT                              0x00002000
#define EMBER_AF_METERING_NF2_PUBLISH_TIER_LABELS                            0x00004000
#define EMBER_AF_METERING_NF2_CANCEL_TARIFF                                  0x00008000

// Notification Flags 3
#define EMBER_AF_METERING_NF3_PUBLISH_CALENDAR                               0x00000001
#define EMBER_AF_METERING_NF3_PUBLISH_SPECIAL_DAYS                           0x00000002
#define EMBER_AF_METERING_NF3_PUBLISH_SEASONS                                0x00000004
#define EMBER_AF_METERING_NF3_PUBLISH_WEEK                                   0x00000008
#define EMBER_AF_METERING_NF3_PUBLISH_DAY                                    0x00000010
#define EMBER_AF_METERING_NF3_CANCEL_CALENDAR                                0x00000020

// Notification Flags 4
#define EMBER_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDIT              0x00000001
#define EMBER_AF_METERING_NF4_CHANGE_DEBT                                    0x00000002
#define EMBER_AF_METERING_NF4_EMERGENCY_CREDIT_SETUP                         0x00000004
#define EMBER_AF_METERING_NF4_CONSUMER_TOP_UP                                0x00000008
#define EMBER_AF_METERING_NF4_CREDIT_ADJUSTMENT                              0x00000010
#define EMBER_AF_METERING_NF4_CHANGE_PAYMENT_MODE                            0x00000020
#define EMBER_AF_METERING_NF4_GET_PREPAY_SNAPSHOT                            0x00000040
#define EMBER_AF_METERING_NF4_GET_TOP_UP_LOG                                 0x00000080
#define EMBER_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVEL                   0x00000100
#define EMBER_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOG                         0x00000200
#define EMBER_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMIT                       0x00000400
#define EMBER_AF_METERING_NF4_SET_OVERALL_DEBT_CAP                           0x00000800

// Notification Flags 5
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCY                      0x00000001
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIER                     0x00000002
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSE                0x00000004
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSE                0x00000008
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSE                0x00000010
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSE                0x00000020
#define EMBER_AF_METERING_NF5_UPDATE_SITE_ID                                 0x00000040
#define EMBER_AF_METERING_NF5_RESET_BATTERY_COUNTER                          0x00000080
#define EMBER_AF_METERING_NF5_UPDATE_CIN                                     0x00000100

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfCbkeKeyEstablishmentSuite
#else
typedef uint16_t EmberAfCbkeKeyEstablishmentSuite;
enum
#endif
{
  EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE      = 0x0000,
  EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1   = 0x0001,
  EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1   = 0x0002,
};

#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH (16u)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH (18u)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH (32u)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH (24u)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH (10u)

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfDeviceManagementPasswordType
#else
typedef uint16_t EmberAfDeviceManagementPasswordType;
enum
#endif
{
  UNUSED_PASSWORD   = 0x00,
  SERVICE_PASSWORD  = 0x01,
  CONSUMER_PASSWORD = 0x02,
};

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfDeviceManagementChangePendingFlags
#else
typedef uint8_t EmberAfDeviceManagementChangePendingFlags;
enum
#endif
{
  EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK              = 0x01,
  EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK             = 0x02,
  EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK                 = 0x04,
  EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK                     = 0x08,
  EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK        = 0x10,
  EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK       = 0x20,
};

typedef struct {
  // Optional fields only used by Gas Proxy Function plugin.
  uint32_t providerId;
  uint32_t issuerEventId;
  uint8_t tariffType;

  // always used fields
  uint32_t implementationDateTime;
  uint32_t tenancy;
} EmberAfDeviceManagementTenancy;

typedef struct {
  uint32_t proposedProviderId;
  uint32_t implementationDateTime;
  uint32_t providerChangeControl;
  uint8_t proposedProviderName[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH + 1];
  uint8_t proposedProviderContactDetails[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH + 1];
} EmberAfDeviceManagementSupplier;

typedef struct {
  uint32_t requestDateTime;
  uint32_t implementationDateTime;
  uint8_t supplyStatus;
  uint8_t originatorIdSupplyControlBits;
} EmberAfDeviceManagementSupply;

typedef struct {
  uint8_t siteId[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH + 1];
  uint32_t implementationDateTime;
  uint32_t issuerEventId;
} EmberAfDeviceManagementSiteId;

typedef struct {
  uint8_t cin[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH + 1];
  uint32_t implementationDateTime;
  uint32_t issuerEventId;
} EmberAfDeviceManagementCIN;

typedef struct {
  bool supplyTamperState;
  bool supplyDepletionState;
  bool supplyUncontrolledFlowState;
  bool loadLimitSupplyState;
} EmberAfDeviceManagementSupplyStatusFlags;

typedef struct {
  uint16_t uncontrolledFlowThreshold;
  uint16_t multiplier;
  uint16_t divisor;
  uint16_t measurementPeriod;
  uint8_t unitOfMeasure;
  uint8_t stabilisationPeriod;
} EmberAfDeviceManagementUncontrolledFlowThreshold;

typedef struct {
  uint32_t implementationDateTime;
  uint8_t supplyStatus;
} EmberAfDeviceManagementSupplyStatus;

typedef struct {
  uint8_t password[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH + 1];
  uint32_t implementationDateTime;
  uint16_t durationInMinutes;
  EmberAfDeviceManagementPasswordType passwordType;
} EmberAfDeviceManagementPassword;

typedef struct {
  EmberAfDeviceManagementTenancy tenancy;
  EmberAfDeviceManagementSupplier supplier;
  EmberAfDeviceManagementSupply supply;
  EmberAfDeviceManagementSiteId siteId;
  EmberAfDeviceManagementCIN cin;
  EmberAfDeviceManagementSupplyStatusFlags supplyStatusFlags;
  EmberAfDeviceManagementSupplyStatus supplyStatus;
  //TODO: These passwords ought to be tokenized / hashed
  EmberAfDeviceManagementPassword servicePassword;
  EmberAfDeviceManagementPassword consumerPassword;
  EmberAfDeviceManagementUncontrolledFlowThreshold threshold;
  uint32_t providerId;
  uint32_t issuerEventId;
  uint8_t proposedLocalSupplyStatus;
  EmberAfTariffType tariffType;
  EmberAfDeviceManagementChangePendingFlags pendingUpdates;
} EmberAfDeviceManagementInfo;

typedef struct {
  uint8_t startIndex;
  uint8_t endIndex;
} EmberAfDeviceManagementAttributeRange;

// attrRange is a list of attributeId values in a cluster. It's needed to track contiguous
// segments of valid attributeId's with gaps in the middle.
// attributeSetId is the value of the upper byte in the attributeId. It ranges from 0x01(Price)
// to 0x08(OTA Event Configuration)
// Eg. {0x00,0x05} and {0x08,0x0A}
// We're betting that there isn't a list of cluster attributes that has more than 5 gaps.
typedef struct {
  uint8_t attributeSetId;
  EmberAfDeviceManagementAttributeRange attributeRange[7];
} EmberAfDeviceManagementAttributeTable;

typedef struct {
  bool encryption;

  uint8_t * plainPayload;
  uint16_t plainPayloadLength;

  uint8_t * encryptedPayload;
  uint16_t encryptedPayloadLength;
} EmberAfGbzMessageData;

typedef struct {
  uint8_t * gbzCommands;
  uint16_t  gbzCommandsLength;
  uint8_t * gbzCommandsResponse;
  uint16_t  gbzCommandsResponseLength;
  uint16_t  messageCode;
} EmberAfGpfMessage;

typedef uint16_t EmberAfRemoteClusterType;

#define EMBER_AF_REMOTE_CLUSTER_TYPE_NONE     0x0000u
#define EMBER_AF_REMOTE_CLUSTER_TYPE_SERVER   0x0001u
#define EMBER_AF_REMOTE_CLUSTER_TYPE_CLIENT   0x0002u
#define EMBER_AF_REMOTE_CLUSTER_TYPE_INVALID  0xFFFFu

typedef struct {
  EmberAfClusterId clusterId;
  EmberAfProfileId profileId;
  uint16_t deviceId;
  uint8_t endpoint;
  EmberAfRemoteClusterType type;
} EmberAfRemoteClusterStruct;

typedef struct {
  EmberEUI64 targetEUI64;
  uint8_t sourceEndpoint;
  uint8_t destEndpoint;
  uint16_t clusterId;
  EmberEUI64 destEUI64;
  EmberEUI64 sourceEUI64;
} EmberAfRemoteBindingStruct;

typedef struct {
  EmberAfClusterId clusterId;
  bool server;
} EmberAfClusterInfo;

#ifdef UC_BUILD
#include "sl_component_catalog.h"
#ifdef SL_CATALOG_ZIGBEE_DEVICE_DATABASE_PRESENT
#include "device-database-config.h"
#else
#define EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT 3u
#define EMBER_AF_MAX_ENDPOINTS_PER_DEVICE  1u
#endif
#else // UC_BUILD
#if !defined(EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT)
#define EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT 3u
#define EMBER_AF_MAX_ENDPOINTS_PER_DEVICE  1u
#endif
#endif // UC_BUILD

typedef struct {
  EmberAfClusterInfo clusters[EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT];
  EmberAfProfileId profileId;
  uint16_t deviceId;
  uint8_t endpoint;
  uint8_t clusterCount;
} EmberAfEndpointInfoStruct;

// Although we treat this like a bitmap, only 1 bit is set at a time.
// We use the bitmap feature to allow us to find all devices
// with any in a set of status codes using
// emberAfPluginDeviceDatabaseFindDeviceByStatus().
typedef enum {
  EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE                 = 0x00,
  EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW                  = 0x01,
  EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS       = 0x02,
  EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS        = 0x04,
  EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION  = 0x08,

  EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE      = 0x40,
  EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED    = 0x80,
} EmberAfDeviceDiscoveryStatus;

typedef struct {
  EmberEUI64 eui64;
  EmberAfEndpointInfoStruct endpoints[EMBER_AF_MAX_ENDPOINTS_PER_DEVICE];
  EmberAfDeviceDiscoveryStatus status;
  uint8_t discoveryFailures;
  uint8_t capabilities;
  uint8_t endpointCount;
  uint8_t stackRevision;
} EmberAfDeviceInfo;

typedef struct {
  uint16_t deviceIndex;
} EmberAfDeviceDatabaseIterator;

typedef struct {
  EmberNodeId emberNodeId;
  uint32_t timeStamp;
} EmberAfJoiningDevice;

#define EMBER_AF_INVALID_CLUSTER_ID 0xFFFFu

#define EMBER_AF_INVALID_ENDPOINT 0xFFu

#define EMBER_AF_INVALID_PAN_ID 0xFFFFu

#define EMBER_AF_PERMIT_JOIN_FOREVER     0xFFu
#define EMBER_AF_PERMIT_JOIN_MAX_TIMEOUT 0xFEu

#define EMBER_AF_ZDO_RESPONSE_OVERHEAD 2u

#endif // SILABS_AF_API_TYPES

Macros#

#define
EMBER_AF_NULL_MANUFACTURER_CODE 0x0000u

A distinguished manufacturer code that is used to indicate the absence of a manufacturer-specific profile, cluster, command, or attribute.

#define
EMBER_AF_INVALID_PROFILE_ID 0xFFFFu

An invalid profile ID This is a reserved profileId.

#define
EMBER_AF_INTER_PAN_UNICAST 0x00u
#define
EMBER_AF_INTER_PAN_BROADCAST 0x08u
#define
EMBER_AF_INTER_PAN_MULTICAST 0x0Cu
#define
INTER_PAN_UNICAST EMBER_AF_INTER_PAN_UNICAST
#define
INTER_PAN_BROADCAST EMBER_AF_INTER_PAN_BROADCAST
#define
INTER_PAN_MULTICAST EMBER_AF_INTER_PAN_MULTICAST
#define
EMBER_AF_INTERPAN_OPTION_NONE 0x0000u
#define
EMBER_AF_INTERPAN_OPTION_APS_ENCRYPT 0x0001u
#define
EMBER_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESS 0x0002u
#define
InterPanHeader EmberAfInterpanHeader
#define
EMBER_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVER 0x01u
#define
EMBER_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENT 0x02u
#define
EMBER_AF_INTERPAN_DIRECTION_BOTH 0x03u
#define
EMBER_AF_INTERPAN_GLOBAL_COMMAND 0x04u
#define
EMBER_AF_INTERPAN_MANUFACTURER_SPECIFIC 0x08u
#define
EMBER_AF_ALLOW_TC_KEY_REQUESTS EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY
#define
EMBER_AF_DENY_TC_KEY_REQUESTS EMBER_DENY_TC_LINK_KEY_REQUESTS
#define
EMBER_AF_ALLOW_APP_KEY_REQUESTS EMBER_ALLOW_APP_LINK_KEY_REQUEST
#define
EMBER_AF_DENY_APP_KEY_REQUESTS EMBER_DENY_APP_LINK_KEY_REQUESTS
#define
EM_AF_DISCOVERY_RESPONSE_MASK (0x05u)
#define
emberAfHaveDiscoveryResponseStatus (status)

A simple way to determine if the service discovery callback has a response.

#define
EMBER_AF_GROUP_TABLE_NULL_INDEX 0xFFu

Indicate the absence of a Group table entry.

#define
EMBER_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID 0x00u

Value used when setting or getting the endpoint in a Group table entry. It indicates that the entry is not in use.

#define
ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH 16u

Maximum length of Group names, not including the length byte.

#define
EMBER_AF_SCENE_TABLE_NULL_INDEX 0xFFu

Indicates the absence of a Scene table entry.

#define
EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID 0x00u

Value used when setting or getting the endpoint in a Scene table entry. It indicates that the entry is not in use.

#define
ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH 16u

Maximum length of Scene names, not including the length byte.

#define
ZCL_SCENES_GLOBAL_SCENE_GROUP_ID 0x0000u

The group identifier for the global scene.

#define
ZCL_SCENES_GLOBAL_SCENE_SCENE_ID 0x00u

The scene identifier for the global scene.

#define
EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE 0
#define
ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH 11u
#define
EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID 0x00u

Use when setting or getting the endpoint in a report table entry. It indicates that the entry is not in use.

#define
EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH 32u

The maximum size of the string that is present in the header of the Zigbee Over-the-air file format.

#define
UID_SIZE 32u
#define
APP_NOTIFY_ERROR_CODE_START NO_LOCAL_RESOURCES
#define
APP_NOTIFY_MESSAGE_TEXT undefined
#define
EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH 16u

The length of the hardware tag in the Ember Bootloader Query Response.

#define
EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METER 0
#define
EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METER 1
#define
EMBER_AF_METERING_FNF_NEW_OTA_FIRMWARE 0x00000001
#define
EMBER_AF_METERING_FNF_CBKE_UPDATE_REQUEST 0x00000002
#define
EMBER_AF_METERING_FNF_TIME_SYNC 0x00000004
#define
EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_HAN 0x00000010
#define
EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_WAN 0x00000020
#define
EMBER_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SET 0x000001C0
#define
EMBER_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SET 0x00000E00
#define
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTER 0x00001000
#define
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTER 0x00002000
#define
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTER 0x00004000
#define
EMBER_AF_METERING_FNF_NETWORK_KEY_ACTIVE 0x00008000
#define
EMBER_AF_METERING_FNF_DISPLAY_MESSAGE 0x00010000
#define
EMBER_AF_METERING_FNF_CANCEL_ALL_MESSAGES 0x00020000
#define
EMBER_AF_METERING_FNF_CHANGE_SUPPLY 0x00040000
#define
EMBER_AF_METERING_FNF_LOCAL_CHANGE_SUPPLY 0x00080000
#define
EMBER_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLD 0x00100000
#define
EMBER_AF_METERING_FNF_TUNNEL_MESSAGE_PENDING 0x00200000
#define
EMBER_AF_METERING_FNF_GET_SNAPSHOT 0x00400000
#define
EMBER_AF_METERING_FNF_GET_SAMPLED_DATA 0x00800000
#define
EMBER_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLE 0x01000000
#define
EMBER_AF_METERING_FNF_ENERGY_SCAN_PENDING 0x02000000
#define
EMBER_AF_METERING_FNF_CHANNEL_CHANGE_PENDING 0x04000000
#define
EMBER_AF_METERING_NF2_PUBLISH_PRICE 0x00000001
#define
EMBER_AF_METERING_NF2_PUBLISH_BLOCK_PERIOD 0x00000002
#define
EMBER_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATION 0x00000004
#define
EMBER_AF_METERING_NF2_PUBLISH_CONVERSION_FACTOR 0x00000008
#define
EMBER_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUE 0x00000010
#define
EMBER_AF_METERING_NF2_PUBLISH_CO2_VALUE 0x00000020
#define
EMBER_AF_METERING_NF2_PUBLISH_BILLING_PERIOD 0x00000040
#define
EMBER_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILL 0x00000080
#define
EMBER_AF_METERING_NF2_PUBLISH_PRICE_MATRIX 0x00000100
#define
EMBER_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDS 0x00000200
#define
EMBER_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSION 0x00000400
#define
EMBER_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFO 0x00001000
#define
EMBER_AF_METERING_NF2_PUBLISH_CPP_EVENT 0x00002000
#define
EMBER_AF_METERING_NF2_PUBLISH_TIER_LABELS 0x00004000
#define
EMBER_AF_METERING_NF2_CANCEL_TARIFF 0x00008000
#define
EMBER_AF_METERING_NF3_PUBLISH_CALENDAR 0x00000001
#define
EMBER_AF_METERING_NF3_PUBLISH_SPECIAL_DAYS 0x00000002
#define
EMBER_AF_METERING_NF3_PUBLISH_SEASONS 0x00000004
#define
EMBER_AF_METERING_NF3_PUBLISH_WEEK 0x00000008
#define
EMBER_AF_METERING_NF3_PUBLISH_DAY 0x00000010
#define
EMBER_AF_METERING_NF3_CANCEL_CALENDAR 0x00000020
#define
EMBER_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDIT 0x00000001
#define
EMBER_AF_METERING_NF4_CHANGE_DEBT 0x00000002
#define
EMBER_AF_METERING_NF4_EMERGENCY_CREDIT_SETUP 0x00000004
#define
EMBER_AF_METERING_NF4_CONSUMER_TOP_UP 0x00000008
#define
EMBER_AF_METERING_NF4_CREDIT_ADJUSTMENT 0x00000010
#define
EMBER_AF_METERING_NF4_CHANGE_PAYMENT_MODE 0x00000020
#define
EMBER_AF_METERING_NF4_GET_PREPAY_SNAPSHOT 0x00000040
#define
EMBER_AF_METERING_NF4_GET_TOP_UP_LOG 0x00000080
#define
EMBER_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVEL 0x00000100
#define
EMBER_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOG 0x00000200
#define
EMBER_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMIT 0x00000400
#define
EMBER_AF_METERING_NF4_SET_OVERALL_DEBT_CAP 0x00000800
#define
EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCY 0x00000001
#define
EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIER 0x00000002
#define
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSE 0x00000004
#define
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSE 0x00000008
#define
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSE 0x00000010
#define
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSE 0x00000020
#define
EMBER_AF_METERING_NF5_UPDATE_SITE_ID 0x00000040
#define
EMBER_AF_METERING_NF5_RESET_BATTERY_COUNTER 0x00000080
#define
EMBER_AF_METERING_NF5_UPDATE_CIN 0x00000100
#define
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH (16u)

Device Management plugin types.

#define
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH (18u)
#define
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH (32u)
#define
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH (24u)
#define
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH (10u)
#define
EMBER_AF_REMOTE_CLUSTER_TYPE_NONE 0x0000u
#define
EMBER_AF_REMOTE_CLUSTER_TYPE_SERVER 0x0001u
#define
EMBER_AF_REMOTE_CLUSTER_TYPE_CLIENT 0x0002u
#define
EMBER_AF_REMOTE_CLUSTER_TYPE_INVALID 0xFFFFu
#define
EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT 3u
#define
EMBER_AF_MAX_ENDPOINTS_PER_DEVICE 1u
#define
EMBER_AF_INVALID_CLUSTER_ID 0xFFFFu
#define
EMBER_AF_INVALID_ENDPOINT 0xFFu
#define
EMBER_AF_INVALID_PAN_ID 0xFFFFu
#define
EMBER_AF_PERMIT_JOIN_FOREVER 0xFFu

Permit join times.

#define
EMBER_AF_PERMIT_JOIN_MAX_TIMEOUT 0xFEu
#define
EMBER_AF_ZDO_RESPONSE_OVERHEAD 2u

The overhead of the ZDO response. 1 byte for the sequence and 1 byte for the status code.

Enumerations#

enum
EMBER_AF_SECURITY_PROFILE_NONE = 0x00
EMBER_AF_SECURITY_PROFILE_HA = 0x01
EMBER_AF_SECURITY_PROFILE_HA12 = 0x02
EMBER_AF_SECURITY_PROFILE_SE_TEST = 0x03
EMBER_AF_SECURITY_PROFILE_SE_FULL = 0x04
EMBER_AF_SECURITY_PROFILE_Z3 = 0x05
EMBER_AF_SECURITY_PROFILE_CUSTOM = 0xFF
}
enum
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE = 0x00
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED = 0x01
EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT = 0x02
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x03
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x04
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x05
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x06
}

Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.

enum
EMBER_AF_LONG_POLL
EMBER_AF_SHORT_POLL
}

Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.

enum
EMBER_AF_OK_TO_SLEEP
EMBER_AF_OK_TO_HIBERNATE = EMBER_AF_OK_TO_SLEEP
EMBER_AF_OK_TO_NAP
EMBER_AF_STAY_AWAKE
}

Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.

enum
EMBER_AF_WAITING_FOR_DATA_ACK = 0x00000001
EMBER_AF_LAST_POLL_GOT_DATA = 0x00000002
EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY = 0x00000004
EMBER_AF_WAITING_FOR_ZDO_RESPONSE = 0x00000008
EMBER_AF_WAITING_FOR_ZCL_RESPONSE = 0x00000010
EMBER_AF_WAITING_FOR_REGISTRATION = 0x00000020
EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE = 0x00000040
EMBER_AF_FORCE_SHORT_POLL = 0x00000080
EMBER_AF_FRAGMENTATION_IN_PROGRESS = 0x00000100
EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY = 0x00000200
EMBER_AF_WAITING_FOR_TC_KEY_UPDATE = 0x00000400
}

Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.

enum
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING = 0
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED = 1
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED = 2
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED = 3
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED = 4
}

Specifies CPP Authorization values.

enum
EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS = 0x00
EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY = 0x01
EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS = 0x02
EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED = 0x03
EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED = 0x04
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED = 0xF9
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND = 0xFA
EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL = 0xFB
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED = 0xFC
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED = 0xFD
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED = 0xFE
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT = 0xFF
}
enum
EMBER_AF_ZLL_ABORTED_BY_APPLICATION = 0x00
EMBER_AF_ZLL_CHANNEL_CHANGE_FAILED = 0x01
EMBER_AF_ZLL_JOINING_FAILED = 0x02
EMBER_AF_ZLL_NO_NETWORKS_FOUND = 0x03
EMBER_AF_ZLL_PREEMPTED_BY_STACK = 0x04
EMBER_AF_ZLL_SENDING_START_JOIN_FAILED = 0x05
EMBER_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED = 0x06
EMBER_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED = 0x07
EMBER_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED = 0x08
EMBER_AF_ZLL_NETWORK_FORMATION_FAILED = 0x09
EMBER_AF_ZLL_NETWORK_UPDATE_OPERATION = 0x0A
}

Status codes used by the ZLL Commissioning plugin.

enum
EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE = 0x00
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT = 0x01
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER = 0x02
EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST = 0x04
}

The list of options possible for the image block request/response.

enum
EMBER_AF_OTA_STORAGE_SUCCESS = 0
EMBER_AF_OTA_STORAGE_ERROR = 1
EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG = 2
EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND = 3
EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS = 4
}

Contain the success or error code of an OTA storage device operation.

enum
EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS = 0
EMBER_AF_OTA_DOWNLOAD_TIME_OUT = 1
EMBER_AF_OTA_VERIFY_FAILED = 2
EMBER_AF_OTA_SERVER_ABORTED = 3
EMBER_AF_OTA_CLIENT_ABORTED = 4
EMBER_AF_OTA_ERASE_FAILED = 5
}

Contain the success or error code of an OTA download operation.

enum
NO_APP_MESSAGE = 0
RECEIVED_PARTNER_CERTIFICATE = 1
GENERATING_EPHEMERAL_KEYS = 2
GENERATING_SHARED_SECRET = 3
KEY_GENERATION_DONE = 4
GENERATE_SHARED_SECRET_DONE = 5
LINK_KEY_ESTABLISHED = 6
NO_LOCAL_RESOURCES = 7
PARTNER_NO_RESOURCES = 8
TIMEOUT_OCCURRED = 9
INVALID_APP_COMMAND = 10
MESSAGE_SEND_FAILURE = 11
PARTNER_SENT_TERMINATE = 12
INVALID_PARTNER_MESSAGE = 13
PARTNER_SENT_DEFAULT_RESPONSE_ERROR = 14
BAD_CERTIFICATE_ISSUER = 15
KEY_CONFIRM_FAILURE = 16
BAD_KEY_ESTABLISHMENT_SUITE = 17
KEY_TABLE_FULL = 18
NO_ESTABLISHMENT_ALLOWED = 19
INVALID_CERTIFICATE_KEY_USAGE = 20
}
enum
EMBER_AF_IMAGE_GOOD = 0
EMBER_AF_IMAGE_BAD = 1
EMBER_AF_IMAGE_VERIFY_IN_PROGRESS = 2
}

Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.

enum
EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE = 0x0000
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 = 0x0001
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 = 0x0002
}

CBKE Library types.

enum
UNUSED_PASSWORD = 0x00
SERVICE_PASSWORD = 0x01
CONSUMER_PASSWORD = 0x02
}
enum
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK = 0x01
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK = 0x02
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK = 0x04
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK = 0x08
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK = 0x10
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK = 0x20
}
enum
EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE = 0x00
EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW = 0x01
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS = 0x02
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS = 0x04
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION = 0x08
EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE = 0x40
EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED = 0x80
}

Typedefs#

typedef uint16_t

Refer to the Zigbee application profile ID.

typedef uint16_t

Refer to the ZCL attribute ID.

typedef uint16_t

Refer to the ZCL cluster ID.

typedef uint8_t

Refer to the ZCL attribute type.

typedef uint8_t

User for the cluster mask.

typedef uint8_t

User for the attribute mask.

typedef void(*

Use for either of the cluster functions.

typedef uint64_t
typedef uint8_t

Interpan Message type: unicast, broadcast, or multicast.

typedef uint16_t

The options for sending/receiving interpan messages.

typedef uint8_t

The options for what interpan messages are allowed.

typedef EmberTcLinkKeyRequestPolicy
typedef EmberAppLinkKeyRequestPolicy
typedef uint8_t

Bitmask data type for storing one bit of information for each ESI in the ESI table.

typedef void()
EmberAfServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult *result)

Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.

typedef void()

Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.

typedef void(*

Refer to the handler for network events.

typedef void(*
EmberAfEndpointEventHandler)(uint8_t endpoint)

Refer to the handler for endpoint events.

typedef void(*
EmberAfTickFunction)(uint8_t endpoint)

Refer to the tick callback for cluster.

typedef void(*
EmberAfInitFunction)(uint8_t endpoint)

Refer to the init callback for cluster.

typedef void(*
EmberAfClusterAttributeChangedCallback)(uint8_t endpoint, EmberAfAttributeId attributeId)

Refer to the attribute changed callback function.

typedef void(*
EmberAfManufacturerSpecificClusterAttributeChangedCallback)(uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode)

Refer to the manufacturer-specific attribute changed callback function.

typedef EmberAfStatus(*
EmberAfClusterPreAttributeChangedCallback)(uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value)

Refer to the pre-attribute changed callback function.

typedef void(*
EmberAfDefaultResponseFunction)(uint8_t endpoint, uint8_t commandId, EmberAfStatus status)

Refer to the default response callback function.

typedef void(*
EmberAfMessageSentFunction)(EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status)

Refer to the message sent callback function.

typedef uint16_t

Zigbee Internet Client/Server Remote Cluster Types.

 

Enumeration Documentation#

EmberAfSecurityProfile#

EmberAfSecurityProfile
Enumerator
EMBER_AF_SECURITY_PROFILE_NONE
EMBER_AF_SECURITY_PROFILE_HA
EMBER_AF_SECURITY_PROFILE_HA12
EMBER_AF_SECURITY_PROFILE_SE_TEST
EMBER_AF_SECURITY_PROFILE_SE_FULL
EMBER_AF_SECURITY_PROFILE_Z3
EMBER_AF_SECURITY_PROFILE_CUSTOM

EmberAfServiceDiscoveryStatus#

EmberAfServiceDiscoveryStatus

Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.

Enumerator
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED
EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE

EmberAfEventPollControl#

EmberAfEventPollControl

Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.

Enumerator
EMBER_AF_LONG_POLL
EMBER_AF_SHORT_POLL

EmberAfEventSleepControl#

EmberAfEventSleepControl

Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.

Enumerator
EMBER_AF_OK_TO_SLEEP
EMBER_AF_OK_TO_HIBERNATE

Deprecated.

EMBER_AF_OK_TO_NAP

Deprecated.

EMBER_AF_STAY_AWAKE

EmberAfApplicationTask#

EmberAfApplicationTask

Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.

Some tasks do not necessarily have a response. For example, a ZDO request may or may not have a response. In this case, the application framework cannot rely on the fact that a response will come in to end the wake cycle, so the Application framework must time out the wake cycle if no expected response is received or no other event can be relied upon to end the wake cycle.

Add these types of tasks to the wake timeout mask by calling emberAfSetWakeTimeoutBitmaskCallback so that they can be governed by a timeout instead of a request / response.

The current tasks bitmask is an uint32_t bitmask used to track which tasks are active at any given time. The bottom 16 bits, values 0x01 - 0x8000 are reserved for Ember's use. The top 16 bits are reserved for the customer, values 0x10000 - 0x80000000

Enumerator
EMBER_AF_WAITING_FOR_DATA_ACK
EMBER_AF_LAST_POLL_GOT_DATA
EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY
EMBER_AF_WAITING_FOR_ZDO_RESPONSE
EMBER_AF_WAITING_FOR_ZCL_RESPONSE
EMBER_AF_WAITING_FOR_REGISTRATION
EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE
EMBER_AF_FORCE_SHORT_POLL
EMBER_AF_FRAGMENTATION_IN_PROGRESS
EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY
EMBER_AF_WAITING_FOR_TC_KEY_UPDATE

EmberAfPluginPriceCppAuth#

EmberAfPluginPriceCppAuth

Specifies CPP Authorization values.

Enumerator
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED

EmberAfPluginTunnelingClientStatus#

EmberAfPluginTunnelingClientStatus
Enumerator
EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS
EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY
EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS
EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND
EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT

EmberAfZllCommissioningStatus#

EmberAfZllCommissioningStatus

Status codes used by the ZLL Commissioning plugin.

Enumerator
EMBER_AF_ZLL_ABORTED_BY_APPLICATION
EMBER_AF_ZLL_CHANNEL_CHANGE_FAILED
EMBER_AF_ZLL_JOINING_FAILED
EMBER_AF_ZLL_NO_NETWORKS_FOUND
EMBER_AF_ZLL_PREEMPTED_BY_STACK
EMBER_AF_ZLL_SENDING_START_JOIN_FAILED
EMBER_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED
EMBER_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED
EMBER_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED
EMBER_AF_ZLL_NETWORK_FORMATION_FAILED
EMBER_AF_ZLL_NETWORK_UPDATE_OPERATION

EmberAfImageBlockRequestOptions#

EmberAfImageBlockRequestOptions

The list of options possible for the image block request/response.

Enumerator
EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER
EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST

EmberAfOtaStorageStatus#

EmberAfOtaStorageStatus

Contain the success or error code of an OTA storage device operation.

Enumerator
EMBER_AF_OTA_STORAGE_SUCCESS
EMBER_AF_OTA_STORAGE_ERROR
EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG
EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND
EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS

EmberAfOtaDownloadResult#

EmberAfOtaDownloadResult

Contain the success or error code of an OTA download operation.

Enumerator
EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS
EMBER_AF_OTA_DOWNLOAD_TIME_OUT
EMBER_AF_OTA_VERIFY_FAILED
EMBER_AF_OTA_SERVER_ABORTED
EMBER_AF_OTA_CLIENT_ABORTED
EMBER_AF_OTA_ERASE_FAILED

EmberAfKeyEstablishmentNotifyMessage#

EmberAfKeyEstablishmentNotifyMessage
Enumerator
NO_APP_MESSAGE
RECEIVED_PARTNER_CERTIFICATE
GENERATING_EPHEMERAL_KEYS
GENERATING_SHARED_SECRET
KEY_GENERATION_DONE
GENERATE_SHARED_SECRET_DONE
LINK_KEY_ESTABLISHED

LINK_KEY_ESTABLISHED indicates Success, key establishment done.

NO_LOCAL_RESOURCES

Error codes: Transient failures where Key Establishment could be retried.

PARTNER_NO_RESOURCES
TIMEOUT_OCCURRED
INVALID_APP_COMMAND
MESSAGE_SEND_FAILURE
PARTNER_SENT_TERMINATE
INVALID_PARTNER_MESSAGE
PARTNER_SENT_DEFAULT_RESPONSE_ERROR
BAD_CERTIFICATE_ISSUER

Fatal Errors: These results are not worth retrying because the outcome will not change.

KEY_CONFIRM_FAILURE
BAD_KEY_ESTABLISHMENT_SUITE
KEY_TABLE_FULL
NO_ESTABLISHMENT_ALLOWED

Neither initiator nor responder is an ESP/TC so the key establishment is not allowed per the spec.

INVALID_CERTIFICATE_KEY_USAGE

EmberAfImageVerifyStatus#

EmberAfImageVerifyStatus

Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.

Enumerator
EMBER_AF_IMAGE_GOOD
EMBER_AF_IMAGE_BAD
EMBER_AF_IMAGE_VERIFY_IN_PROGRESS

EmberAfCbkeKeyEstablishmentSuite#

EmberAfCbkeKeyEstablishmentSuite

CBKE Library types.

Enumerator
EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1

EmberAfDeviceManagementPasswordType#

EmberAfDeviceManagementPasswordType
Enumerator
UNUSED_PASSWORD
SERVICE_PASSWORD
CONSUMER_PASSWORD

EmberAfDeviceManagementChangePendingFlags#

EmberAfDeviceManagementChangePendingFlags
Enumerator
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK

EmberAfDeviceDiscoveryStatus#

EmberAfDeviceDiscoveryStatus
Enumerator
EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE
EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION
EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE
EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED

Typedef Documentation#

EmberAfProfileId#

typedef uint16_t EmberAfProfileId

Refer to the Zigbee application profile ID.


EmberAfAttributeId#

typedef uint16_t EmberAfAttributeId

Refer to the ZCL attribute ID.


EmberAfClusterId#

typedef uint16_t EmberAfClusterId

Refer to the ZCL cluster ID.


EmberAfAttributeType#

typedef uint8_t EmberAfAttributeType

Refer to the ZCL attribute type.


EmberAfClusterMask#

typedef uint8_t EmberAfClusterMask

User for the cluster mask.


EmberAfAttributeMask#

typedef uint8_t EmberAfAttributeMask

User for the attribute mask.


EmberAfGenericClusterFunction#

typedef void(* EmberAfGenericClusterFunction) (void) )(void)

Use for either of the cluster functions.

This type is used for the array of the cluster functions and should always be cast into one of the specific functions before being called.


EmberAfDifferenceType#

typedef uint64_t EmberAfDifferenceType

Compare two ZCL attribute values. The size of this data type depends on the platform.


EmberAfInterpanMessageType#

typedef uint8_t EmberAfInterpanMessageType

Interpan Message type: unicast, broadcast, or multicast.


EmberAfInterpanOptions#

typedef uint16_t EmberAfInterpanOptions

The options for sending/receiving interpan messages.


EmberAfAllowedInterpanOptions#

typedef uint8_t EmberAfAllowedInterpanOptions

The options for what interpan messages are allowed.


EmberAfTcLinkKeyRequestPolicy#

typedef EmberTcLinkKeyRequestPolicy EmberAfTcLinkKeyRequestPolicy

EmberAfAppLinkKeyRequestPolicy#

typedef EmberAppLinkKeyRequestPolicy EmberAfAppLinkKeyRequestPolicy

EmberAfPluginEsiManagementBitmask#

typedef uint8_t EmberAfPluginEsiManagementBitmask

Bitmask data type for storing one bit of information for each ESI in the ESI table.


EmberAfServiceDiscoveryCallback#

typedef void() EmberAfServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult *result) (const EmberAfServiceDiscoveryResult *result)

Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.


EmberAfPartnerLinkKeyExchangeCallback#

typedef void() EmberAfPartnerLinkKeyExchangeCallback(bool success) (bool success)

Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.


EmberAfNetworkEventHandler#

typedef void(* EmberAfNetworkEventHandler) (void) )(void)

Refer to the handler for network events.


EmberAfEndpointEventHandler#

typedef void(* EmberAfEndpointEventHandler) (uint8_t endpoint) )(uint8_t endpoint)

Refer to the handler for endpoint events.


EmberAfTickFunction#

typedef void(* EmberAfTickFunction) (uint8_t endpoint) )(uint8_t endpoint)

Refer to the tick callback for cluster.

Tick function will be called once for each tick for each endpoint in the cluster. The rate of tick is determined by the metadata of the cluster.


EmberAfInitFunction#

typedef void(* EmberAfInitFunction) (uint8_t endpoint) )(uint8_t endpoint)

Refer to the init callback for cluster.

Init function is called when the application starts up, once for each cluster/endpoint combination.


EmberAfClusterAttributeChangedCallback#

typedef void(* EmberAfClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId) )(uint8_t endpoint, EmberAfAttributeId attributeId)

Refer to the attribute changed callback function.

This function is called just after an attribute changes.


EmberAfManufacturerSpecificClusterAttributeChangedCallback#

typedef void(* EmberAfManufacturerSpecificClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode) )(uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode)

Refer to the manufacturer-specific attribute changed callback function.

This function is called just after a manufacturer-specific attribute changes.


EmberAfClusterPreAttributeChangedCallback#

typedef EmberAfStatus(* EmberAfClusterPreAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value) )(uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value)

Refer to the pre-attribute changed callback function.

This function is called before an attribute changes.


EmberAfDefaultResponseFunction#

typedef void(* EmberAfDefaultResponseFunction) (uint8_t endpoint, uint8_t commandId, EmberAfStatus status) )(uint8_t endpoint, uint8_t commandId, EmberAfStatus status)

Refer to the default response callback function.

This function is called when default response is received, before the global callback. Global callback is called immediately afterwards.


EmberAfMessageSentFunction#

typedef void(* EmberAfMessageSentFunction) (EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status) )(EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status)

Refer to the message sent callback function.

This function is called when a message is sent.


EmberAfRemoteClusterType#

typedef uint16_t EmberAfRemoteClusterType

Zigbee Internet Client/Server Remote Cluster Types.