Zigbee Over-the-Air Update#
Zigbee OTA Bootload Cluster Server and Client Setup: Describes how to perform a Zigbee over-the-air (OTA) bootload cluster download between a client and server device. The instructions are for devices using an EFR32MG12 development kit. Users can also refer to this procedure when setting up or testing Zigbee OTA bootload cluster download in their own development environments with their own hardware.
Instructions for Using Image Builder: Provides instructions for creating Zigbee Over-the-air (OTA) bootloader files with Image Builder, which takes an existing file (or multiple files) and wraps them in the file format as declared in the Zigbee specification.