Basic node descriptor information.

This is a ZigBee Node Descriptor and contains information about incoming, and outgoing transfer size, as well as descriptor capability.

Public Attribute Documentation#

max_incoming_transfer_size#

uint16_t sl_zigbee_node_descriptor_info_t::max_incoming_transfer_size

The maximum incoming transfer size for the local node


max_outgoing_transfer_size#

uint16_t sl_zigbee_node_descriptor_info_t::max_outgoing_transfer_size

The maximum outgoing transfer size for the local node


capability#

uint8_t sl_zigbee_node_descriptor_info_t::capability

descriptor capability field of the node