Endpoint information (a ZigBee Simple Descriptor).

This is a ZigBee Simple Descriptor and contains information about an endpoint. This information is shared with other nodes in the network by the ZDO.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

profileId#

uint16_t sl_zigbee_endpoint_description_t::profileId

Identifies the endpoint's application profile.


Definition at line 3284 of file stack/include/sl_zigbee_types.h

deviceId#

uint16_t sl_zigbee_endpoint_description_t::deviceId

The endpoint's device ID within the application profile.


Definition at line 3286 of file stack/include/sl_zigbee_types.h

deviceVersion#

uint8_t sl_zigbee_endpoint_description_t::deviceVersion

The endpoint's device version.


Definition at line 3288 of file stack/include/sl_zigbee_types.h

inputClusterCount#

uint8_t sl_zigbee_endpoint_description_t::inputClusterCount

The number of input clusters.


Definition at line 3290 of file stack/include/sl_zigbee_types.h

outputClusterCount#

uint8_t sl_zigbee_endpoint_description_t::outputClusterCount

The number of output clusters.


Definition at line 3292 of file stack/include/sl_zigbee_types.h