User-configurable stack memory allocation defaults.
Note
Application developers should not modify any portion of this file. Doing so may cause mysterious bugs. Allocations should be adjusted only by defining the appropriate macros in the application's CONFIGURATION_HEADER.
See Configuration for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
// Todo:
// - explain how to use a configuration header
// - the documentation of the custom handlers should
// go in config/sl_zigbee_configuration.c, not here
// - the stack profile documentation is out of date
#ifndef SILABS_EMBER_CONFIGURATION_DEFAULTS_H
#define SILABS_EMBER_CONFIGURATION_DEFAULTS_H
#ifdef CONFIGURATION_HEADER
#include CONFIGURATION_HEADER
#endif
#ifdef SL_COMPONENT_CATALOG_PRESENT
#include "sl_component_catalog.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT)
#include "sl_zigbee_green_power_config.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_SECURITY_LINK_KEYS_PRESENT)
#include "sl_zigbee_security_link_keys_config.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_SOURCE_ROUTE_PRESENT)
#include "sl_zigbee_source_route_config.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_DEVICE_CONFIG_PRESENT)
#include "zigbee_device_config.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_PRO_STACK_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_MAC_TEST_CMDS_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_ALT_MAC_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_NON_DEFAULT_MAC_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_RAIL_MUX_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_WITH_HIGH_DATARATE_PHY_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_ROUTER_STACK_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_STACK_WITH_HIGH_DATARATE_PHY_RAIL_MUX)
#include "sl_zigbee_pro_stack_config.h"
#elif defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_WITH_CSL_PRESENT) \
|| defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_MAC_TEST_CMDS_PRESENT)
#include "sl_zigbee_pro_leaf_stack_config.h"
#elif defined(SL_ZIGBEE_SCRIPTED_TEST) || defined(ZAPTEST) || defined(IMAGE_BUILDER) || defined(SLI_ZIGBEE_LIBRARY_BUILD) || defined(EZSP_HOST) || defined(RAIL_MAKE_TEST)
#else
#error "No stack configuration header included"
#endif
#if defined(SL_CATALOG_ZIGBEE_LIGHT_LINK_PRESENT)
#include "sl_zigbee_light_link_config.h"
#endif
#if defined(SL_CATALOG_ZIGBEE_NCP_CONFIGURATION_PRESENT)
#include "ncp-configuration-config.h"
#endif
#ifndef SL_ZIGBEE_API_MAJOR_VERSION
#define SL_ZIGBEE_API_MAJOR_VERSION 2
#endif
#ifndef SL_ZIGBEE_API_MINOR_VERSION
#define SL_ZIGBEE_API_MINOR_VERSION 0
#endif
#ifndef SL_ZIGBEE_STACK_PROFILE
#define SL_ZIGBEE_STACK_PROFILE 0
#endif
#if (SL_ZIGBEE_STACK_PROFILE == 2)
#define SL_ZIGBEE_MAX_DEPTH 15
#define SL_ZIGBEE_SECURITY_LEVEL 5
#define SL_ZIGBEE_MIN_DISCOVERY_TABLE_SIZE 4
#define SL_ZIGBEE_INDIRECT_TRANSMISSION_TIMEOUT 7680
#define SL_ZIGBEE_SEND_MULTICASTS_TO_SLEEPY_ADDRESS false
#ifndef SL_ZIGBEE_MIN_ROUTE_TABLE_SIZE // this value is set to zero on leaf stack
#define SL_ZIGBEE_MIN_ROUTE_TABLE_SIZE 10
#endif
#endif
#ifndef SL_ZIGBEE_STACK_COMPLIANCE_REVISION
#define SL_ZIGBEE_STACK_COMPLIANCE_REVISION 22
#endif
#ifndef SL_ZIGBEE_MAX_END_DEVICE_CHILDREN
#define SL_ZIGBEE_MAX_END_DEVICE_CHILDREN 6
#endif
#ifndef DOXYGEN_SHOULD_SKIP_THIS
/* Need to put in a compile time check to make sure that too many child devices
* aren't specified.
*/
#if SL_ZIGBEE_MAX_END_DEVICE_CHILDREN > 64
#error "SL_ZIGBEE_MAX_END_DEVICE_CHILDREN can not exceed 64."
#endif
#endif // DOXYGEN_SHOULD_SKIP_THIS
#ifndef SL_ZIGBEE_SECURITY_LEVEL
#define SL_ZIGBEE_SECURITY_LEVEL 5
#endif
#if !(SL_ZIGBEE_SECURITY_LEVEL == 0 \
|| SL_ZIGBEE_SECURITY_LEVEL == 5)
#error "Unsupported security level"
#endif
#ifdef SL_ZIGBEE_CHILD_TABLE_SIZE
#if (SL_ZIGBEE_MAX_END_DEVICE_CHILDREN < SL_ZIGBEE_CHILD_TABLE_SIZE)
#undef SL_ZIGBEE_CHILD_TABLE_SIZE
#endif
#endif
#ifndef SL_ZIGBEE_CHILD_TABLE_SIZE
#define SL_ZIGBEE_CHILD_TABLE_SIZE SL_ZIGBEE_MAX_END_DEVICE_CHILDREN
#endif
#ifndef SL_ZIGBEE_KEY_TABLE_SIZE
#define SL_ZIGBEE_KEY_TABLE_SIZE 0
#endif
#ifndef SL_ZIGBEE_CERTIFICATE_TABLE_SIZE
#define SL_ZIGBEE_CERTIFICATE_TABLE_SIZE 0
#else
#if SL_ZIGBEE_CERTIFICATE_TABLE_SIZE > 1
#error "SL_ZIGBEE_CERTIFICATE_TABLE_SIZE > 1 is not supported!"
#endif
#endif
#ifndef SL_ZIGBEE_MAX_DEPTH
#define SL_ZIGBEE_MAX_DEPTH 15
#elif (SL_ZIGBEE_MAX_DEPTH > 15)
// Depth is a 4-bit field
#error "SL_ZIGBEE_MAX_DEPTH cannot be greater than 15"
#endif
#ifndef SL_ZIGBEE_MAX_HOPS
#define SL_ZIGBEE_MAX_HOPS (2 * SL_ZIGBEE_MAX_DEPTH)
#endif
#ifndef SL_ZIGBEE_PACKET_BUFFER_HEAP_SIZE
#define SL_ZIGBEE_PACKET_BUFFER_HEAP_SIZE 4096
#endif // SL_ZIGBEE_PACKET_BUFFER_HEAP_SIZE
#ifndef SL_ZIGBEE_MAX_BEACONS_TO_STORE
// Packet buffers can be maxed out and we dont necessarily want to cache all those
// many beacons. Cap number of beacons to a reasonable size based on buffer heap configuration
// NOTE 2048 is the 'small' packet buffer heap size
#define SL_ZIGBEE_MAX_BEACONS_TO_STORE ( (SL_ZIGBEE_PACKET_BUFFER_HEAP_SIZE <= 2048) ? 18 : 37)
#endif
#ifndef BEACON_STORAGE_TIMEOUT_MS
#define BEACON_STORAGE_TIMEOUT_MS (3 * 60 * 1000) // 3 minutes
#endif
#define SL_ZIGBEE_MAX_NEIGHBOR_TABLE_SIZE 26
#ifndef SL_ZIGBEE_NEIGHBOR_TABLE_SIZE
#define SL_ZIGBEE_NEIGHBOR_TABLE_SIZE 16
#endif
#if (SL_ZIGBEE_NEIGHBOR_TABLE_SIZE != SL_ZIGBEE_MAX_NEIGHBOR_TABLE_SIZE) && (SL_ZIGBEE_NEIGHBOR_TABLE_SIZE != 16) && (SL_ZIGBEE_NEIGHBOR_TABLE_SIZE != 1)
#error "Unsupported neighbor table size is configured. Supported values are 1, 16 and 26."
#endif
#ifndef SL_ZIGBEE_INDIRECT_TRANSMISSION_TIMEOUT
#define SL_ZIGBEE_INDIRECT_TRANSMISSION_TIMEOUT 3000
#endif
#define SL_ZIGBEE_MAX_INDIRECT_TRANSMISSION_TIMEOUT 30000
#if (SL_ZIGBEE_INDIRECT_TRANSMISSION_TIMEOUT \
> SL_ZIGBEE_MAX_INDIRECT_TRANSMISSION_TIMEOUT)
#error "Indirect transmission timeout too large."
#endif
#ifndef SL_ZIGBEE_SEND_MULTICASTS_TO_SLEEPY_ADDRESS
#define SL_ZIGBEE_SEND_MULTICASTS_TO_SLEEPY_ADDRESS false
#endif
/* @brief End Device keep alive support mode
*/
#ifndef SL_ZIGBEE_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE
#define SL_ZIGBEE_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE SL_ZIGBEE_KEEP_ALIVE_SUPPORT_ALL
#endif
#define SECONDS_10 0
#define MINUTES_2 1
#define MINUTES_4 2
#define MINUTES_8 3
#define MINUTES_16 4
#define MINUTES_32 5
#define MINUTES_64 6
#define MINUTES_128 7
#define MINUTES_256 8
#define MINUTES_512 9
#define MINUTES_1024 10
#define MINUTES_2048 11
#define MINUTES_4096 12
#define MINUTES_8192 13
#define MINUTES_16384 14
#ifndef SL_ZIGBEE_END_DEVICE_POLL_TIMEOUT
#define SL_ZIGBEE_END_DEVICE_POLL_TIMEOUT MINUTES_256
#endif
#ifndef SL_ZIGBEE_SHORT_CHILD_TIMEOUT
#if (SL_ZIGBEE_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
#define SL_ZIGBEE_SHORT_CHILD_TIMEOUT SECONDS_10
#else // (SL_ZIGBEE_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
#define SL_ZIGBEE_SHORT_CHILD_TIMEOUT MINUTES_2
#endif // (SL_ZIGBEE_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
#endif // SL_ZIGBEE_SHORT_CHILD_TIMEOUT
#ifndef SL_ZIGBEE_LINK_POWER_DELTA_INTERVAL
#define SL_ZIGBEE_LINK_POWER_DELTA_INTERVAL 300
#endif
#ifndef SL_ZIGBEE_APS_UNICAST_MESSAGE_COUNT
#define SL_ZIGBEE_APS_UNICAST_MESSAGE_COUNT 10
#endif
#ifndef SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES
// NOTE a size of 1 is basically the same thing as no duplicate rejection
#define SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES 5
#endif
#ifndef SL_ZIGBEE_BINDING_TABLE_SIZE
#define SL_ZIGBEE_BINDING_TABLE_SIZE 0
#endif
#ifndef SL_ZIGBEE_ADDRESS_TABLE_SIZE
#define SL_ZIGBEE_ADDRESS_TABLE_SIZE 8
#endif
#ifndef SL_ZIGBEE_ROUTE_TABLE_SIZE //in leaf stack this value is defined to be 0
#define SL_ZIGBEE_ROUTE_TABLE_SIZE 16
#elif defined(SL_ZIGBEE_MIN_ROUTE_TABLE_SIZE) \
&& SL_ZIGBEE_ROUTE_TABLE_SIZE < SL_ZIGBEE_MIN_ROUTE_TABLE_SIZE
#error "SL_ZIGBEE_ROUTE_TABLE_SIZE is less than required by stack profile."
#endif
#ifndef SL_ZIGBEE_DISCOVERY_TABLE_SIZE
#ifdef SL_ZIGBEE_MIN_DISCOVERY_TABLE_SIZE
#define SL_ZIGBEE_DISCOVERY_TABLE_SIZE SL_ZIGBEE_MIN_DISCOVERY_TABLE_SIZE
#else
#define SL_ZIGBEE_DISCOVERY_TABLE_SIZE 8
#endif
#elif defined(SL_ZIGBEE_MIN_DISCOVERY_TABLE_SIZE) \
&& SL_ZIGBEE_DISCOVERY_TABLE_SIZE < SL_ZIGBEE_MIN_DISCOVERY_TABLE_SIZE
#error "SL_ZIGBEE_DISCOVERY_TABLE_SIZE is less than required by stack profile."
#endif
#ifndef SL_ZIGBEE_MULTICAST_TABLE_SIZE
#define SL_ZIGBEE_MULTICAST_TABLE_SIZE 8
#endif
#ifndef SL_ZIGBEE_SOURCE_ROUTE_TABLE_SIZE
#define SL_ZIGBEE_SOURCE_ROUTE_TABLE_SIZE 0
#endif
#ifndef SL_ZIGBEE_MAX_SOURCE_ROUTE_RELAY_COUNT
#define SL_ZIGBEE_MAX_SOURCE_ROUTE_RELAY_COUNT 11
#endif
/* The minimum broadcast table size per the Zigbee Pro spec is 9. */
#define SL_ZIGBEE_DEFAULT_BROADCAST_TABLE_SIZE 15
#ifndef SL_ZIGBEE_BROADCAST_TABLE_SIZE
#define SL_ZIGBEE_BROADCAST_TABLE_SIZE SL_ZIGBEE_DEFAULT_BROADCAST_TABLE_SIZE
#elif SL_ZIGBEE_BROADCAST_TABLE_SIZE < SL_ZIGBEE_DEFAULT_BROADCAST_TABLE_SIZE
#error "SL_ZIGBEE_BROADCAST_TABLE_SIZE is less than the minimum value of 15."
#elif 254 < SL_ZIGBEE_BROADCAST_TABLE_SIZE
#error "SL_ZIGBEE_BROADCAST_TABLE_SIZE is larger than the maximum value of 254."
#endif
#ifndef SL_ZIGBEE_RETRY_QUEUE_SIZE
#define SL_ZIGBEE_RETRY_QUEUE_SIZE 16
#endif
#ifndef SL_ZIGBEE_STORE_AND_FORWARD_QUEUE_SIZE
#define SL_ZIGBEE_STORE_AND_FORWARD_QUEUE_SIZE 5
#endif
#if !defined(SL_ZIGBEE_ASSERT_OUTPUT_DISABLED) \
&& !defined(SL_ZIGBEE_ASSERT_SERIAL_PORT)
#define SL_ZIGBEE_ASSERT_SERIAL_PORT 1
#endif
#ifndef SL_ZIGBEE_FRAGMENT_DELAY_MS
#define SL_ZIGBEE_FRAGMENT_DELAY_MS 0
#endif
#define SL_ZIGBEE_FRAGMENT_MAX_WINDOW_SIZE 8
#ifndef SL_ZIGBEE_FRAGMENT_WINDOW_SIZE
#define SL_ZIGBEE_FRAGMENT_WINDOW_SIZE 1
#elif SL_ZIGBEE_FRAGMENT_MAX_WINDOW_SIZE < SL_ZIGBEE_FRAGMENT_WINDOW_SIZE
#error "SL_ZIGBEE_FRAGMENT_WINDOW_SIZE is too large."
#endif
#ifndef SL_ZIGBEE_REQUEST_KEY_TIMEOUT
#define SL_ZIGBEE_REQUEST_KEY_TIMEOUT 0
#elif SL_ZIGBEE_REQUEST_KEY_TIMEOUT > 10
#error "SL_ZIGBEE_REQUEST_KEY_TIMEOUT is too large."
#endif
#ifndef SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S
#define SL_ZIGBEE_TRANSIENT_KEY_TIMEOUT_S (300)
#endif
#ifndef SL_ZIGBEE_TRANSIENT_KEY_SESSION_TIMEOUT_VAL
#define SL_ZIGBEE_TRANSIENT_KEY_SESSION_TIMEOUT_VAL 0xFFFF
#endif
#ifndef SL_ZIGBEE_PAN_ID_CONFLICT_REPORT_THRESHOLD
#define SL_ZIGBEE_PAN_ID_CONFLICT_REPORT_THRESHOLD 2
#endif
#define SL_ZIGBEE_MAX_NETWORK_RETRIES 15
#ifndef SL_ZIGBEE_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT
#define SL_ZIGBEE_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT 15
#endif
#if (SL_ZIGBEE_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT > SL_ZIGBEE_MAX_NETWORK_RETRIES)
#error "Unsupported network retry attempts is configured. Supported values are 0..15"
#endif
#ifndef SL_ZIGBEE_TASK_COUNT
#define SL_ZIGBEE_TASK_COUNT (5)
#endif
#define SL_ZIGBEE_MAX_SUPPORTED_NETWORKS 2
#ifdef UC_BUILD
#if (SLI_ZIGBEE_SECONDARY_NETWORK_ENABLED == 0)
#define SL_ZIGBEE_SUPPORTED_NETWORKS 1
#else
#define SL_ZIGBEE_SUPPORTED_NETWORKS 2
#endif
#if (defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT) \
&& (defined(SL_CATALOG_ZIGBEE_MULTI_PAN_PRESENT) || defined(SL_CATALOG_ZIGBEE_MULTI_NETWORK_PRESENT)))
#undef SL_ZIGBEE_SUPPORTED_NETWORKS
#define SL_ZIGBEE_SUPPORTED_NETWORKS 2
#endif
#else // !UC_BUILD
#ifndef SL_ZIGBEE_SUPPORTED_NETWORKS
#ifdef SL_ZIGBEE_TEST
#define SL_ZIGBEE_SUPPORTED_NETWORKS 2
#else
#define SL_ZIGBEE_SUPPORTED_NETWORKS 1
#endif
#endif
#endif // UC_BUILD
#ifndef SL_ZIGBEE_ZLL_GROUP_ADDRESSES
#define SL_ZIGBEE_ZLL_GROUP_ADDRESSES 1
#endif
#ifndef SL_ZIGBEE_ZLL_RSSI_THRESHOLD
#define SL_ZIGBEE_ZLL_RSSI_THRESHOLD -128
#endif
#ifndef EZSP_HOST
#ifndef SL_ZIGBEE_GP_PROXY_TABLE_SIZE
#define SL_ZIGBEE_GP_PROXY_TABLE_SIZE 5
#endif
#ifndef SL_ZIGBEE_GP_SINK_TABLE_SIZE
#define SL_ZIGBEE_GP_SINK_TABLE_SIZE 0
#endif
#endif //EZSP_HOST
#ifndef SL_ZIGBEE_GP_INCOMING_FC_TOKEN_TIMEOUT
#define SL_ZIGBEE_GP_INCOMING_FC_TOKEN_TIMEOUT 7 // between 0 seconds (never) to 60 seconds
#endif
#ifndef SL_ZIGBEE_GP_INCOMING_FC_TOKEN_TABLE_SIZE
#define SL_ZIGBEE_GP_INCOMING_FC_TOKEN_TABLE_SIZE 0 //SL_ZIGBEE_GP_PROXY_TABLE_SIZE
#endif
#ifndef SL_ZIGBEE_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT
#define SL_ZIGBEE_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT 7 // between 0 seconds (never) to 60 seconds
#endif
#ifndef SL_ZIGBEE_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE
#define SL_ZIGBEE_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE 0 //SL_ZIGBEE_GP_SINK_TABLE_SIZE
#endif
#define SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED 2
#if SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED > SL_ZIGBEE_SUPPORTED_NETWORKS
#undef SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED
#define SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED SL_ZIGBEE_SUPPORTED_NETWORKS
#endif
#ifdef UC_BUILD
#if (SLI_ZIGBEE_PRIMARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_COORDINATOR_OR_ROUTER \
|| SLI_ZIGBEE_PRIMARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_ROUTER)
// Primary network is coordinator or router
#define NETWORK_0_ZC_AND_ZR_COUNT (1)
#else
// Primary network is end device
#define NETWORK_0_ZC_AND_ZR_COUNT (0)
#endif
#if (SLI_ZIGBEE_SECONDARY_NETWORK_ENABLED > 0 \
&& (SLI_ZIGBEE_SECONDARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_COORDINATOR_OR_ROUTER \
|| SLI_ZIGBEE_SECONDARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_ROUTER))
// Secondary network is coordinator or router
#define NETWORK_1_ZC_AND_ZR_COUNT (1)
#else
// Secondary network not enabled or it is end device
#define NETWORK_1_ZC_AND_ZR_COUNT (0)
#endif
// Handle the NCP Multi pan case and set the SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT to 2
#if defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT) && defined(SL_CATALOG_ZIGBEE_MULTI_PAN_PRESENT)
#undef SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT
#define SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT 2
#elif (defined(SL_ZIGBEE_NO_STACK) && !defined(SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT))
// For no stack application such nodetest/sniffer.
#define SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT (1)
#else
#define SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT (NETWORK_0_ZC_AND_ZR_COUNT + NETWORK_1_ZC_AND_ZR_COUNT)
#endif
#if (SL_ZIGBEE_ZC_AND_ZR_DEVICE_COUNT > SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED)
#error "Exceeded the maximum number of supported ZC and ZR devices."
#endif
#else // !UC_BUILD
#if defined(SL_ZIGBEE_AF_NCP) && defined(EMBER_AF_PLUGIN_MULTI_PAN_LIBRARY)
#undef SL_ZIGBEE_AF_ZC_AND_ZR_DEVICE_COUNT // ToDo: Remove #if part, would not need it with UC apps.
#define SL_ZIGBEE_AF_ZC_AND_ZR_DEVICE_COUNT 2 // For Multi-PAN NCP
#elif defined(SL_ZIGBEE_NO_STACK) && !defined(SL_ZIGBEE_AF_ZC_AND_ZR_DEVICE_COUNT)
// For no stack application such nodetest/sniffer.
#define SL_ZIGBEE_AF_ZC_AND_ZR_DEVICE_COUNT 1
#endif
#if (SL_ZIGBEE_AF_ZC_AND_ZR_DEVICE_COUNT > SL_ZIGBEE_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED)
#error "Exceeded the maximum number of supported ZC and ZR devices."
#endif
#endif // UC_BUILD
// This table temporarily keeps track of devices that are joining
// To allow "n" devices to join simulataneously, this table needs to be capable of
// holding n entries. Since this space is only used when necessary and times out fairly
// quickly, we set it to 64 (same as max child table size) to prevent all the additional
// code to allow configuration of this table size
#ifndef SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY
#define SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY 64
#endif
#ifndef SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS
#ifdef SL_CATALOG_ZIGBEE_DELAYED_JOIN_PRESENT
#define SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS (65535u)
#define SL_ZIGBEE_TRANSIENT_DEVICE_MINIMUM_TIMEOUT_MS (10000u)
#else
#define SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS (10000u)
#endif
#endif
//Allows the aps acks for APSME commands to be turned off or on
//This should be "true" by default but to keep it consistend with the current stack behaviour this is "false" by default.
#ifndef SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS
#define SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS (false)
#endif
#ifndef SL_ZIGBEE_CUSTOM_MAC_FILTER_TABLE_SIZE
#define SL_ZIGBEE_CUSTOM_MAC_FILTER_TABLE_SIZE 2
#endif
#ifdef SL_CATALOG_RAIL_LIB_PRESENT
#include "rail_ieee802154.h"
#ifndef SL_ZIGBEE_RADIO_802154_CCA_MODE
#define SL_ZIGBEE_RADIO_802154_CCA_MODE RAIL_IEEE802154_CCA_MODE_RSSI
#endif // SL_ZIGBEE_RADIO_802154_CCA_MODE
#endif // SL_CATALOG_RAIL_LIB_PRESENT
#if defined(SL_ZIGBEE_TEST) || defined(ZIGBEE_STACK_ON_HOST)
#undef SL_ZIGBEE_RADIO_802154_CCA_MODE
#define SL_ZIGBEE_RADIO_802154_CCA_MODE 0
#endif
#ifndef SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS
#define SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS 8
#endif
#endif //__EMBER_CONFIGURATION_DEFAULTS_H__
Macros#
The major version number of the Ember stack release that the application is built against.
The minor version number of the Ember stack release that the application is built against.
Specify the stack profile. The default is Profile 0.
The maximum number of end device children that a router will support.
The security level used for security at the MAC and network layers. The supported values are 0 (no security) and 5 (payload is encrypted and a four-byte MIC is used for authentication).
The maximum number of children that a node may have.
The maximum number of link and master keys that a node can store, not including the Trust Center Link Key. The stack maintains special storage for the Trust Center Link Key.
The number of entries for the field upgradeable certificate table. Normally, certificates, such as SE certs, are stored in the runtime-unmodifiable MFG area. However, those devices wishing to add new certificates after manufacturing will have to use the normal token space. This defines the size of that table. For most devices 0 is appropriate since there is no need to change certificates in the field. For those wishing to field upgrade devices with new certificates, 1 is the correct size. Anything more is wasting storage.
The maximum depth of the tree in ZigBee 2006. This implicitly determines the maximum diameter of the network (SL_ZIGBEE_MAX_HOPS) if that value is not overridden.
The maximum number of hops for a message.
The amount of memory to allocate for Packet Buffers available to the stack the default is 4096.
The maximum number of beacons to record when performing an active scan to find networks. Legacy APIs such as sli_zigbee_stack_join_network and the several sli_zigbee_stack_find_and_rejoin_network APIs set the number of beacons to record to 1, while the Network Steering plugin will attempt to record the maximum number of beacons.
The amount of time after which any caches beacons are purged from the cache in RAM. Each beacon stored consumes one packet buffer. The timeout for beacons begins once the first beacon is added to the cache.
The maximum number of router neighbors the stack can keep track of.
The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child.
Define the behavior for the address that the multicasts are sent to. The normal address is RxOnWhenIdle=true (0xFFFD). However, setting this to true can change locally generated multicasts to be sent to the sleepy broadcast address (0xFFFF). Changing the default is NOT Zigbee Pro compliant and may not be inter-operable.
The default index into the R21 Child Aging timeout The default value is a timeout of 256 minutes.
The temporary, short timeout that is given to a joining or insecurely rejoining child. The child is expected to send a network encrypted packet to set its timeout to the default value.
The maximum number of APS retried messages that the stack can transmit at any time. Here, transmitting describes the time between the call to ::sli_zigbee_stack_send_unicast() and the subsequent callback to ::sli_zigbee_stack_message_sent_handler().
Size of 1 is basically the same thing as no duplicate rejection.
The maximum number of bindings supported by the stack. The default is 0 bindings. Each binding consumes 2 bytes of RAM.
The maximum number of EUI64<->network address associations that the stack can maintain. The default value is 8.
The maximum number of destinations to which a node can route messages. This include both messages originating at this node and those relayed for others. The default value is 16.
The number of simultaneous route discoveries that a node will support.
The maximum number of multicast groups that the device may be a member of. The default value is 8.
The number of source route table entries if the source route library is not included. The maximum source route table size is 255 entries, since a one-byte index is used, and the index 0xFF is reserved. The default value is 0.
The maximum number of broadcasts during a single broadcast timeout period. The minimum and default value is 15 and can only be changed on compatible Ember stacks. Be very careful when changing the broadcast table size as it affects timing of the broadcasts and the number of possible broadcasts. Additionally, this value must be universal for all devices in the network. Otherwise, a single router can overwhelm all its neighbors with more broadcasts than they can support. In general, this value should be left alone.
Settings to control if and where assert information will be printed.
The time the stack will wait (in milliseconds) between sending blocks of a fragmented message. The default value is 0.
The maximum number of blocks of a fragmented message that can be sent in a single window is defined to be 8.
The number of blocks of a fragmented message that can be sent in a single window. The maximum is SL_ZIGBEE_FRAGMENT_MAX_WINDOW_SIZE. The default value is 1.
The length of time that the device will wait for an answer to its Application Key Request. For the Trust Center, this is the time it will hold the first request and wait for a second matching request. If both arrive within this time period, the Trust Center will reply to both with the new key. If both requests are not received, the Trust Center will discard the request. The time is in minutes, with the maximum time being 10 minutes. A value of 0 minutes indicates that the Trust Center will not buffer the request but instead respond immediately. Only 1 outstanding request is supported at a time.
The length of time, in seconds, that a trust center will store a transient link key that a device can use to join its network. A transient key is added with a call to sli_zigbee_stack_sec_man_import_transient_key. After the transient key is added, it will be removed once this amount of time has passed. A joining device will not be able to use that key to join until it is added again on the trust center. The default value is 300 seconds, i.e., 5 minutes.
A reserved transient key timeout value that, when stored with a "transient" key, prevents its removal from the transient key table when the session is active. Note that some standard security procedures (e.g. Zigbee Direct) require session keys to remain active indefinitely for the duration of the of the exchange.
The number of PAN ID conflict reports that must be received by the network manager within one minute to trigger a PAN ID change. Very rarely, a corrupt beacon can pass the CRC check and trigger a false PAN id conflict. This is more likely to happen in very large dense networks. Setting this value to 2 or 3 dramatically reduces the chances of a spurious PAN ID change. The maximum value is 63. The default value is 2.
The number of network level retries before network layer gives up sending a message, and return with an error. This could be seen as an extension to mac retries, and can take a range between 0..15. Setting the value to 0 disables network retries.
The number of event tasks that can be tracked for the purpose of processor idling. The Ember Zigbee Pro Stack requires two tasks, an application and associated libraries may use additional tasks, though typically no more than 5 are needed for most applications.
The number of networks supported by the stack.
The number of unique group identifiers that this device requires.
The RSSI threshold applied to incoming scan requests.
The number of proxy table entries supported. Only on SoC images.
The number of sink table entries supported. Only on SoC images.
The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).
The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or SL_ZIGBEE_GP_PROXY_TABLE_SIZE).
The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).
The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or SL_ZIGBEE_GP_SINK_TABLE_SIZE).
The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.
The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.
The number of ZC and ZR device types are present in the application. This configuration is used to expand the various stack tables and events required to support the multi PAN application. Note that for SoC, this define is generated by app builder based on the device type(s) present in the application.
The 802.15.4 CCA mode that should be used at startup. The default value is RAIL_IEEE802154_CCA_MODE_RSSI. This value is configured in the radio during initialization. The user may override this value at runtime using ::sli_zigbee_stack_set_radio_ieee802154_cca_mode.