Ember data type definitions.
See Ember ZigBee Light Link (ZLL) Data Types for details.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_ZLL_TYPES_H
#define SILABS_ZLL_TYPES_H
#include "stack/include/sl_zigbee_types.h"
#define SL_ZIGBEE_ZLL_PRIMARY_CHANNEL_MASK ((uint32_t)(BIT32(11)   \
                                                       | BIT32(15) \
                                                       | BIT32(20) \
                                                       | BIT32(25)))
#define SL_ZIGBEE_ZLL_SECONDARY_CHANNEL_MASK ((uint32_t)(BIT32(12)   \
                                                         | BIT32(13) \
                                                         | BIT32(14) \
                                                         | BIT32(16) \
                                                         | BIT32(17) \
                                                         | BIT32(18) \
                                                         | BIT32(19) \
                                                         | BIT32(21) \
                                                         | BIT32(22) \
                                                         | BIT32(23) \
                                                         | BIT32(24) \
                                                         | BIT32(26)))
#define SL_ZIGBEE_ZLL_NULL_NODE_ID 0x0000
#define SL_ZIGBEE_ZLL_MIN_NODE_ID 0x0001
#define SL_ZIGBEE_ZLL_MAX_NODE_ID 0xFFF7
#define SL_ZIGBEE_ZLL_NULL_GROUP_ID 0x0000
#define SL_ZIGBEE_ZLL_MIN_GROUP_ID 0x0001
#define SL_ZIGBEE_ZLL_MAX_GROUP_ID 0xFEFF
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_zll_state_t
#else
typedef uint16_t sl_zigbee_zll_state_t;
enum
#endif
{
  SL_ZIGBEE_ZLL_STATE_NONE                       = 0x0000,
  SL_ZIGBEE_ZLL_STATE_FACTORY_NEW                = 0x0001,
  SL_ZIGBEE_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE = 0x0002,
  SL_ZIGBEE_ZLL_STATE_LINK_INITIATOR             = 0x0010,
  SL_ZIGBEE_ZLL_STATE_LINK_PRIORITY_REQUEST      = 0x0020,
  SL_ZIGBEE_ZLL_STATE_PROFILE_INTEROP            = 0x0080,
  SL_ZIGBEE_ZLL_STATE_NON_ZLL_NETWORK            = 0x0100,
  SL_ZIGBEE_ZLL_TOKEN_POINTS_TO_PSA_ID           = 0x0200,
};
typedef struct {
  uint32_t transactionId;
  uint32_t responseId;
  uint16_t bitmask;
} sl_zigbee_zll_security_algorithm_data_t;
typedef struct {
  sl_zigbee_zigbee_network_t zigbeeNetwork;
  sl_zigbee_zll_security_algorithm_data_t securityAlgorithm;
  sl_802154_long_addr_t eui64;
  sl_802154_short_addr_t nodeId;
  sl_zigbee_zll_state_t state;
  sl_zigbee_node_type_t nodeType;
  uint8_t numberSubDevices;
  uint8_t totalGroupIdentifiers;
  uint8_t rssiCorrection;
} sl_zigbee_zll_network_t;
typedef struct {
  sl_802154_long_addr_t ieeeAddress;
  uint8_t endpointId;
  uint16_t profileId;
  uint16_t deviceId;
  uint8_t version;
  uint8_t groupIdCount;
} sl_zigbee_zll_device_info_record_t;
typedef struct {
  sl_802154_short_addr_t nodeId;
  sl_802154_short_addr_t freeNodeIdMin;
  sl_802154_short_addr_t freeNodeIdMax;
  sl_zigbee_multicast_id_t groupIdMin;
  sl_zigbee_multicast_id_t groupIdMax;
  sl_zigbee_multicast_id_t freeGroupIdMin;
  sl_zigbee_multicast_id_t freeGroupIdMax;
} sl_zigbee_zll_address_assignment_t;
#define SL_ZIGBEE_ZLL_CLUSTER_ID 0x1000
#define SL_ZIGBEE_ZLL_PROFILE_ID 0xC05E
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_zll_key_index_t
#else
typedef uint8_t sl_zigbee_zll_key_index_t;
enum
#endif
{
  SL_ZIGBEE_ZLL_KEY_INDEX_DEVELOPMENT   = 0x00,
  SL_ZIGBEE_ZLL_KEY_INDEX_MASTER        = 0x04,
  SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION = 0x0F,
};
#define SL_ZIGBEE_ZLL_KEY_MASK_DEVELOPMENT (1 << SL_ZIGBEE_ZLL_KEY_INDEX_DEVELOPMENT)
#define SL_ZIGBEE_ZLL_KEY_MASK_MASTER (1 << SL_ZIGBEE_ZLL_KEY_INDEX_MASTER)
#define SL_ZIGBEE_ZLL_KEY_MASK_CERTIFICATION (1 << SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION)
#define SL_ZIGBEE_ZLL_CERTIFICATION_ENCRYPTION_KEY  \
  { 0xC0, 0xC1, 0xC2, 0xC3, 0xC4, 0xC5, 0xC6, 0xC7, \
    0xC8, 0xC9, 0xCA, 0xCB, 0xCC, 0xCD, 0xCE, 0xCF }
#define SL_ZIGBEE_ZLL_CERTIFICATION_PRECONFIGURED_LINK_KEY \
  { 0xD0, 0xD1, 0xD2, 0xD3, 0xD4, 0xD5, 0xD6, 0xD7,        \
    0xD8, 0xD9, 0xDA, 0xDB, 0xDC, 0xDD, 0xDE, 0xDF }
typedef struct {
  uint32_t bitmask;
  sl_zigbee_zll_key_index_t keyIndex;
  sl_zigbee_key_data_t encryptionKey;
  sl_zigbee_key_data_t preconfiguredKey;
} sl_zigbee_zll_initial_security_state_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_zll_policy_t
#else
typedef uint8_t sl_zigbee_zll_policy_t;
enum
#endif
{
  SL_ZIGBEE_ZLL_POLICY_DISABLED = 0x00,
  SL_ZIGBEE_ZLL_POLICY_ENABLED = 0x01,
  SL_ZIGBEE_ZLL_POLICY_TARGET = 0x02,
  SL_ZIGBEE_ZLL_POLICY_STEALING_ENABLED = 0x04,
  SL_ZIGBEE_ZLL_POLICY_REMOTE_RESET_ENABLED = 0x08,
};
typedef struct {
  uint32_t bitmask;
  uint16_t freeNodeIdMin;
  uint16_t freeNodeIdMax;
  uint16_t myGroupIdMin;
  uint16_t freeGroupIdMin;
  uint16_t freeGroupIdMax;
  uint8_t rssiCorrection;
} sl_zigbee_tok_type_stack_zll_data_t;
typedef struct {
  uint32_t bitmask;
  uint8_t keyIndex;
  uint8_t encryptionKey[SL_ZIGBEE_ENCRYPTION_KEY_SIZE];
  uint8_t preconfiguredKey[SL_ZIGBEE_ENCRYPTION_KEY_SIZE];
} sl_zigbee_tok_type_stack_zll_security_t;
#endif // SILABS_ZLL_TYPES_H
Modules#
sl_zigbee_zll_security_algorithm_data_t
sl_zigbee_zll_device_info_record_t
sl_zigbee_zll_address_assignment_t
sl_zigbee_zll_initial_security_state_t
sl_zigbee_tok_type_stack_zll_data_t
sl_zigbee_tok_type_stack_zll_security_t
ZigBee Light Link Types#
The list of primary ZLL channels.
The list of secondary ZLL channels.
A distinguished network identifier in the ZLL network address space that indicates no free network identifiers were assigned to the device.
The minimum network identifier in the ZLL network address space.
The maximum network identifier in the ZLL network address space.
A distinguished group identifier in the ZLL group address space that indicates no free group identifiers were assigned to the device.
The minimum group identifier in the ZLL group address space.
The maximum group identifier in the ZLL group address space.
The ZigBee Light Link Commissioning cluster ID.
The ZigBee Light Link Profile ID.
The key encryption bitmask corresponding to encryption key index SL_ZIGBEE_ZLL_KEY_INDEX_DEVELOPMENT.
The key encryption bitmask corresponding to encryption key index SL_ZIGBEE_ZLL_KEY_INDEX_MASTER.
THe key encryption bitmask corresponding to encryption key index SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION.
The encryption key for use during development and certification in conjunction with SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION.
The pre-configured link key for use during development and certification in conjunction with SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION.
A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.
The key encryption algorithms supported by the stack.
This enumeration indicates whether or not the stack processes ZLL messages.
ZigBee Light Link Types Documentation#
sl_zigbee_zll_state_t#
sl_zigbee_zll_state_t
A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.
| Enumerator | |
|---|---|
| SL_ZIGBEE_ZLL_STATE_NONE | No state.  | 
| SL_ZIGBEE_ZLL_STATE_FACTORY_NEW | The device is factory new.  | 
| SL_ZIGBEE_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE | The device is capable of assigning addresses to other devices.  | 
| SL_ZIGBEE_ZLL_STATE_LINK_INITIATOR | The device is initiating a link operation.  | 
| SL_ZIGBEE_ZLL_STATE_LINK_PRIORITY_REQUEST | The device is requesting link priority.  | 
| SL_ZIGBEE_ZLL_STATE_PROFILE_INTEROP | The device is a ZigBee 3.0 device.  | 
| SL_ZIGBEE_ZLL_STATE_NON_ZLL_NETWORK | The device is on a non-ZLL network.  | 
| SL_ZIGBEE_ZLL_TOKEN_POINTS_TO_PSA_ID | Internal use: the ZLL token's key values point to a PSA key identifier  | 
sl_zigbee_zll_key_index_t#
sl_zigbee_zll_key_index_t
The key encryption algorithms supported by the stack.
| Enumerator | |
|---|---|
| SL_ZIGBEE_ZLL_KEY_INDEX_DEVELOPMENT | The key encryption algorithm for use during development.  | 
| SL_ZIGBEE_ZLL_KEY_INDEX_MASTER | The key encryption algorithm shared by all certified devices.  | 
| SL_ZIGBEE_ZLL_KEY_INDEX_CERTIFICATION | The key encryption algorithm for use during development and certification.  | 
sl_zigbee_zll_policy_t#
sl_zigbee_zll_policy_t
This enumeration indicates whether or not the stack processes ZLL messages.
| Enumerator | |
|---|---|
| SL_ZIGBEE_ZLL_POLICY_DISABLED | Initial state - all touchlinking is disabled.  | 
| SL_ZIGBEE_ZLL_POLICY_ENABLED | Indicates that ZLL processing is enabled.  | 
| SL_ZIGBEE_ZLL_POLICY_TARGET | Indicates that ZLL target is enabled.  | 
| SL_ZIGBEE_ZLL_POLICY_STEALING_ENABLED | Indicates that stealing and network update are enabled for non factory new devices.  | 
| SL_ZIGBEE_ZLL_POLICY_REMOTE_RESET_ENABLED | Indicates that remote reset is enabled for non factory new devices.  |