Zigbee Green Power types and defines. See greenpower for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_GP_TYPES_H
#define SILABS_GP_TYPES_H
#include "stack/include/sl_zigbee_types.h"
#define SL_ZIGBEE_GP_BIDIRECTION_INFO_RX_AFTER_TX_MASK 0x01
#define SL_ZIGBEE_GP_BIDIRECTION_INFO_TX_QUEUE_AVAILABLE_MASK 0x02
#define GP_SINK_LIST_ENTRIES 2
#define GP_SIZE_OF_SINK_LIST_ENTRIES_OCTET_STRING (1 + (GP_SINK_LIST_ENTRIES * (sizeof(sl_zigbee_gp_sink_group_t))))
#define GP_PROXY_TABLE_OPTIONS_IN_RANGE (BIT(10))
#define GP_COMMISSIONING_MAX_BYTES (55 - 3)
#define GP_GPD_SRC_ID_FOR_CAHNNEL_CONFIG 0x00000000
#define GP_GPD_SRC_ID_WILDCARD 0xFFFFFFFF
#define GP_GPD_SRC_ID_RESERVED_0 0x00000000
#define GP_GPD_SRC_ID_RESERVED_FFFFFF9 0xFFFFFFF9
#define GP_GPD_SRC_ID_RESERVED_FFFFFFE 0xFFFFFFFE
#define GP_DERIVED_GROUP_ALIAS_NOT_USED 0xffff
#define GP_DMIN_B 32
#define GP_DMIN_U 5
#define GP_DMAX 100
#define SL_ZIGBEE_GP_MAX_APPLICATION_PAYLOAD 100
typedef uint32_t sl_zigbee_gp_source_id_t;
typedef uint32_t sl_zigbee_gp_security_frame_counter_t;
typedef uint32_t sl_zigbee_gp_mic_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_status_t
#else
typedef uint8_t sl_zigbee_gp_status_t;
enum
#endif
{
SL_ZIGBEE_GP_STATUS_OK,
SL_ZIGBEE_GP_STATUS_MATCH,
SL_ZIGBEE_GP_STATUS_DROP_FRAME,
SL_ZIGBEE_GP_STATUS_UNPROCESSED,
SL_ZIGBEE_GP_STATUS_PASS_UNPROCESSED,
SL_ZIGBEE_GP_STATUS_TX_THEN_DROP,
SL_ZIGBEE_GP_STATUS_NO_SECURITY,
SL_ZIGBEE_GP_STATUS_AUTH_FAILURE,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_security_level_t
#else
typedef uint8_t sl_zigbee_gp_security_level_t;
enum
#endif
{
SL_ZIGBEE_GP_SECURITY_LEVEL_NONE = 0x00,
SL_ZIGBEE_GP_SECURITY_LEVEL_RESERVED = 0x01,
SL_ZIGBEE_GP_SECURITY_LEVEL_FC_MIC = 0x02,
SL_ZIGBEE_GP_SECURITY_LEVEL_FC_MIC_ENCRYPTED = 0x03,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_key_type_t
#else
typedef uint8_t sl_zigbee_gp_key_type_t;
enum
#endif
{
SL_ZIGBEE_GP_SECURITY_KEY_NONE = 0x00,
SL_ZIGBEE_GP_SECURITY_KEY_NWK = 0x01,
SL_ZIGBEE_GP_SECURITY_KEY_GPD_GROUP = 0x02,
SL_ZIGBEE_GP_SECURITY_KEY_NWK_DERIVED = 0x03,
SL_ZIGBEE_GP_SECURITY_KEY_GPD_OOB = 0x04,
SL_ZIGBEE_GP_SECURITY_KEY_GPD_DERIVED = 0x07,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_application_id_t
#else
typedef uint8_t sl_zigbee_gp_application_id_t;
enum
#endif
{
SL_ZIGBEE_GP_APPLICATION_SOURCE_ID = 0x00,
SL_ZIGBEE_GP_APPLICATION_IEEE_ADDRESS = 0x02,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_proxy_table_entry_status_t
#else
typedef uint8_t sl_zigbee_gp_proxy_table_entry_status_t;
enum
#endif
{
SL_ZIGBEE_GP_PROXY_TABLE_ENTRY_STATUS_ACTIVE = 0x01,
SL_ZIGBEE_GP_PROXY_TABLE_ENTRY_STATUS_UNUSED = 0xFF,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_gp_sink_table_entry_status_t
#else
typedef uint8_t sl_zigbee_gp_sink_table_entry_status_t;
enum
#endif
{
SL_ZIGBEE_GP_SINK_TABLE_ENTRY_STATUS_ACTIVE = 0x01,
SL_ZIGBEE_GP_SINK_TABLE_ENTRY_STATUS_UNUSED = 0xFF,
};
typedef struct {
union {
sl_802154_long_addr_t gpdIeeeAddress;
sl_zigbee_gp_source_id_t sourceId;
} id;
sl_zigbee_gp_application_id_t applicationId;
uint8_t endpoint;
} sl_zigbee_gp_address_t;
typedef enum {
SL_ZIGBEE_GP_SINK_TYPE_FULL_UNICAST,
SL_ZIGBEE_GP_SINK_TYPE_D_GROUPCAST,
SL_ZIGBEE_GP_SINK_TYPE_GROUPCAST,
SL_ZIGBEE_GP_SINK_TYPE_LW_UNICAST,
SL_ZIGBEE_GP_SINK_TYPE_UNUSED = 0xFF
} sl_zigbee_gp_sink_type_t;
typedef struct {
sl_802154_long_addr_t sinkEUI;
sl_802154_short_addr_t sinkNodeId;
} sl_zigbee_gp_sink_address_t;
typedef struct {
uint16_t groupID;
uint16_t alias;
} sl_zigbee_gp_sink_group_t;
typedef struct {
sl_zigbee_gp_sink_type_t type;
union {
sl_zigbee_gp_sink_address_t unicast;
sl_zigbee_gp_sink_group_t groupcast;
sl_zigbee_gp_sink_group_t groupList; // Entry for Sink Group List
} target;
} sl_zigbee_gp_sink_list_entry_t;
typedef struct {
sl_zigbee_gp_proxy_table_entry_status_t status;
uint32_t options;
sl_zigbee_gp_address_t gpd;
sl_802154_short_addr_t assignedAlias;
uint8_t securityOptions;
sl_zigbee_gp_security_frame_counter_t gpdSecurityFrameCounter;
sl_zigbee_key_data_t gpdKey;
sl_zigbee_gp_sink_list_entry_t sinkList[GP_SINK_LIST_ENTRIES];
uint8_t groupcastRadius;
uint8_t searchCounter;
} sl_zigbee_gp_proxy_table_entry_t;
typedef struct {
sl_zigbee_gp_sink_table_entry_status_t status;
uint16_t options;
sl_zigbee_gp_address_t gpd;
uint8_t deviceId;
sl_zigbee_gp_sink_list_entry_t sinkList[GP_SINK_LIST_ENTRIES];
sl_802154_short_addr_t assignedAlias;
uint8_t groupcastRadius;
uint8_t securityOptions;
sl_zigbee_gp_security_frame_counter_t gpdSecurityFrameCounter;
sl_zigbee_key_data_t gpdKey;
} sl_zigbee_gp_sink_table_entry_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_c_gp_tx_option_t
#else
typedef uint8_t sl_zigbee_c_gp_tx_option_t;
enum
#endif
{
SL_ZIGBEE_CGP_TX_OPTION_NONE = 0x00,
SL_ZIGBEE_CGP_TX_OPTION_USE_CSMA_CA = 0x01,
SL_ZIGBEE_CGP_TX_OPTION_USE_MAC_ACK = 0x02,
SL_ZIGBEE_CGP_TX_OPTION_RESERVED = 0xFC,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_c_gp_address_mode_t
#else
typedef uint8_t sl_zigbee_c_gp_address_mode_t;
enum
#endif
{
SL_ZIGBEE_CGP_ADDRESS_MODE_NONE = 0x00,
SL_ZIGBEE_CGP_ADDRESS_MODE_RESERVED = 0x01,
SL_ZIGBEE_CGP_ADDRESS_MODE_SHORT = 0x02,
SL_ZIGBEE_CGP_ADDRESS_MODE_EXTENDED = 0x03,
};
typedef struct {
union {
sl_802154_short_addr_t shortId;
sl_802154_long_addr_t extendedId;
} address;
sl_802154_pan_id_t panId;
sl_zigbee_c_gp_address_mode_t mode;
} sl_zigbee_c_gp_address_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_d_gp_tx_option_t
#else
typedef uint8_t sl_zigbee_d_gp_tx_option_t;
enum
#endif
{
SL_ZIGBEE_DGP_TX_OPTION_NONE = 0x00,
SL_ZIGBEE_DGP_TX_OPTION_USE_GP_TX_QUEUE = 0x01,
SL_ZIGBEE_DGP_TX_OPTION_USE_CSMA_CA = 0x02,
SL_ZIGBEE_DGP_TX_OPTION_USE_MAC_ACK = 0x04,
SL_ZIGBEE_DGP_TX_OPTION_FRAME_TYPE_DATA = 0x00,
SL_ZIGBEE_DGP_TX_OPTION_FRAME_TYPE_MAINTENANCE = 0x08,
SL_ZIGBEE_DGP_TX_OPTION_RESERVED = 0xE0,
};
typedef struct {
uint8_t foo;
} sl_zigbee_gp_proxy_cluster_attributes_t;
typedef struct {
bool inUse;
bool useCca;
sl_zigbee_gp_address_t addr;
uint8_t gpdCommandId;
uint8_t gpepHandle;
uint16_t queueEntryLifetimeMs;
} sl_zigbee_gp_tx_queue_entry_t;
typedef struct {
uint8_t deviceId;
uint8_t applInfoBitmap;
uint16_t manufacturerId;
uint16_t modelId;
uint8_t numberOfGpdCommands;
uint8_t gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1];
uint8_t numberOfPairedEndpoints;
uint8_t pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1];
uint8_t numberOfGpdClientCluster;
uint8_t numberOfGpdServerCluster;
uint16_t serverClusters[15];
uint16_t clientClusters[15];
} sl_zigbee_gp_application_info_t;
typedef struct {
uint16_t attributeID;
uint8_t attributeDataType;
uint8_t remainingAttributRecordLength; // on 4 bits
uint8_t reported;
uint8_t attrValuePresent;
uint8_t attrOffsetWithinReport;
// TODO change "attrValue" from u32 to a pointer, as the data could be up to a string
// the field "attributeDataType" tell with format it is, among more than 55 possibilities)
// so a add a private field which just tell the length of attrValue to easier
// process it
uint32_t attrValue;
uint8_t attrValueSize;
} sl_zigbee_gp_attribute_record_t;
typedef struct {
// Note: it is "N-1", if there is 2 attr record then nbAttrRecord=1 and not 2 !
uint8_t nbAttrRecord;
uint8_t clientServer;
uint8_t ManIdPresent;
uint8_t datapointOptions;
uint16_t clusterID;
uint16_t manufacturerID;
sl_zigbee_gp_attribute_record_t attrRecord;
} sl_zigbee_gp_data_point_descriptor_t;
typedef struct {
uint8_t repId;
uint8_t reportOptions;
uint16_t timeoutPeriod;
uint8_t totalLength;
sl_zigbee_gp_data_point_descriptor_t dataPoint;
} sl_zigbee_gp_report_descriptor_t;
typedef struct {
uint8_t switchInfoLength;
uint8_t nbOfContacts;
uint8_t switchType;
uint8_t currentContact;
uint8_t savedContact;
}sl_zigbee_gp_switch_information_t;
typedef struct {
uint8_t currentStatus;
uint8_t contactBitmask;
} sl_zigbee_gp_generic_switch_data_t;
typedef struct {
uint8_t totalLengthOfAddInfoBlock;
uint8_t optionSelector;
union {
struct {
uint8_t reportIdentifier;
uint8_t attrOffsetWithinReport;
uint16_t clusterID;
uint16_t attributeID;
uint8_t attributeDataType;
uint8_t attributeOptions; //clientServer bit0 manufacturerIdPresent bit1
uint16_t manufacturerID;
} compactAttr;
struct {
uint8_t contactStatus;
uint8_t contactBitmask;
} genericSwitch;
} optionData;//sl_zigbee_gp_translation_table_additional_info_block_option_record_option_data_field_t;
} sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t;
typedef struct {
sl_zigbee_gp_status_t status;
uint8_t gpdLink;
uint8_t sequenceNumber;
sl_zigbee_gp_address_t addr;
sl_zigbee_gp_security_level_t gpdfSecurityLevel;
sl_zigbee_gp_key_type_t gpdfSecurityKeyType;
bool autoCommissioning;
uint8_t bidirectionalInfo;
uint32_t gpdSecurityFrameCounter;
uint8_t gpdCommandId;
uint32_t mic;
uint8_t proxyTableIndex;
uint8_t gpdCommandPayloadLength;
uint8_t gpdCommandPayload[SL_ZIGBEE_GP_MAX_APPLICATION_PAYLOAD];
sl_zigbee_rx_packet_info_t packetInfo;
} sl_zigbee_gp_params_t;
// -----------------------------------------------------------------------------
// API
sl_status_t sl_zigbee_d_gp_send(bool action,
bool useCca,
sl_zigbee_gp_address_t *addr,
uint8_t gpdCommandId,
uint8_t gpdAsduLength,
uint8_t const *gpdAsdu,
uint8_t gpepHandle,
uint16_t gpTxQueueEntryLifetimeMs);
// Tx Queue APIs
sli_zigbee_message_buffer_queue_t * sl_zigbee_gp_get_tx_queue_head(void);
void sl_zigbee_gp_set_max_tx_queue_entry(uint16_t maxEntries);
uint16_t sl_zigbee_get_gp_max_tx_q_list_count(void);
uint16_t sl_zigbee_get_gp_tx_q_list_count(void);
sli_buffer_manager_buffer_t sl_zigbee_gp_get_tx_queue_entry_from_queue(sl_zigbee_gp_tx_queue_entry_t *txQueue,
uint8_t *data,
uint16_t *dataLength,
uint16_t allocatedDataLength);
sl_status_t sl_zigbee_gp_get_tx_queue_entry_from_queue_index(uint8_t index,
sl_zigbee_gp_tx_queue_entry_t *txQueue,
uint8_t *payload,
uint16_t *payload_len);
sli_buffer_manager_buffer_t sl_zigbee_gp_add_gp_tx_queue_entry_with_payload(sl_zigbee_gp_tx_queue_entry_t *txQueue,
uint8_t *data,
uint16_t dataLength);
bool sl_zigbee_gp_remove_from_tx_queue(sl_zigbee_gp_tx_queue_entry_t *txQueue);
void sl_zigbee_gp_clear_tx_queue(void);
void sli_zigbee_gp_init_tokens(void);
#endif // SILABS_GP_TYPES_H
// end of name API
Modules#
sl_zigbee_gp_sink_list_entry_t
sl_zigbee_gp_proxy_table_entry_t
sl_zigbee_gp_sink_table_entry_t
sl_zigbee_gp_proxy_cluster_attributes_t
sl_zigbee_gp_application_info_t
sl_zigbee_gp_attribute_record_t
sl_zigbee_gp_data_point_descriptor_t
sl_zigbee_gp_report_descriptor_t
sl_zigbee_gp_switch_information_t
sl_zigbee_gp_generic_switch_data_t
sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t
GP Types#
Green Power Security Level.
Green Power Security Level.
Green Power Security Security Key Type.
Green Power Application ID.
GP proxy table entry status.
GP sink table entry status.
GP Sink Type.
CGp Transmit options.
Addressing modes for CGp messages.
Transmit options for DGp messages.
API#
DGp Send.
Gets tx queue head.
Sets maximum limit for number of entries in the tx queue.
Gets the limit set for maximum number of entries in the tx queue.
Gets the number of entries in the tx queue.
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns SL_ZIGBEE_NULL_MESSAGE_BUFFER if not found.
Gets the entry at the specified index of Tx Queue The function goes through the tx queue and populates the output parameters with the relevant entry if it exists.
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
Remove an entry from Tx Queue This function searches and removes the entry provided.
Purges Tx Queue This function purges the tx queue.
Initialize GP tokens This function initializes GP tokens for SoC usage.
Macros#
Mask used in the green power endpoint incoming message handler to pass bidirectional information. Incoming GPDF has rxAfterTx bit set.
Mask to test if transmit queue is available at green power stub layer to hold an outgoing GPDF.
Number of GP sink list entries. Minimum is 2 sink list entries.
The size of the SinkList entries in sink table in form of octet string that has a format of [<1 byte length>, <n bytes for sink groups>].
Bit mask for the proxy table ebtry option bit representing in-range bit field.
Maximum number of bytes in a green power commissioning frame excluding 3 bytes for device ID, option and application information fields.
GPD Source ID when requesting channel request.
GPD wildcard Source ID.
GPD Reserved Source ID. Used in maintenance frame.
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
GPD Reserved Source ID. All addresses between 0xFFFFFFF9 and 0xFFFFFFFE are reserved.
Default value for derived group ID when alias is not used.
Tunneling delay constant Dmin_b in milliseconds. Ref green power specification for more information on this constant.
Tunneling delay constant Dmin_u in milliseconds. Ref green power specification for more information on this constant.
Tunneling delay constant Dmax in milliseconds. Ref green power specification for more information on this constant.
Defines the maximum size of the application payload for Green Power (GP) commands in the Zigbee stack.
GP Types Documentation#
sl_zigbee_gp_status_t#
sl_zigbee_gp_status_t
Green Power Security Level.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_STATUS_OK | Success Status |
| SL_ZIGBEE_GP_STATUS_MATCH | Match Frame |
| SL_ZIGBEE_GP_STATUS_DROP_FRAME | Drop Frame |
| SL_ZIGBEE_GP_STATUS_UNPROCESSED | Frame Unprocessed |
| SL_ZIGBEE_GP_STATUS_PASS_UNPROCESSED | Frame Pass Unprocessed |
| SL_ZIGBEE_GP_STATUS_TX_THEN_DROP | Frame TX Then Drop |
| SL_ZIGBEE_GP_STATUS_NO_SECURITY | No Security |
| SL_ZIGBEE_GP_STATUS_AUTH_FAILURE | Security Failure |
sl_zigbee_gp_security_level_t#
sl_zigbee_gp_security_level_t
Green Power Security Level.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_SECURITY_LEVEL_NONE | No Security |
| SL_ZIGBEE_GP_SECURITY_LEVEL_RESERVED | Reserved |
| SL_ZIGBEE_GP_SECURITY_LEVEL_FC_MIC | 4 Byte Frame Counter and 4 Byte MIC |
| SL_ZIGBEE_GP_SECURITY_LEVEL_FC_MIC_ENCRYPTED | 4 Byte Frame Counter and 4 Byte MIC with encryption |
sl_zigbee_gp_key_type_t#
sl_zigbee_gp_key_type_t
Green Power Security Security Key Type.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_SECURITY_KEY_NONE | No Key |
| SL_ZIGBEE_GP_SECURITY_KEY_NWK | GP Security Key Type is Zigbee Network Key |
| SL_ZIGBEE_GP_SECURITY_KEY_GPD_GROUP | GP Security Key Type is Group Key |
| SL_ZIGBEE_GP_SECURITY_KEY_NWK_DERIVED | GP Security Key Type is Derived Network Key |
| SL_ZIGBEE_GP_SECURITY_KEY_GPD_OOB | GP Security Key Type is Out Of Box Key |
| SL_ZIGBEE_GP_SECURITY_KEY_GPD_DERIVED | GP Security Key Type is GPD Derived Key |
sl_zigbee_gp_application_id_t#
sl_zigbee_gp_application_id_t
Green Power Application ID.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_APPLICATION_SOURCE_ID | Source identifier. |
| SL_ZIGBEE_GP_APPLICATION_IEEE_ADDRESS | IEEE address. |
sl_zigbee_gp_proxy_table_entry_status_t#
sl_zigbee_gp_proxy_table_entry_status_t
GP proxy table entry status.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_PROXY_TABLE_ENTRY_STATUS_ACTIVE | The GP table entry is in use for a Proxy Table Entry. |
| SL_ZIGBEE_GP_PROXY_TABLE_ENTRY_STATUS_UNUSED | The proxy table entry is not in use. |
sl_zigbee_gp_sink_table_entry_status_t#
sl_zigbee_gp_sink_table_entry_status_t
GP sink table entry status.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_SINK_TABLE_ENTRY_STATUS_ACTIVE | The GP table entry is in use for a Sink Table Entry. |
| SL_ZIGBEE_GP_SINK_TABLE_ENTRY_STATUS_UNUSED | The proxy table entry is not in use. |
sl_zigbee_gp_sink_type_t#
sl_zigbee_gp_sink_type_t
GP Sink Type.
| Enumerator | |
|---|---|
| SL_ZIGBEE_GP_SINK_TYPE_FULL_UNICAST | Sink Type is Full Unicast |
| SL_ZIGBEE_GP_SINK_TYPE_D_GROUPCAST | Sink Type is Derived groupcast, the group ID is derived from the GpdId during commissioning. The sink is added to the APS group with that groupId. |
| SL_ZIGBEE_GP_SINK_TYPE_GROUPCAST | Sink type SL_ZIGBEE_GP_SINK_TYPE_GROUPCAST, the groupId can be obtained from the APS group table or from the sink table. |
| SL_ZIGBEE_GP_SINK_TYPE_LW_UNICAST | Sink Type is Light Weight Unicast. |
| SL_ZIGBEE_GP_SINK_TYPE_UNUSED | Unused sink type |
sl_zigbee_c_gp_tx_option_t#
sl_zigbee_c_gp_tx_option_t
CGp Transmit options.
| Enumerator | |
|---|---|
| SL_ZIGBEE_CGP_TX_OPTION_NONE | No options. |
| SL_ZIGBEE_CGP_TX_OPTION_USE_CSMA_CA | Use CSMA/CA. |
| SL_ZIGBEE_CGP_TX_OPTION_USE_MAC_ACK | Use MAC ACK. |
| SL_ZIGBEE_CGP_TX_OPTION_RESERVED | Reserved. |
sl_zigbee_c_gp_address_mode_t#
sl_zigbee_c_gp_address_mode_t
Addressing modes for CGp messages.
| Enumerator | |
|---|---|
| SL_ZIGBEE_CGP_ADDRESS_MODE_NONE | No address (PAN identifier and address omitted). |
| SL_ZIGBEE_CGP_ADDRESS_MODE_RESERVED | Reserved. |
| SL_ZIGBEE_CGP_ADDRESS_MODE_SHORT | 16-bit short address. |
| SL_ZIGBEE_CGP_ADDRESS_MODE_EXTENDED | 64-bit extended address. |
sl_zigbee_d_gp_tx_option_t#
sl_zigbee_d_gp_tx_option_t
Transmit options for DGp messages.
| Enumerator | |
|---|---|
| SL_ZIGBEE_DGP_TX_OPTION_NONE | No options. |
| SL_ZIGBEE_DGP_TX_OPTION_USE_GP_TX_QUEUE | Use gpTxQueue. |
| SL_ZIGBEE_DGP_TX_OPTION_USE_CSMA_CA | Use CSMA/CA. |
| SL_ZIGBEE_DGP_TX_OPTION_USE_MAC_ACK | Use MAC ACK. |
| SL_ZIGBEE_DGP_TX_OPTION_FRAME_TYPE_DATA | Data frame. |
| SL_ZIGBEE_DGP_TX_OPTION_FRAME_TYPE_MAINTENANCE | Maintenance frame. |
| SL_ZIGBEE_DGP_TX_OPTION_RESERVED | Reserved. |
sl_zigbee_gp_security_frame_counter_t#
typedef uint32_t sl_zigbee_gp_security_frame_counter_t
32-bit security frame counter
API Documentation#
sl_zigbee_d_gp_send#
sl_status_t sl_zigbee_d_gp_send (bool action, bool useCca, sl_zigbee_gp_address_t * addr, uint8_t gpdCommandId, uint8_t gpdAsduLength, uint8_t const * gpdAsdu, uint8_t gpepHandle, uint16_t gpTxQueueEntryLifetimeMs)
DGp Send.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | action | Action to add (true) or remove (false) |
| bool | N/A | useCca | Use CCA for GPDF transmission. |
| sl_zigbee_gp_address_t * | N/A | addr | The gpd address sl_zigbee_gp_address_t. |
| uint8_t | N/A | gpdCommandId | GPD Command ID |
| uint8_t | N/A | gpdAsduLength | ASDU Length. |
| uint8_t const * | N/A | gpdAsdu | The ASDU buffer that holds the outgoing GPDF as payload. |
| uint8_t | N/A | gpepHandle | Handle for the asdu. |
| uint16_t | N/A | gpTxQueueEntryLifetimeMs | Life time in milliseconds in Tx queue after which it gets cleared. |
This API adds or removes an outgoing GPDF (passed as ASDU) in the GP stub layer. As part of Gp Response command processing by green power client cluster, this API submits a outgoing a channel configuration or a commissioning reply GPDF. Similarly, it is called with appropriate action to clear the Tx queue upon channel request timeout.
Returns
An ::sl_status_t as status.
sl_zigbee_gp_get_tx_queue_head#
sli_zigbee_message_buffer_queue_t * sl_zigbee_gp_get_tx_queue_head (void )
Gets tx queue head.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function gets the head pointer of the tx queue. Note : since it returns a pointer to memory the head, it 'll not be useful on host.
Returns
pointer to head of tx queue sli_zigbee_message_buffer_queue_t
sl_zigbee_gp_set_max_tx_queue_entry#
void sl_zigbee_gp_set_max_tx_queue_entry (uint16_t maxEntries)
Sets maximum limit for number of entries in the tx queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | maxEntries |
This function sets the maximum number of entries the tx queue is supposed to grow.
sl_zigbee_get_gp_max_tx_q_list_count#
uint16_t sl_zigbee_get_gp_max_tx_q_list_count (void )
Gets the limit set for maximum number of entries in the tx queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function gets the limit set for the maximum number of entries the tx queue is supposed to hold.
Returns
limit to the maximum number of entries.
sl_zigbee_get_gp_tx_q_list_count#
uint16_t sl_zigbee_get_gp_tx_q_list_count (void )
Gets the number of entries in the tx queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function gets the number of entries present in tx queue.
Returns
number of entries.
sl_zigbee_gp_get_tx_queue_entry_from_queue#
sli_buffer_manager_buffer_t sl_zigbee_gp_get_tx_queue_entry_from_queue (sl_zigbee_gp_tx_queue_entry_t * txQueue, uint8_t * data, uint16_t * dataLength, uint16_t allocatedDataLength)
Gets an entry from Tx Queue The function searches the tx queue using gpd address pointed by supplied in the input/output argument txQueue and returns the message buffer that currently holding the outgoing gpdf information, returns SL_ZIGBEE_NULL_MESSAGE_BUFFER if not found.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_gp_tx_queue_entry_t * | N/A | txQueue | sl_zigbee_gp_tx_queue_entry_t A pointer to an allocated memory to get a copy of the tx queue entry from the buffer queue. The caller populates the addr field of this parameter which is used as a search key. |
| uint8_t * | N/A | data | A pointer to an allocated memory to get a copy of the gpd command payload if an entry is found. This can be passed as NULL if payload is not required by caller. |
| uint16_t * | N/A | dataLength | A pointer to hold the length of the gpd command payload when an entry is found and the data collector is non-NULL. |
| uint16_t | N/A | allocatedDataLength | Size in bytes for the allocated memory for the data collector. If this value is smaller compared to length of the data in the queue, no data gets copied out. |
Returns
Buffer sli_buffer_manager_buffer_t that holds the entry if found, null message buffer if not found.
sl_zigbee_gp_get_tx_queue_entry_from_queue_index#
sl_status_t sl_zigbee_gp_get_tx_queue_entry_from_queue_index (uint8_t index, sl_zigbee_gp_tx_queue_entry_t * txQueue, uint8_t * payload, uint16_t * payload_len, allocatedDataLength)
Gets the entry at the specified index of Tx Queue The function goes through the tx queue and populates the output parameters with the relevant entry if it exists.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index in the queue to retrieve from. |
| sl_zigbee_gp_tx_queue_entry_t * | N/A | txQueue | sl_zigbee_gp_tx_queue_entry_t A pointer to an allocated memory to get a copy of the tx queue entry from the buffer queue. The caller populates the addr field of this parameter which is used as a search key. |
| uint8_t * | N/A | payload | A pointer to an allocated memory to get a copy of the gpd command payload if an entry is found. This can be passed as NULL if payload is not required by caller. |
| uint16_t * | N/A | payload_len | A pointer to hold the length of the gpd command payload when an entry is found and the data collector is non-NULL. |
| N/A | allocatedDataLength | Size in bytes for the allocated memory for the data collector. If this value is smaller compared to length of the data in the queue, no data gets copied out. |
Returns
sl_status_t SL_STATUS_OK if a valid entry was retrieved, SL_STATUS_NOT_FOUND if not.
sl_zigbee_gp_add_gp_tx_queue_entry_with_payload#
sli_buffer_manager_buffer_t sl_zigbee_gp_add_gp_tx_queue_entry_with_payload (sl_zigbee_gp_tx_queue_entry_t * txQueue, uint8_t * data, uint16_t dataLength)
Adds an entry to Tx Queue This function adds an entry along with supplied payload data to the Buffer queue. Returns the buffer handle if success else null message buffer upon failure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_gp_tx_queue_entry_t * | N/A | txQueue | sl_zigbee_gp_tx_queue_entry_t A pointer to an allocated memory holding the entry with all the members of the structure assigned as needed. |
| uint8_t * | N/A | data | A pointer holding the data payload. Can be supplied as NULL if there is no data payload. |
| uint16_t | N/A | dataLength | Length of the data. |
Returns
Buffer sli_buffer_manager_buffer_t that holds the entry upon success else null message buffer.
sl_zigbee_gp_remove_from_tx_queue#
bool sl_zigbee_gp_remove_from_tx_queue (sl_zigbee_gp_tx_queue_entry_t * txQueue)
Remove an entry from Tx Queue This function searches and removes the entry provided.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_gp_tx_queue_entry_t * | N/A | txQueue | sl_zigbee_gp_tx_queue_entry_t A pointer to an allocated memory holding the entry with gpd addr field assigned, which is used as for searching the tx queue. NOTE : Use of wildcard gpd addr (AppId = 0,SrcId = 0xFFFFFFFF) , removes all the entries of the tx queue. |
Returns
True upon success else false.
sl_zigbee_gp_clear_tx_queue#
void sl_zigbee_gp_clear_tx_queue (void )
Purges Tx Queue This function purges the tx queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sli_zigbee_gp_init_tokens#
void sli_zigbee_gp_init_tokens (void )
Initialize GP tokens This function initializes GP tokens for SoC usage.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |