Running Matter with OpenThread, Zigbee, and Bluetooth Concurrently on a System-on-Chip#
Note: This section replaces AN1418: Running Zigbee, OpenThread, and Bluetooth Concurrently on a System-on-Chip. Further updates to this application note will be provided here.
This application note describes how to run a combination of Zigbee, Matter with OpenThread, and Bluetooth networking stacks and the Zigbee application layer on a System-on-Chip (SoC). One of the main functions of a Concurrent Multiprotocol (CMP) device is to act as a bridge between Zigbee and OpenThread networks.
Note that, depending on the chip, memory size restrictions may prevent running Matter on SoC devices.