Interface for querying library status.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef SILABS_LIBRARY_H
#define SILABS_LIBRARY_H

#include "stack/include/sl_zigbee_types.h"

// A library's status is an 8-bit value with information about it.
// The high bit indicates whether the library is present (1), or if it is a
// stub (0).  The lower 7-bits can be used for codes specific to the library.
// This allows a library, like the security library, to specify what additional
// features are present.
// A value of 0xFF is reserved, it indicates an error in retrieving the
// library status.
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_library_status_t
#else
typedef uint8_t sl_zigbee_library_status_t;
enum {
  // Base return codes. These may be ORed with statuses further below.
  SL_ZIGBEE_LIBRARY_PRESENT_MASK  = 0x80,
  SL_ZIGBEE_LIBRARY_IS_STUB       = 0x00,
  SL_ZIGBEE_LIBRARY_ERROR         = 0xFF,

  // The ZigBee Pro library uses the following to indicate additional
  // functionality:
  SL_ZIGBEE_ZIGBEE_PRO_LIBRARY_END_DEVICE_ONLY        = 0x00, // no router capability
  SL_ZIGBEE_ZIGBEE_PRO_LIBRARY_HAVE_ROUTER_CAPABILITY = 0x01,
  SL_ZIGBEE_ZIGBEE_PRO_LIBRARY_ZLL_SUPPORT            = 0x02,

  // The Security library uses the following to indicate additional
  // functionality:
  SL_ZIGBEE_SECURITY_LIBRARY_END_DEVICE_ONLY      = 0x00,
  SL_ZIGBEE_SECURITY_LIBRARY_HAVE_ROUTER_SUPPORT  = 0x01,  // router or trust center support

  // The Packet Validate library may be globally turned on/off.
  // Bit 0 indicates whether the library is enabled/disabled.
  SL_ZIGBEE_PACKET_VALIDATE_LIBRARY_DISABLED      = 0x00,
  SL_ZIGBEE_PACKET_VALIDATE_LIBRARY_ENABLED       = 0x01,
  SL_ZIGBEE_PACKET_VALIDATE_LIBRARY_ENABLE_MASK   = 0x01
};
#endif

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_library_id_t
#else
typedef uint8_t sl_zigbee_library_id_t;
enum {
  SL_ZIGBEE_FIRST_LIBRARY_ID              = 0x00,

  SL_ZIGBEE_ZIGBEE_PRO_LIBRARY_ID         = 0x00,
  SL_ZIGBEE_BINDING_LIBRARY_ID            = 0x01,
  SL_ZIGBEE_END_DEVICE_BIND_LIBRARY_ID    = 0x02,
  SL_ZIGBEE_SECURITY_CORE_LIBRARY_ID      = 0x03,
  SL_ZIGBEE_SECURITY_LINK_KEYS_LIBRARY_ID = 0x04,
  SL_ZIGBEE_ALARM_LIBRARY_ID              = 0x05,
  SL_ZIGBEE_CBKE_LIBRARY_ID               = 0x06,
  SL_ZIGBEE_CBKE_DSA_SIGN_LIBRARY_ID      = 0x07,
  SL_ZIGBEE_ECC_LIBRARY_ID                = 0x08,
  SL_ZIGBEE_CBKE_DSA_VERIFY_LIBRARY_ID    = 0x09,
  SL_ZIGBEE_PACKET_VALIDATE_LIBRARY_ID    = 0x0A,
  SL_ZIGBEE_INSTALL_CODE_LIBRARY_ID       = 0x0B,
  SL_ZIGBEE_ZLL_LIBRARY_ID                = 0x0C,
  SL_ZIGBEE_CBKE_LIBRARY_283K1_ID         = 0x0D,
  SL_ZIGBEE_ECC_LIBRARY_283K1_ID          = 0x0E,
  SL_ZIGBEE_CBKE_CORE_LIBRARY_ID          = 0x0F,
  SL_ZIGBEE_NCP_LIBRARY_ID                = 0x10,
  SL_ZIGBEE_MULTI_NETWORK_LIBRARY_ID      = 0x11,
  SL_ZIGBEE_ENHANCED_BEACON_REQUEST_LIBRARY_ID = 0x12,
  SL_ZIGBEE_CBKE_283K1_DSA_VERIFY_LIBRARY_ID   = 0x13,
  SL_ZIGBEE_MULTI_PAN_LIBRARY_ID          = 0x14,

  SL_ZIGBEE_NUMBER_OF_LIBRARIES           = 0x15,
  SL_ZIGBEE_NULL_LIBRARY_ID               = 0xFF
};
#endif

#define SL_ZIGBEE_LIBRARY_NAMES \
  "Zigbee Pro",                 \
  "Binding",                    \
  "", /*"End Device Bind"*/     \
  "Security Core",              \
  "Security Link Keys",         \
  "",  /*"Alarm",*/             \
  "CBKE 163K1",                 \
  "CBKE DSA Sign",              \
  "ECC",                        \
  "CBKE DSA Verify",            \
  "Packet Validate",            \
  "Install Code",               \
  "ZLL",                        \
  "CBKE 283K1",                 \
  "ECC 283K1",                  \
  "CBKE core",                  \
  "NCP",                        \
  "Multi network",              \
  "Enhanced Beacon Req",        \
  "CBKE 283K1 DSA Verify",      \
  "Multi-PAN",                  \

#if !defined(EZSP_HOST)
// This will be defined elsewhere for the EZSP Host applications.

sl_zigbee_library_status_t sl_zigbee_get_library_status(sl_zigbee_library_id_t libraryId);
#endif

#endif // SILABS_LIBRARY_H

Macros#

#define

Functions#

enum sl_zigbee_library_status_t enum sl_zigbee_library_id_t sl_zigbee_library_status_t
sl_zigbee_get_library_status(sl_zigbee_library_id_t libraryId)

This indicates the presence, absence, or status of an Ember stack library.

Macro Definition Documentation#

SL_ZIGBEE_LIBRARY_NAMES#

#define SL_ZIGBEE_LIBRARY_NAMES
Value:
"Zigbee Pro", \
"Binding", \
"", /*"End Device Bind"*/ \
"Security Core", \
"Security Link Keys", \
"", /*"Alarm",*/ \
"CBKE 163K1", \
"CBKE DSA Sign", \
"ECC", \
"CBKE DSA Verify", \
"Packet Validate", \
"Install Code", \
"ZLL", \
"CBKE 283K1", \
"ECC 283K1", \
"CBKE core", \
"NCP", \
"Multi network", \
"Enhanced Beacon Req", \
"CBKE 283K1 DSA Verify", \
"Multi-PAN", \

Function Documentation#

sl_zigbee_get_library_status#

enum sl_zigbee_library_status_t enum sl_zigbee_library_id_t sl_zigbee_library_status_t sl_zigbee_get_library_status (sl_zigbee_library_id_t libraryId)

This indicates the presence, absence, or status of an Ember stack library.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_library_id_tN/AlibraryId

An enumerated list of library identifiers.

This routine takes a library identifier and returns whether the library is enabled or not. See ::sl_zigbee_library_status_t for return codes.