Application Components#

WiSeConnect™ SDK v3.x has revamped the component organization such that almost none of the v2.x components remain in v3.x.

The following sections provide a list of v3.x components.

The component category path is listed for each component, specifying how to navigate to the component in the SOFTWARE COMPONENTS tab of Simplicity Studio. Components are listed in alphabetical order of the component category path.

Studio Software Components tab

Common#

Component Name

Component Category Path

Description

WiSeConnect3 Common Library

Common

Commonly used components

WiSeConnect3 Resources

Resources

Default values and certificates

Si91x Support Library

Si91x Support library

Library with utilities for the NCP UART interface

Unity test framework

Test > Framework

Unity test framework

Wireless#

Component Name

Component Category Path

Description

BLE

Device > Si91x > Wireless

API for Bluetooth Low Energy (BLE) functionality

Si91x Wireless Subsystem

Device > Si91x > Wireless

API to manage the wireless subsystem in the SiWx91x™ chipset

Basic Buffer Manager

Device > Si91x > Wireless > Buffer Manager

SiWx91x memory buffer manager for malloc-based memory management

Internal Network Stack

Device > Si91x > Wireless > Network Stack

API for running the networking layers on the SiWx91x chipset

LwIP Network Stack (Hosted)

Device > Si91x > Wireless > Network Stack

Lightweight Internet Protocol (LwIP) third party library-based API for running networking layers on a host MCU

Si91x NCP bus interface

Device > Si91x > Wireless > Network Stack

API to manage bus communication to SiWx91x from the host MCU

Si91x NCP SPI interface

Device > Si91x > Wireless > Network Stack

API to manage SPI communication to SiWx91x from the host MCU

Si91x NCP UART interface

Device > Si91x > Wireless > Network Stack

API to manage UART communication to SiWx91x from the host MCU

Wi-Fi

Protocol

Application programming interface (API) for Wi-Fi functionality

Network Management#

Component Name

Component Category Path

Description

Network Manager

Service > Network Management

API to manage network interfaces and their behaviour

Basic Network Configuration Manager

Service > Network Management > Configuration

Basic reference implementation for managing network credentials and profiles

NVM3 Network Configuration Manager

Service > Network Management > Configuration

API for managing network credentials and profiles in non-volatile memory with key-based storage

Sockets#

Component Name

Component Category Path

Description

BSD Socket API

Common

Berkeley Software Distribution (BSD) standard API for socket programming

Si91x Asynchronous Socket

Device > Si91x > Wireless > Socket

API for SiWx91x asynchronous socket programming

Si91x Socket

Device > Si91x > Wireless > Socket

API for SiWx91x socket programming

BSD Socket

Service

API for BSD-style communication over the Transport Control Protocol (TCP) and Internet Protocol (IP) networking layers

IoT Socket

Third Party

ARM Internet-of-Things (IoT) standard API for socket programming

SiWx91x MCU#

The following SiWx91x MCU (application processor) components are available:

Common MCU components#

Component Name

Component Category Path

Description

Board Configuration Header Files

N/A (no category)

Radio board configuration header files

brd4338a config

Board > Configuration

Configuration files for radio board BRD4338A

brd4342a config

Board > Configuration

Configuration files for radio board BRD4342A

EFx32 - Si91x Connection Configurator

Board > Configuration

Configuration for connections between SiWx91x and EFx32 host MCU

Si91x SoC Board Configurations

Board > Configuration

Hardware configurations for SiWx91x SoC boards

BRD4338A

Board > Radio Board

Radio Board support for BRD4338A

BRD4342A

Board > Radio Board

Radio Board support for BRD4342A

Default Configuration

Device > Si91x > Memory Configuration

Default memory configuration

MCU Advanced Features and Wireless Basic Features

Device > Si91x > Memory Configuration

Configuration for random-access memory (RAM) split option 3 between processors - 256KB for network processor and 448KB for application processor.

MCU Basic Features and Wireless Advanced Features

Device > Si91x > Memory Configuration

Configuration for default RAM split (option 1) between processors - 512KB for network processor and 192KB for application processor.

MCU Medium Features and Wireless Medium Features

Device > Si91x > Memory Configuration

Configuration for RAM split option 2 between processors - 448KB for network processor and 256KB for application processor.

Si91x MCU Subsystem

Device > Si91x > MCU

Initializing the SiWx91x MCU (application processor) subsystem on startup

Debug Unit

Device > Si91x > MCU > Common

Debug functionality for the SiWx91x MCU

System Calls

Device > Si91x > MCU > Common

System call support for the SiWx91x MCU

Core

Device > Si91x > MCU > Core

Core SiWx91x MCU functionality

CMSIS Core

Device > Si91x > MCU > Core

Common Microcontroller Software Interface Standard (CMSIS) core functionality

FreeRTOS Configuration

Device > Si91x > MCU > Core

Default configuration for FreeRTOS (operating system) instance on the SiWx91x MCU

NVIC Interrupt Priorities Configuration

Device > Si91x > MCU > Core

Configuration of nested vector interrupt controller (NVIC) priorities

RAM Execution

Device > Si91x > MCU > Core

Enabling certain pre-determined components to execute from random-access memory (RAM)

RSI User Configuration

Device > Si91x > MCU > Core

User configuration for the SiWx91x MCU

UDMA Linker Configuration

Device > Si91x > MCU > Core

Linker configuration for unified direct memory access (UDMA)

ulp_mode_execution

Device > Si91x > MCU > Core

Enabling ultra low power (ULP) mode

Debug

Device > Si91x > MCU > Debug

Debug functionality for the SiWx91x application processor

SI917-SB00

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SI917-SB00

SIWG917M100MGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M100MGTBA

SIWG917M100XNTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M100XNTBA

SIWG917M110LGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M110LGTBA

SIWG917M111MGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M111MGTBA

SIWG917M111XGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M111XGTBA

SIWG917M121XGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M121XGTBA

SIWG917M141XGTBA

Device > Si91x > MCU > Device Part > SiWG917

CMSIS device part headers for SIWG917M141XGTBA

8MB Flash (External)

Device > Si91x > MCU > Flash

Adding 8MB external flash to the SiWx91x SoC

8MB PSRAM (External)

Device > Si91x > MCU > Flash

Adding 8MB external pseudo-static random-access memory (PSRAM) to the SiWx91x SoC

No External Flash

Device > Si91x > MCU > Flash

Excluding the external flash from the SiWx91x SoC

No External PSRAM

Device > Si91x > MCU > Flash

Excluding the external PSRAM from the SiWx91x SoC

HAL

Device > Si91x > MCU > HAL

Hardware abstraction layer (HAL) for the SiWx91x MCU

Soft Reset

Device > Si91x > MCU > HAL

Soft reset functionality for the SiWx91x MCU

SL errno

Device > Si91x > MCU > Service

Enabling thread-safe error numbers

GCC Toolchain Support

Device > Si91x > MCU > Toolchain

Support for the Gnu's Not UNIX (GNU) Compiler Collection (GCC) toolchain

SIWG917Y111MGAB

Platform > Device > Si91x > MCU > Family > SIWG917Y

CMSIS device part headers for SIWG917Y111MGAB

SIWG917Y111MGNB

Platform > Device > Si91x > MCU > Family > SIWG917Y

CMSIS device part headers for SIWG917Y111MGNB

Peripherals#

Component Name

Component Category Path

Description

ADC

Device > Si91x > MCU > Peripheral

API for the analog-to-digital-converter (ADC) peripheral

ADC Instance

Device > Si91x > MCU > Peripheral

ADC peripheral instance

Calendar

Device > Si91x > MCU > Peripheral

API for the calendar peripheral

Config Timer

Device > Si91x > MCU > Peripheral

API for the config timer peripheral

DMA

Device > Si91x > MCU > Peripheral

API for the direct memory access (DMA) peripheral

Efuse

Device > Si91x > MCU > Peripheral

API for the e-fuse peripheral

GPIO

Device > Si91x > MCU > Peripheral

API for the general-purpose input/output (GPIO) ports

GSPI

Device > Si91x > MCU > Peripheral

API for the Generic Serial Peripheral Interface (GSPI) peripheral

I2C

Device > Si91x > MCU > Peripheral

API for the Inter-Integrated Circuit (I2C) peripheral

I2C Instance

Device > Si91x > MCU > Peripheral

I2C peripheral instance

I2S

Device > Si91x > MCU > Peripheral

API for the Inter-Integrated Circuit Sound (I2S) peripheral

IO Stream: USART

Device > Si91x > MCU > Peripheral

API for input-output (I/O) stream over a Universal Synchronous/Asynchronous Receiver/Transmitter (USART) interface

PWM

Device > Si91x > MCU > Peripheral

API for the Pulse width modulation (PWM) peripheral

PWM Instance

Device > Si91x > MCU > Peripheral

PWM peripheral instance

SIO

Device > Si91x > MCU > Peripheral

API for the Serial Input Output (SIO) peripheral

SSI

Device > Si91x > MCU > Peripheral

API for the Synchronous Serial Interface (SSI) peripheral

SysRTC

Device > Si91x > MCU > Peripheral

API for the system real-time clock (SysRTC) peripheral

ULP Timer

Device > Si91x > MCU > Peripheral

API for the ultra low power (ULP) timer peripheral

ULP Timer Instance

Device > Si91x > MCU > Peripheral

ULP timer peripheral instance

USART

Device > Si91x > MCU > Peripheral

API for the USART peripheral

WDT

Device > Si91x > MCU > Peripheral

API for the watchdog timer peripheral

SL GPIO Peripheral

Device > Si91x > MCU > Peripheral > Register-Level API

API for GPIO ports

SL I2C Peripheral

Device > Si91x > MCU > Peripheral > Register-Level API

API for the Inter-Integrated Circuit (I2C) peripheral

SL SDIO Secondary Peripheral

Device > Si91x > MCU > Peripheral > Register-Level API

API for Secure Digital Input Output (SDIO) peripheral as secondary

PSRAM Core

Device > Si91x > MCU > Peripheral > PSRAM Driver

PSRAM driver core functionality

APS1604M-SQR PSRAM Device

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Device

AP Memory APS1604M-SQR PSRAM device related configurations

APS6404L_SQH PSRAM Device

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Device

AP Memory APS6404L-SQH PSRAM device related configurations

APS6404L_SQRH PSRAM Device

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Device

AP Memory APS6404L-SQRH PSRAM device related configurations

BSS Segment in PSRAM

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Linker Configurations

Adding the Block Starting Symbol (BSS) segment in pseudo-static random-access memory (PSRAM)

Data Segment in PSRAM

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Linker Configurations

Adding the data segment in PSRAM

Heap Segment in PSRAM

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Linker Configurations

Adding the heap segment in PSRAM

Stack Segment in PSRAM

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Linker Configurations

Adding the stack segment in PSRAM

Text Segment in PSRAM

Device > Si91x > MCU > Peripheral > PSRAM Driver > PSRAM Linker Configurations

Adding the text segment in PSRAM

SDIO Secondary

Device > Si91x > MCU > Peripheral > SDIO Slave Driver

API for SDIO secondary driver

SDIO Slave Driver

Device > Si91x > MCU > Peripheral > SDIO Slave Driver

SDIO slave driver

ADC

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP ADC peripheral

BOD

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP BOD peripheral

Calendar

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP Calendar

Comparator

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP Comparator

CTS

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP CTS peripheral

DAC

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP digital-to-analog converter (DAC)

DMA

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP DMA peripheral

GPIO

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP GPIO ports

Low-Power Debug

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

Debug functionality in low power mode

I2C

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP I2C peripheral

I2S

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP I2S peripheral

IR

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP IR peripheral

SSI

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP SSI peripheral

SysRTC

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP SysRTC peripheral

UART

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP UART peripheral

ULP Timer

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP timer peripheral

User Files

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP user files execution from random-access memory (RAM)

Watchdog Timer

Device > Si91x > MCU > Service > Power Manager > ULP Peripheral

ULP watchdog timer

Drivers#

Component Name

Component Category Path

Description

Button

Device > Si91x > MCU > Hardware

API for the button driver

Joystick

Device > Si91x > MCU > Hardware

API for the joystick peripheral driver

LED

Device > Si91x > MCU > Hardware

API for the light-emitting diode (LED) peripheral driver

Memory LCD SPI driver

Device > Si91x > MCU > Hardware

API for the memory liquid crystal display (LCD) peripheral driver over the Serial Peripheral Interface (SPI)

Si70xx Humidity and Temperature Sensor

Device > Si91x > MCU > Hardware

API for the Si70XX humidity and temperature sensor driver

Services#

Component Name

Component Category Path

Description

Sensor Hub

Device > Si91x > MCU > Service

API for the sensor hub on the SiWx91x

NVM3 Common Flash

Device > Si91x > MCU > Service

Non-volatile memory (NVM3) API for SiWx91x common flash chip variants

NVM3 Dual Flash

Device > Si91x > MCU > Service

NVM3 API for SiWx91x dual flash chip variants

NVM3 for Si91x

Device > Si91x > MCU > Service

Common features for NVM3 APIs

IO Stream Si91x

Device > Si91x > MCU > Service

Data transfer over physical communication interfaces

Sleep Timer for Si91x

Device > Si91x > MCU > Service

Sleep timers

Sleep Timer SysRTC HAL

Device > Si91x > MCU > Service

Sleep timers using the system real-time clock (SysRTC)

Sleep Timer ULP Timer HAL

Device > Si91x > MCU > Service

Sleep timers using the ultra low power (ULP) timer

Power Manager

Device > Si91x > MCU > Service > Power Manager

API for SiWx91x power management

Cryptography#

Component Name

Component Category Path

Description

AES

Device > Si91x > Wireless > Crypto

API for encyption using the Advanced Encryption Standard (AES) method

ATTESTATION

Device > Si91x > Wireless > Crypto

API for performing attestation of the SiWx91x using cryptographic methods

CCM

Device > Si91x > Wireless > Crypto

API for encryption using the counter with cipher block chaining message authentication code (CCM) method

CHACHAPOLY

Device > Si91x > Wireless > Crypto

API for encryption using the ChaChaPoly method

Crypto - Common

Device > Si91x > Wireless > Crypto

API for cryptographic functionality

CRYPTO MULTITHREAD

Device > Si91x > Wireless > Crypto

Thread-safe mechanism in cryptography hardware accelerators

Crypto - Utility

Device > Si91x > Wireless > Crypto

API for cryptographic utilities

ECDH

Device > Si91x > Wireless > Crypto

API for encryption using the elliptic-curve Diffie-Hellman (ECDH) method

GCM

Device > Si91x > Wireless > Crypto

API for the Galois/Counter Mode (GCM) of operation

HMAC

Device > Si91x > Wireless > Crypto

API for encryption using the hash-based message authentication code (HMAC) method

PSA WRAP

Device > Si91x > Wireless > Crypto

API for Platform Security Architecture (PSA) standard cryptography using key wrap algorithms

SHA

Device > Si91x > Wireless > Crypto

API for encryption using the secure hash algorithm (SHA) method

TRNG

Device > Si91x > Wireless > Crypto

API for the True Random Number Generator (TRNG) algorithm

WRAP

Device > Si91x > Wireless > Crypto

API for encryption using key wrap algorithms

PSA AEAD

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptography with the authenticated encryption with associated data (AEAD) method

PSA AES

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptography with the AES method

PSA Crypto - Utility

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptographic utilities

PSA ECDH

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptography with the ECDH method

PSA HMAC

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptography with the HMAC method

PSA SHA

Device > Si91x > Wireless > PSA Crypto

API for PSA standard cryptography with the SHA method

PSA TRNG

Device > Si91x > Wireless > PSA Crypto

API for the PSA standard TRNG algorithm

Network Protocols#

Component Name

Component Category Path

Description

SNTP Client

Service

API for Simple Network Time Protocol (SNTP) client functionality

Application Protocols#

Component Name

Component Category Path

Description

AWS IoT Device SDK

Third Party

API for accessing the Amazon Web Services (AWS) Internet-of-Things (IoT) cloud service

AZURE FreeRTOS Middleware

Third Party

AZURE IoT Device SDK for Embedded C

Core MQTT

Third Party

Core MQTT

HTTP Client

Service

API for Hyper-Text Transfer Protocol (HTTP) client functionality

HTTP Server

Service

API for Hyper-Text Transfer Protocol (HTTP) server functionality

MQTT Client

Service

API for Message Queue Telemetry Transport (MQTT) client functionality

MDNS

Service

API for utilizing the multicast domain name service (mDNS) standard protocol to advertise services over the network

Built-In Command Database

Service > Console

Built-in console commands for WiSeConnect SDK v3.x features

Console

Service > Console

Console command-line interpreter (CLI) functionality

Console Variables

Service > Console

Functionality for reading and writing console variables