Radio Interfaces#

Radio Interfaces#

The Radio Interfaces module provides interfaces for interacting with radio hardware within the Sidewalk SDK. These interfaces ensure consistent and platform-independent access to radio functionalities, such as transmission, reception, and configuration of radio parameters. Developers can create applications that are portable across different hardware platforms while maintaining consistent radio behavior and performance.

The Radio Interfaces module includes support for various radio operations, including:

  • Transmission and Reception: Interfaces for sending and receiving data over the radio.

  • Configuration: Interfaces for configuring radio parameters such as data rate, channel, and power settings.

  • Event Handling: Mechanisms for handling radio events such as transmission completion, reception completion, and errors.

  • State Management: Interfaces for managing the state of the radio, including transitions between different states such as sleep, standby, and active modes.

By utilizing the Radio Interfaces module, developers can ensure that their applications can effectively communicate over the radio within the Amazon Sidewalk network, regardless of the underlying hardware platform.

Modules#

FSK Interface

LoRa Interface

Sub-GHz Interface