You are viewing documentation for version:
PDFSidewalk phy lora packet parameters.
Public Attribute Documentation#
preamble_length#
uint16_t sid_pal_radio_lora_packet_params_t::preamble_length
Length of the preamble
header_type
uint8_t sid_pal_radio_lora_packet_params_t::header_type
Type of the header
payload_length#
uint8_t sid_pal_radio_lora_packet_params_t::payload_length
Length of the payload
crc_mode#
uint8_t sid_pal_radio_lora_packet_params_t::crc_mode
Type of the CRC
invert_IQ#
uint8_t sid_pal_radio_lora_packet_params_t::invert_IQ
IQ inversion