Ensure Access to the Amazon Sidewalk Network#
When it executes, the "out-of-the-box" demo firmware on the Silicon Labs Kit forms a Sidewalk endpoint. To reach the cloud, this device must be in range of a suitable Amazon Sidewalk gateway.
Sidewalk Network Coverage#
Amazon currently supports the Amazon Sidewalk network only on gateways that communicate with AWS from US-based IP addresses.
⚠ WARNING ⚠: Regional regulations may also restrict unauthorized usage of the Sidewalk-supported sub-GHz bands outside of the United States. Consult local laws and ensure compliance (radio isolation by RF chamber, etc.) as needed. See Using Sidewalk Gateways Outside the USA for more information.
You may already have access to the Amazon Sidewalk network at your location. Amazon provides a Sidewalk Network Coverage map you can use to see if this is likely: https://coverage.sidewalk.amazon.


Set up a Gateway#
If you aren't already in range of a Sidewalk gateway, you can easily create your own.
The list of Amazon Sidewalk gateways and their supported capabilities is available at the following link: https://docs.sidewalk.amazon/introduction/sidewalk-gateways.html
The Ring Bridge 2nd generation is the recommended Amazon Sidewalk gateway for development purposes.
Follow the standard product configuration procedures, and make sure to enable Sidewalk support on your gateway so it will access the Sidewalk network.
Ⓘ INFO Ⓘ: To enable Sidewalk support, visit Enable or Disable Amazon Sidewalk for Your Account for more help.
For more information on this topic, see the Getting Started Prerequisites page.
Next Step: Run the Demo#
After you have access to the Amazon Sidewalk network, you are ready to Run the Demo.