Sidewalk Phy settings to configure radio prior to transmission and reception.

Public Attribute Documentation#

data_rate#

sid_pal_radio_data_rate_t sid_pal_radio_packet_cfg_t::data_rate

Data rate for the packet


channel#

uint8_t sid_pal_radio_packet_cfg_t::channel

Channel on which the packet will be transmitted or received


invert_IQ#

uint8_t sid_pal_radio_packet_cfg_t::invert_IQ

Flag to indicate if IQ inversion is enabled


preamble_len#

uint16_t sid_pal_radio_packet_cfg_t::preamble_len

Length of the preamble


symbol_timeout#

uint32_t sid_pal_radio_packet_cfg_t::symbol_timeout

Symbol timeout value


crc_enabled#

bool sid_pal_radio_packet_cfg_t::crc_enabled

Flag to indicate if CRC is enabled


side_sf_enabled#

bool sid_pal_radio_packet_cfg_t::side_sf_enabled

Flag to indicate if Sidewalk SF is enabled