Type definitions#
Modules#
Enumerations#
Describes the bit order of messages exchanged on serial bus interface.
Describes the client selection or deselection.
Typedefs#
Callback delivered by the backend as bytes arrive on the bus.
Enumeration Documentation#
sid_pal_serial_bus_bit_order#
sid_pal_serial_bus_bit_order
Describes the bit order of messages exchanged on serial bus interface.
| Enumerator | |
|---|---|
| SID_PAL_SERIAL_BUS_BIT_ORDER_MSB_FIRST | Most significant bit first. |
| SID_PAL_SERIAL_BUS_BIT_ORDER_LSB_FIRST | Least significant bit first. |
sid_pal_serial_bus_client_select#
sid_pal_serial_bus_client_select
Describes the client selection or deselection.
| Enumerator | |
|---|---|
| SID_PAL_SERIAL_BUS_CLIENT_DESELECT | Deselect the serial bus client |
| SID_PAL_SERIAL_BUS_CLIENT_SELECT | Select the serial bus client |
Typedef Documentation#
sid_pal_serial_bus_rx_cb_t#
typedef void(* sid_pal_serial_bus_rx_cb_t) (const uint8_t *data, size_t len, void *context) )(const uint8_t *data, size_t len, void *context)
Callback delivered by the backend as bytes arrive on the bus.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | data | received bytes (never NULL when len > 0) | |
| [in] | len | number of valid bytes in | |
| [in] | context | the context registered with set_rx_callback |
Invoked from the backend's receive context (typically an ISR on UART backends). The callback MUST return quickly and MUST NOT call back into the bus interface – copy the bytes into caller-owned storage and defer any real work. data is only valid for the duration of the call.