You are viewing documentation for version:1.0.0Table of Contents by Wireless Use Case#NameEmbedded to EmbeddedEmbedded to GatewayEmbedded to MobileWirelessAdding Custom CLIProprietary RailAir Quality Monitor application with BLE✔BLEApple Notification Center Service✔BLEBLE Ethernet Gateway✔BLEBLE HID Keyboard✔BLEBLE IR Generator Example✔BLEBLE man-in-the-middle example✔BLEBLE SPP with Windows✔BLEBluetooth - RSSI based room finding✔✔BLEBluetooth Cellular Gateway with BG 96B✔BLEBluetooth Explorer Kit accelerometer example using BMA400 sensor with SPI bus✔BLEBluetooth Module Explorer Kit HRM/SpO2 Software Demo using MAXM86161 sensor✔BLEBluetooth Module Explorer Kit HRM/SpO2 Software Demo using MAXM86161 sensor and OLED display✔BLEbtmesh_data_log✔Bluetooth MeshCompanion example for KBA - A reliable way for SED to receive asynchronous transmissions from other devices without frequent polling✔ZigbeeConnect Multi-Region Sensor✔Proprietary ConnectContact SensorZWaveControlling LEDs from a Smartphone✔BLEDeprecation NoticeBLEDistance Monitor example application using VL53L1X distance sensor and BLE✔BLEDoor lock example application with BLE✔BLEEnvironment humidity and temperature data logger with BLE✔✔BLEExplorer Kit Bluetooth accelerometer example using I2C bus BMA400 accelerometer✔BLEExplorer Kit Bluetooth barometer example using I2C bus DPS310 pressure sensor✔BLEExplorer Kit Bluetooth example using the I2C-bus Joystick and the SPI-bus 7-segment LED display✔BLEGreen Power gateway example✔ZigbeeHealth Care - Blood Glucose Meters ✔BLEHealth Care - Continuous Glucose Monitoring✔BLEHow to optimize the current consumption of Long Preamble Duty Cycle application on FG14Proprietary RailHow to Test Sensitivity of Long Range DSSS PHY on E4432BProprietary RailImplementing OTA Firmware Update in User Application✔BLEImplementing Wireless Direct Test Mode (DTM)✔✔BLELarge Network Testing guidelinesZigbeeLog System✔✔BLEManufacturing Library Extension✔ZigbeeMesh Room Monitor application✔✔Bluetooth MeshMIDI over BLE✔BLEMLX90632 IrThermo 3 click Bluetooth example✔BLEMovement Detection application with BLE✔BLEMulti-Slave Multi-Master Dual-Topology Example✔✔BLENCI PN71x0 T2T Read✔NFCNCI PN71x0 T2T Write✔NFCNT3H2111 and NT3H2211✔BLENT3H2x11 Field Detection✔NFCNT3H2x11 Format T2T✔NFCNT3H2x11 I2C Read Tag✔NFCNT3H2x11 I2C Write Tag NDEF✔NFCOptimization on EM2 Current Consumption of the Sleepy Z3Switch Example Project in EmberZNet 7.0✔ZigbeeOptimization on the EM2 Current Consumption of the DynamicMultiprotocolLightSed Example Project✔ZigbeeOptimize Boot-up Rejoin✔ZigbeePeople counting application with BLE✔BLERAIL Using Token on SDKv3.xProprietary RailReporting Battery Voltage over BLE✔BLERFID Card Scan over BLE✔BLERHT Si7021 Zigbee Sleepy End-Device and Gateway example✔ZigbeeSecure Device Attestation and Application Layer Encryption✔BLESecure SPP (Serial Port Profile) over BLE✔BLESPP (Serial Port Profile) over BLE✔BLESwitching Between Two Zigbee Applications✔ZigbeeSwitching Between Two Zigbee Applications Using Slot Manager✔ZigbeeThermometer Example with EFR32 Internal Temperature Sensor✔BLETutorial OverviewZigbeeUploading Images to Internal/External Flash Using OTA DFU✔BLEUsing EM4 Energy Mode in Bluetooth Beacon AppBLEWho is this boot camp for?ZigbeeZ-Wave Ambient Light Sensor ExampleZWaveZ-Wave Gesture Sensor Wall Controller ExampleZWaveZ-Wave Motion Sensor PIR ExampleZWaveZigbee Battery Monitor Example✔ZigbeeZigbee Motion Sensor PIR ExampleZigbeeZigbee Network Testing Plugin✔ZigbeeZigbee RTC Time✔ZigbeeZigbee Smart Lighting with PIR and Ambient light sensorZigbeeZigbee Source Routing Repair Plugin✔ZigbeeZigBee Virtual UART example✔Zigbee