Repositories#

The hardware drivers and application examples are stored on Github in public Git repositories.

Hardware Drivers#

These are drivers for third-party devices such as sensors, displays, and interfaces for various types of hardware.

Deprecated repository, the newly developed drivers for the application examples are stored in the Third-Party Hardware Drivers GSDK Extension.

https://github.com/SiliconLabs/platform_hardware_drivers

Third-Party Hardware Drivers - GSDK Extension#

SDK Extension for Third-Party hardware drivers for EFM32 and EFR32.

https://github.com/SiliconLabs/third_party_hw_drivers_extension

Wireless Applications by technology#

The Application Examples Program provides real-life application examples for most of the popular wireless technologies. These examples are stored in separate repositories.

https://github.com/SiliconLabs/application_examples

Bluetooth#

Proprietary#

Thread#

Wi-Fi#

Zigbee#

Z-Wave#

Matter#

EFM32-EFR32 Platform#

Utilities and Training Materials#

Trainings

IoT Utilities