Table of Contents by Wireless Use Case#

Name

Embedded to Embedded

Embedded to Gateway

Embedded to Mobile

Wireless

Adding Custom CLI

Proprietary Rail

Air Quality Monitor application with BLE

BLE

Apple Notification Center Service

BLE

BLE Ethernet Gateway

BLE

BLE HID Keyboard

BLE

BLE IR Generator Example

BLE

BLE man-in-the-middle example

BLE

BLE SPP with Windows

BLE

Bluetooth - RSSI based room finding

BLE

Bluetooth Cellular Gateway with BG 96B

BLE

Bluetooth Explorer Kit accelerometer example using BMA400 sensor with SPI bus

BLE

Bluetooth Module Explorer Kit HRM/SpO2 Software Demo using MAXM86161 sensor

BLE

Bluetooth Module Explorer Kit HRM/SpO2 Software Demo using MAXM86161 sensor and OLED display

BLE

btmesh_data_log

Bluetooth Mesh

Companion example for KBA - A reliable way for SED to receive asynchronous transmissions from other devices without frequent polling

Zigbee

Connect Multi-Region Sensor

Proprietary Connect

Contact Sensor

ZWave

Controlling LEDs from a Smartphone

BLE

Deprecation Notice

BLE

Distance Monitor example application using VL53L1X distance sensor and BLE

BLE

Door lock example application with BLE

BLE

Environment humidity and temperature data logger with BLE

BLE

Explorer Kit Bluetooth accelerometer example using I2C bus BMA400 accelerometer

BLE

Explorer Kit Bluetooth barometer example using I2C bus DPS310 pressure sensor

BLE

Explorer Kit Bluetooth example using the I2C-bus Joystick and the SPI-bus 7-segment LED display

BLE

Green Power gateway example

Zigbee

Health Care - Blood Glucose Meters

BLE

Health Care - Continuous Glucose Monitoring

BLE

How to optimize the current consumption of Long Preamble Duty Cycle application on FG14

Proprietary Rail

How to Test Sensitivity of Long Range DSSS PHY on E4432B

Proprietary Rail

Implementing OTA Firmware Update in User Application

BLE

Implementing Wireless Direct Test Mode (DTM)

BLE

Large Network Testing guidelines

Zigbee

Log System

BLE

Manufacturing Library Extension

Zigbee

Mesh Room Monitor application

Bluetooth Mesh

MIDI over BLE

BLE

MLX90632 IrThermo 3 click Bluetooth example

BLE

Movement Detection application with BLE

BLE

Multi-Slave Multi-Master Dual-Topology Example

BLE

NCI PN71x0 T2T Read

NFC

NCI PN71x0 T2T Write

NFC

NT3H2111 and NT3H2211

BLE

NT3H2x11 Field Detection

NFC

NT3H2x11 Format T2T

NFC

NT3H2x11 I2C Read Tag

NFC

NT3H2x11 I2C Write Tag NDEF

NFC

Optimization on EM2 Current Consumption of the Sleepy Z3Switch Example Project in EmberZNet 7.0

Zigbee

Optimization on the EM2 Current Consumption of the DynamicMultiprotocolLightSed Example Project

Zigbee

Optimize Boot-up Rejoin

Zigbee

People counting application with BLE

BLE

RAIL Using Token on SDKv3.x

Proprietary Rail

Reporting Battery Voltage over BLE

BLE

RFID Card Scan over BLE

BLE

RHT Si7021 Zigbee Sleepy End-Device and Gateway example

Zigbee

Secure Device Attestation and Application Layer Encryption

BLE

Secure SPP (Serial Port Profile) over BLE

BLE

SPP (Serial Port Profile) over BLE

BLE

Switching Between Two Zigbee Applications

Zigbee

Switching Between Two Zigbee Applications Using Slot Manager

Zigbee

Thermometer Example with EFR32 Internal Temperature Sensor

BLE

Tutorial Overview

Zigbee

Uploading Images to Internal/External Flash Using OTA DFU

BLE

Using EM4 Energy Mode in Bluetooth Beacon App

BLE

Who is this boot camp for?

Zigbee

Z-Wave Ambient Light Sensor Example

ZWave

Z-Wave Gesture Sensor Wall Controller Example

ZWave

Z-Wave Motion Sensor PIR Example

ZWave

Zigbee Battery Monitor Example

Zigbee

Zigbee Motion Sensor PIR Example

Zigbee

Zigbee Network Testing Plugin

Zigbee

Zigbee RTC Time

Zigbee

Zigbee Smart Lighting with PIR and Ambient light sensor

Zigbee

Zigbee Source Routing Repair Plugin

Zigbee

ZigBee Virtual UART example

Zigbee