NCP Interface#
Component that provides the Bluetooth Network Co-Processor (NCP) communication interface. This is a No-Code component.
Enumerations#
NCP error type.
Functions#
Macros#
Enumeration Documentation#
sl_ncp_error_t#
sl_ncp_error_t
NCP error type.
Enumerator | |
---|---|
SL_NCP_ERROR_RUNTIME | |
SL_NCP_ERROR_RECEIVE | |
SL_NCP_ERROR_TIMER | |
SL_NCP_ERROR_ENCRYPT | |
SL_NCP_ERROR_RSP_BUFFER | |
SL_NCP_ERROR_EVT_ENQUE | |
SL_NCP_ERROR_EVT_DEQUE |
Function Documentation#
sl_ncp_init#
void sl_ncp_init (void )
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
NCP initialization function.
sl_ncp_rta_ready#
void sl_ncp_rta_ready (void )
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
NCP runtime ready.
sl_ncp_user_cmd_message_to_target_cb#
void sl_ncp_user_cmd_message_to_target_cb (void * data)
Type | Direction | Argument Name | Description |
---|---|---|---|
void * | [in] | data | Data received from NCP through UART. |
User command (message_to_target) handler callback.
Handle user defined commands received from NCP-host.
sl_ncp_user_cs_cmd_message_to_target_cb#
void sl_ncp_user_cs_cmd_message_to_target_cb (const void * data)
Type | Direction | Argument Name | Description |
---|---|---|---|
const void * | [in] | data | Data received from NCP through UART. |
CS user command (message_to_target) handler callback.
Handle CS defined user commands received from NCP-host.
sl_ncp_user_cmd_message_to_target_rsp#
void sl_ncp_user_cmd_message_to_target_rsp (sl_status_t result, uint8_t len, uint8_t * data)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_status_t | [out] | result | Result of the response to the command received. |
uint8_t | [out] | len | Message length. |
uint8_t * | [out] | data | Data to send to NCP. |
Send user command (message_to_target) response.
Send response to user defined (message_to_target) command to NCP-host.
sl_ncp_user_evt_message_to_host#
void sl_ncp_user_evt_message_to_host (uint8_t len, uint8_t * data)
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [out] | len | Message length. |
uint8_t * | [out] | data | Data to send to NCP. |
Send user event (message_to_host).
Send user defined (message_to_host) event to NCP-host.
sl_ncp_local_evt_process#
bool sl_ncp_local_evt_process (sl_bt_msg_t * evt)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_bt_msg_t * | [in] | evt | Bluetooth event. |
Local event processor for handling Bluetooth events in the application.
Note
This function can be implemented in the application.
sl_ncp_local_common_evt_process#
bool sl_ncp_local_common_evt_process (sl_bt_msg_t * evt)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_bt_msg_t * | [in] | evt | Bluetooth event. |
Process Bluetooth events locally using template contribution.
Note
Automatically calls sl_ncp_local_evt_process after all component callback is finished.
sl_ncp_on_error#
void sl_ncp_on_error (sl_ncp_error_t error, sl_status_t status)
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_ncp_error_t | N/A | error | error type |
sl_status_t | N/A | status | status code |
NCP runtime error callback.
Note
The error callback is called when an error has occurred in the runtime context. The weak implementation asserts. It can be overridden in user code by adding a strong implementation.