Channel Sounding#
Channel Sounding.
This class provides commands and events for Channel Sounding (CS) between Bluetooth devices.
Any CS command that involves a remote device requires that the connection with the remote device is encrypted.
Modules#
sl_bt_evt_cs_security_enable_complete
sl_bt_evt_cs_procedure_enable_complete
sl_bt_evt_cs_read_remote_supported_capabilities_complete
Enumerations#
Specifies the role for the device during CS procedure.
Defines the status of a given role for an CS capable device.
Defines the CS procedure state for the device.
Defines the different modes for CS steps.
Defines the Round Trip Time (RTT) payload types used during the CS sequence.
Specifies the CS channel selection algorithms.
Specifies the ch3c shapes.
Describes the current status of the procedure or subevents.
Specifies the role for the device during CS procedure.
Specifies the Signal Noise Ration (SNR) used to control transmission of CS_SYNC packets. Currently the SiSDK does not support the SNR control adjustment.
Functions#
Macros#
Enumeration Documentation#
sl_bt_cs_role_t#
sl_bt_cs_role_t
Specifies the role for the device during CS procedure.
| Enumerator | |
|---|---|
| sl_bt_cs_role_initiator | (0x0) The device will initiate the procedure |
| sl_bt_cs_role_reflector | (0x1) The device will reciprocate transmission |
sl_bt_cs_role_status_t#
sl_bt_cs_role_status_t
Defines the status of a given role for an CS capable device.
| Enumerator | |
|---|---|
| sl_bt_cs_role_status_disable | (0x0) The given role is disabled |
| sl_bt_cs_role_status_enable | (0x1) The given role is enabled |
sl_bt_cs_procedure_state_t#
sl_bt_cs_procedure_state_t
Defines the CS procedure state for the device.
| Enumerator | |
|---|---|
| sl_bt_cs_procedure_state_disabled | (0x0) CS procedures are disabled |
| sl_bt_cs_procedure_state_enabled | (0x1) CS procedures are enabled |
sl_bt_cs_mode_t#
sl_bt_cs_mode_t
Defines the different modes for CS steps.
| Enumerator | |
|---|---|
| sl_bt_cs_mode_rtt | (0x1) Round Trip Time (RTT) measurement |
| sl_bt_cs_mode_pbr | (0x2) Phase-Based Ranging (PBR) measurement |
| sl_bt_cs_submode_disabled | (0xff) Submode disabled for the procedure. |
sl_bt_cs_rtt_type_t#
sl_bt_cs_rtt_type_t
Defines the Round Trip Time (RTT) payload types used during the CS sequence.
| Enumerator | |
|---|---|
| sl_bt_cs_rtt_type_aa_only | (0x0) RTT Access Address (AA) only |
| sl_bt_cs_rtt_type_fractional_32_bit_sounding | (0x1) RTT Fractional with 32-bit Sounding Sequence |
| sl_bt_cs_rtt_type_fractional_96_bit_sounding | (0x2) RTT Fractional with 96-bit Sounding Sequence |
| sl_bt_cs_rtt_type_fractional_32_bit_random | (0x3) RTT Fractional with 32-bit Random Sequence |
| sl_bt_cs_rtt_type_fractional_64_bit_random | (0x4) RTT Fractional with 64-bit Random Sequence |
| sl_bt_cs_rtt_type_fractional_96_bit_random | (0x5) RTT Fractional with 96-bit Random Sequence |
| sl_bt_cs_rtt_type_fractional_128_bit_random | (0x6) RTT Fractional with 128-bit Random Sequence |
sl_bt_cs_channel_selection_algorithm_t#
sl_bt_cs_channel_selection_algorithm_t
Specifies the CS channel selection algorithms.
| Enumerator | |
|---|---|
| sl_bt_cs_channel_selection_algorithm_3b | (0x0) Use Channel Selection Algorithm #3b for non-mode 0 CS steps |
| sl_bt_cs_channel_selection_algorithm_3c | (0x1) Use Channel Selection Algorithm #3c for non-mode 0 CS steps |
| sl_bt_cs_channel_selection_algorithm_user_shape_interleaved | (0x2) Use Interleaved shape for user specified channel sequence |
sl_bt_cs_ch3c_shape_t#
sl_bt_cs_ch3c_shape_t
Specifies the ch3c shapes.
| Enumerator | |
|---|---|
| sl_bt_cs_ch3c_shape_hat | (0x0) Use Hat shape for user specified channel sequence |
| sl_bt_cs_chc3_shape_interleaved | (0x1) Use Interleaved shape for user specified channel sequence |
sl_bt_cs_done_status_t#
sl_bt_cs_done_status_t
Describes the current status of the procedure or subevents.
| Enumerator | |
|---|---|
| sl_bt_cs_done_status_complete | (0x0) All results complete for the CS procedure or subevent |
| sl_bt_cs_done_status_partial_results_continue | (0x1) Partial results with more to follow |
| sl_bt_cs_done_status_aborted | (0xf) Current procedure and all subsequent subevents in the procedure aborted or current subevent aborted. |
sl_bt_cs_config_state_t#
sl_bt_cs_config_state_t
Specifies the role for the device during CS procedure.
| Enumerator | |
|---|---|
| sl_bt_cs_config_state_removed | (0x0) The CS device configuration is removed |
| sl_bt_cs_config_state_created | (0x1) The CS device configuration is created |
sl_bt_cs_snr_control_adjustment_t#
sl_bt_cs_snr_control_adjustment_t
Specifies the Signal Noise Ration (SNR) used to control transmission of CS_SYNC packets. Currently the SiSDK does not support the SNR control adjustment.
| Enumerator | |
|---|---|
| sl_bt_cs_snr_control_adjustment_not_applied | (0xff) SNR control adjustment not to be applied |
Function Documentation#
sl_bt_cs_security_enable#
sl_status_t sl_bt_cs_security_enable (uint8_t connection)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle |
Start or restart CS security start procedure for the specified connection. This command returns SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY if the connection is not encrypted.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if the device is not the central in the connection.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_security_enable_complete - Triggered when CS security start procedure has completed.
sl_bt_cs_set_default_settings#
sl_status_t sl_bt_cs_set_default_settings (uint8_t connection, uint8_t initiator_status, uint8_t reflector_status, uint8_t antenna_identifier, int8_t max_tx_power)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle |
| uint8_t | [in] | initiator_status | Enum sl_bt_cs_role_status_t. Enable or disable status of the Initiator role. Values:
|
| uint8_t | [in] | reflector_status | Enum sl_bt_cs_role_status_t. Enable or disable status of the Reflector role. Values:
|
| uint8_t | [in] | antenna_identifier | Antenna identifier to be used for CS sync packets.
|
| int8_t | [in] | max_tx_power | Maximum transmit power level to be used in all CS transmissions. Units: dBm.
|
Set the default CS settings for the specified connection. By default, all roles are disabled and the antenna is set to 1.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if the device is trying to disable a role for which a valid CS configuration is present.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_cs_create_config#
sl_status_t sl_bt_cs_create_config (uint8_t connection, uint8_t config_id, uint8_t create_context, uint8_t main_mode_type, uint8_t sub_mode_type, uint8_t min_main_mode_steps, uint8_t max_main_mode_steps, uint8_t main_mode_repetition, uint8_t mode_calibration_steps, uint8_t role, uint8_t rtt_type, uint8_t cs_sync_phy, const sl_bt_cs_channel_map_t * channel_map, uint8_t channel_map_repetition, uint8_t channel_selection_type, uint8_t ch3c_shape, uint8_t ch3c_jump, uint8_t reserved)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | The connection handle |
| uint8_t | [in] | config_id | CS configuration identifier.
|
| uint8_t | [in] | create_context | Defines in which device the created configuration will be written
|
| uint8_t | [in] | main_mode_type | Enum sl_bt_cs_mode_t. Main mode type. Values:
|
| uint8_t | [in] | sub_mode_type | Enum sl_bt_cs_mode_t. Sub mode type. Values:
|
| uint8_t | [in] | min_main_mode_steps | Minimum number of CS main mode steps to be executed prior to a sub mode step.
|
| uint8_t | [in] | max_main_mode_steps | Maximum number of CS main mode steps to be executed prior to a sub mode step.
|
| uint8_t | [in] | main_mode_repetition | Number of main mode steps taken from the end of the last CS subevent to be repeated at the beginning of the current CS subevent directly after the value r last Mode 0 step of that event.
|
| uint8_t | [in] | mode_calibration_steps | Number of Mode 0 steps to be included at the beginning of the test CS subevent
|
| uint8_t | [in] | role | Enum sl_bt_cs_role_t. Device's role during the CS procedure Values:
|
| uint8_t | [in] | rtt_type | Enum sl_bt_cs_rtt_type_t. RTT payload type used in the CS procedure Values:
|
| uint8_t | [in] | cs_sync_phy | Enum sl_bt_gap_phy_t. Used PHY for CS SYNC exchanges during a procedure Values:
|
| const sl_bt_cs_channel_map_t * | [in] | channel_map | A fixed length byte array of 10 bytes consisting of 80 1-bit fields. The nth such field (in the range 0 to 78) contains the value for the CS channel index n.
The most significant bit (79) is reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for CS. At least 15 channels shall be marked as used. |
| uint8_t | [in] | channel_map_repetition | Number of times the channel_map field will be cycled through for non-Mode 0 steps within an CS procedure.
|
| uint8_t | [in] | channel_selection_type | Enum sl_bt_cs_channel_selection_algorithm_t. Channel selection algorithm Values:
|
| uint8_t | [in] | ch3c_shape | Enum sl_bt_cs_ch3c_shape_t. Ch3c shape Values:
|
| uint8_t | [in] | ch3c_jump | Number of channels skipped in each rising and falling sequence.
|
| uint8_t | [in] | reserved | Reserved for future use. |
Create a new CS configuration in the local and remote controller. The role used in this command must be enabled prior to issuing this command using sl_bt_cs_set_default_settings command.
This command returns SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE if the local or the remote controller does not support that CS feature.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if there is no valid CS configuration previously created for the specified connection. These are created with the sl_bt_cs_set_default_settings.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if a previously created CS configuration is enabled or ongoing for the specified connection, by calling sl_bt_cs_procedure_enable.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_config_complete - Triggered when an CS configuration procedure completed
sl_bt_cs_remove_config#
sl_status_t sl_bt_cs_remove_config (uint8_t connection, uint8_t config_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle |
| uint8_t | [in] | config_id | CS configuration identifier
|
Remove an CS configuration from the local controller.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if the config_id does not exist .
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if there is one or more CS procedures enabled with the sl_bt_cs_procedure_enable command.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_config_complete - Triggered when an CS configuration procedure is completed
sl_bt_cs_set_channel_classification#
sl_status_t sl_bt_cs_set_channel_classification (const sl_bt_cs_channel_map_t * channel_map)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_bt_cs_channel_map_t * | [in] | channel_map | A fixed length byte array of 10 bytes consisting of 80 1-bit fields. The nth field (in the range 0 to 78) contains the value for the link layer channel index n.
The most significant bit (79) is reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for CS. |
Update the channel classification for CS. This classification persists until overwritten with a subsequent command or until the system is reset.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if this command was issued after less than one second before.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if less than 15 channels are enabled.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_cs_set_procedure_parameters#
sl_status_t sl_bt_cs_set_procedure_parameters (uint8_t connection, uint8_t config_id, uint16_t max_procedure_len, uint16_t min_procedure_interval, uint16_t max_procedure_interval, uint16_t max_procedure_count, uint32_t min_subevent_len, uint32_t max_subevent_len, uint8_t tone_antenna_config_selection, uint8_t phy, int8_t tx_pwr_delta, uint8_t preferred_peer_antenna, uint8_t snr_control_initiator, uint8_t snr_control_reflector)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | The connection handle |
| uint8_t | [in] | config_id | CS configuration identifier.
|
| uint16_t | [in] | max_procedure_len | Maximum duration for each measurement procedure. Value in units of 0.625 ms.
|
| uint16_t | [in] | min_procedure_interval | Minimum duration in number of connection events between consecutive measurement procedure.
|
| uint16_t | [in] | max_procedure_interval | Maximum duration in number of connection events between consecutive measurement procedure.
|
| uint16_t | [in] | max_procedure_count | Maximum number of CS procedures to be scheduled.
|
| uint32_t | [in] | min_subevent_len | Minimum suggested duration for each CS subevent. Units: microseconds.
|
| uint32_t | [in] | max_subevent_len | Maximum suggested duration for each CS subevent. Units: microseconds.
|
| uint8_t | [in] | tone_antenna_config_selection | Antenna configuration index
|
| uint8_t | [in] | phy | Enum sl_bt_gap_phy_t. PHY used by the controller to determine the base transmit power for the CS procedure. The final transmit power level will be the lesser of the configured maximum transmission power for the PHY and the sum of the connection transmission power and the remote controller's power delta. Values:
|
| int8_t | [in] | tx_pwr_delta | Indicates the recommended difference between the remote controller's power level for the CS tones and RTT packets and the power level for the PHY indicated by the PHY parameter. Units: dB.
|
| uint8_t | [in] | preferred_peer_antenna | Preferred peer-ordered antenna elements to be used by the remote device for the antenna configuration denoted by the tone antenna config selection.
|
| uint8_t | [in] | snr_control_initiator | Enum sl_bt_cs_snr_control_adjustment_t. The Signal Noise Ratio (SNR) control adjustment for the CS_SYNC transmissions of the initiator. Values:
|
| uint8_t | [in] | snr_control_reflector | Enum sl_bt_cs_snr_control_adjustment_t. The Signal Noise Ratio (SNR) control adjustment for the CS_SYNC transmissions of the reflector. Values:
|
Set the parameters for scheduling CS procedures with the remote device. The parameters set by this command become invalid after removing the config_id with sl_bt_cs_remove_config.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if the config_id does not exists or was previously removed with sl_bt_cs_remove_config
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if less than 15 channels are enabled.
This command returns SL_STATUS_BT_CTRL_INSUFFICIENT_CHANNELS if there are less than 15 channels available.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if the CS procedure has been previously enabled.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_cs_procedure_enable#
sl_status_t sl_bt_cs_procedure_enable (uint8_t connection, uint8_t enable, uint8_t config_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | The connection handle |
| uint8_t | [in] | enable | Enum sl_bt_cs_procedure_state_t. Enabled or disabled CS procedure state. Values:
|
| uint8_t | [in] | config_id | CS configuration identifier |
Enable or disable scheduling CS procedures with the remote device.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if the sl_bt_cs_set_procedure_parameters has not been called previosly for that config_id.
This command returns SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS if the config_id does not exists or was previously removed with sl_bt_cs_remove_config.
This command returns SL_STATUS_BT_CTRL_COMMAND_DISALLOWED if the CS procedure has been previously enabled by calling sl_bt_cs_procedure_enable.
This command returns SL_STATUS_BT_CTRL_INSUFFICIENT_CHANNELS if there are less than 15 channels available.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_procedure_enable_complete - Triggered when local controller has scheduled or disabled an CS procedure measurement
sl_bt_evt_cs_result - Triggered when local controller has results to report for every CS event within the CS procedure
sl_bt_cs_set_antenna_configuration#
sl_status_t sl_bt_cs_set_antenna_configuration (size_t antenna_element_offset_len, const uint8_t * antenna_element_offset)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| size_t | [in] | antenna_element_offset_len | Length of data in |
| const uint8_t * | [in] | antenna_element_offset | Offset of each antenna, each element is a signed 16-bit integer stored in two consecutive bytes in little-endian order. Units: 1 cm. |
Set the antenna configuration for the CS feature.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_cs_read_local_supported_capabilities#
sl_status_t sl_bt_cs_read_local_supported_capabilities (uint8_t * num_config, uint16_t * max_consecutive_procedures, uint8_t * num_antennas, uint8_t * max_antenna_paths, uint8_t * roles, uint8_t * modes, uint8_t * rtt_capability, uint8_t * rtt_aa_only, uint8_t * rtt_sounding, uint8_t * rtt_random_payload, uint8_t * cs_sync_phys, uint16_t * subfeatures, uint16_t * t_ip1_times, uint16_t * t_ip2_times, uint16_t * t_fcs_times, uint16_t * t_pm_times, uint8_t * t_sw_times, uint8_t * tx_snr_capability)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | num_config | The number of CS configurations supported per connection.
|
| uint16_t * | [out] | max_consecutive_procedures | The maximum number of consecutive CS procedures supported.
|
| uint8_t * | [out] | num_antennas | The number of antenna elements available for CS tone exchanges.
|
| uint8_t * | [out] | max_antenna_paths | The maximum number of antenna paths supported.
|
| uint8_t * | [out] | roles | This value is a bitmask of flags to indicate which CS roles are supported by the controller. Flags:
|
| uint8_t * | [out] | modes | This value is a bitmask of flags to indicate which Optional CS modes are supported. Flags:
|
| uint8_t * | [out] | rtt_capability | This value is a bitmask of flags to indicate which Round Trip Time (RTT) CS capabilities accuracy requirement in
|
| uint8_t * | [out] | rtt_aa_only | The support status of RTT Access Address(AA) in the local controller. When supported it establishes the number of SYNC changes needed to satisfy the precision requirements.
|
| uint8_t * | [out] | rtt_sounding | The support status of RTT Sounding is supported in the local controller. When supported it establishes the number of SYNC changes needed to satisfy the precision requirements.
|
| uint8_t * | [out] | rtt_random_payload | The support status of RTT Random Payload in the local controller. When supported it establishes the number of SYNC changes needed to satisfy the precision requirements.
|
| uint8_t * | [out] | cs_sync_phys | This value is a bitmask of flags to indicate which CS_SYNC packages supported in an specific PHY. Flags:
|
| uint16_t * | [out] | subfeatures | This value is a bitmask of flags to indicate which optional CS subfeatures are supported. Flags:
|
| uint16_t * | [out] | t_ip1_times | This value is a bitmask of flags to indicate which time durations of Time for Interlude Period 1 (IP1) are supported. Flags:
|
| uint16_t * | [out] | t_ip2_times | This value is a bitmask of flags to indicate which time durations of Time for Interlude Period 2 (IP2) are supported. Flags:
|
| uint16_t * | [out] | t_fcs_times | This value is a bitmask of flags to indicate which durations of Time for Frequency Change Spacing (FCS) are supported. Flags:
|
| uint16_t * | [out] | t_pm_times | This value is a bitmask of flags to indicate which time durations of Time for Phase Measurement (PM) are supported. Flags:
|
| uint8_t * | [out] | t_sw_times | Time in microseconds for the antenna switch period of the CS tones.
|
| uint8_t * | [out] | tx_snr_capability | This value is a bitmask of flags to indicate the supported SNR levels used in RTT packets. Flags:
|
Read the CS capabilities of the local controller.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_cs_read_remote_supported_capabilities#
sl_status_t sl_bt_cs_read_remote_supported_capabilities (uint8_t connection)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle |
Read the Channel Sounding (CS) capabilities of the remote controller.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_read_remote_supported_capabilities_complete - Triggered when local controller has the requested supported capabilities of the remote controller.
Macro Definition Documentation#
sl_bt_cmd_cs_set_channel_classification_id#
#define sl_bt_cmd_cs_set_channel_classification_idValue:
0x04590020
sl_bt_cmd_cs_set_procedure_parameters_id#
#define sl_bt_cmd_cs_set_procedure_parameters_idValue:
0x05590020
sl_bt_cmd_cs_set_antenna_configuration_id#
#define sl_bt_cmd_cs_set_antenna_configuration_idValue:
0x07590020
sl_bt_cmd_cs_read_local_supported_capabilities_id#
#define sl_bt_cmd_cs_read_local_supported_capabilities_idValue:
0x08590020
sl_bt_cmd_cs_read_remote_supported_capabilities_id#
#define sl_bt_cmd_cs_read_remote_supported_capabilities_idValue:
0x09590020
sl_bt_rsp_cs_set_channel_classification_id#
#define sl_bt_rsp_cs_set_channel_classification_idValue:
0x04590020
sl_bt_rsp_cs_set_procedure_parameters_id#
#define sl_bt_rsp_cs_set_procedure_parameters_idValue:
0x05590020
sl_bt_rsp_cs_set_antenna_configuration_id#
#define sl_bt_rsp_cs_set_antenna_configuration_idValue:
0x07590020
sl_bt_rsp_cs_read_local_supported_capabilities_id#
#define sl_bt_rsp_cs_read_local_supported_capabilities_idValue:
0x08590020
sl_bt_rsp_cs_read_remote_supported_capabilities_id#
#define sl_bt_rsp_cs_read_remote_supported_capabilities_idValue:
0x09590020