Advertiser PAST#
Advertiser PAST.
Transfer the synchronization information of a local active periodic advertising set to a remote device using Periodic Advertising Synchronization Transfer (PAST) over a connection.
Functions#
Macros#
Function Documentation#
sl_bt_advertiser_past_transfer#
sl_status_t sl_bt_advertiser_past_transfer (uint8_t connection, uint16_t service_data, uint8_t advertising_set)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle of the connection used to transmit the sync transfer |
| uint16_t | [in] | service_data | A value provided by the application for use by the peer device. |
| uint8_t | [in] | advertising_set | Handle of the periodic advertising set to transfer |
Transfer the synchronization information of an advertising set that is actively performing periodic advertising. The transfer happens over a connection.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_advertiser_past_transfer_over_pawr_advertiser#
sl_status_t sl_bt_advertiser_past_transfer_over_pawr_advertiser (uint8_t transferring_advertising_set, uint16_t service_data, uint8_t advertising_set, uint8_t repeat_count, size_t subevents_len, const uint8_t * subevents)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | transferring_advertising_set | The handle of the PAwR advertising set used to transfer the synchronization information to the synchronized devices. |
| uint16_t | [in] | service_data | A value provided by the application for use by the peer device. |
| uint8_t | [in] | advertising_set | Handle of the periodic advertising set to transfer |
| uint8_t | [in] | repeat_count | The number of times the synchronization information is sent on the specified subevents of
|
| size_t | [in] | subevents_len | Length of data in |
| const uint8_t * | [in] | subevents | Array of subevent indexes in which to send the synchronization information. If a zero-length array is provided, the synchronization information is sent in all subevents of |
Transfer the synchronization information of an advertising set that is actively performing periodic advertising. The transfer happens over a Periodic Advertising with Responses (PAwR) train.
Returns
SL_STATUS_OK if successful. Error code otherwise.