CS Reflector#

Channel Sounding (CS) Reflector role implementation for all BLE Channel Sounding apps.

Modules#

cs_reflector_config_t

connection_ctx_t

Enumerations#

enum
CS_SYNC_ANTENNA_1 = 1
CS_SYNC_ANTENNA_2 = 2
CS_SYNC_SWITCHING = 0xfe
CS_SYNC_ANTENNA_1 = 1
CS_SYNC_ANTENNA_2 = 2
CS_SYNC_SWITCHING = 0xfe
}

Functions#

bool
cs_reflector_identify(uint8_t conn_handle)
sl_status_t
cs_reflector_create(uint8_t conn_handle, cs_reflector_config_t *reflector_config)
sl_status_t
cs_reflector_delete(uint8_t conn_handle)
bool
cs_reflector_on_bt_event(sl_bt_msg_t *evt)
cs_rcm_get_connection_ctx(const uint8_t conn_handle)
sl_status_t
cs_rcm_add_new_initiator_connection(const uint8_t conn_handle)
void
cs_rcm_remove_initiator_connection(const uint8_t conn_handle)

Macros#

#define
CS_REFLECTOR_MAX_CONNECTIONS SL_BT_CONFIG_MAX_CONNECTIONS
#define
#define
#define

Enumeration Documentation#

cs_sync_antenna_t#

cs_sync_antenna_t
Enumerator
CS_SYNC_ANTENNA_1
CS_SYNC_ANTENNA_2
CS_SYNC_SWITCHING
CS_SYNC_ANTENNA_1
CS_SYNC_ANTENNA_2
CS_SYNC_SWITCHING

Function Documentation#

cs_reflector_identify#

bool cs_reflector_identify (uint8_t conn_handle)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]conn_handle

the connection handle to identify

Determine whether a connection handle has a reflector associated to it

Returns

  • true if the handle has an associated reflector instance, false otherwise


cs_reflector_create#

sl_status_t cs_reflector_create (uint8_t conn_handle, cs_reflector_config_t * reflector_config)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]conn_handle

the connection handle for which to create the reflector

cs_reflector_config_t *[in]reflector_config

reflector configuration parameters

Create a reflector for the given connection handle

Returns

  • status of the operation


cs_reflector_get_active_instance_count#

uint8_t cs_reflector_get_active_instance_count (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get the number of active reflector instances

Returns

  • the number of active reflector instances


cs_reflector_delete#

sl_status_t cs_reflector_delete (uint8_t conn_handle)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]conn_handle

the connection handle for which to delete the reflector

Delete the reflector associated with the given connection handle

Returns

  • status of the operation


cs_reflector_on_bt_event#

bool cs_reflector_on_bt_event (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

the Bluetooth stack event to handle

Handle a Bluetooth stack event

Returns

  • true to forward the message to the host in NCP case


cs_rcm_get_connection_ctx#

connection_ctx_t * cs_rcm_get_connection_ctx (const uint8_t conn_handle)
Parameters
TypeDirectionArgument NameDescription
const uint8_t[in]conn_handle

the connection handle to search for

Find the pointer to a connection context which belongs to the provided connection handle.

Returns

  • the pointer of the context corresponding to the provided connection handle, NULL if not found


cs_rcm_add_new_initiator_connection#

sl_status_t cs_rcm_add_new_initiator_connection (const uint8_t conn_handle)
Parameters
TypeDirectionArgument NameDescription
const uint8_t[in]conn_handle

the connection handle to register

Register a new initiator connection with the provided handle.

Returns

  • status of the operation


cs_rcm_remove_initiator_connection#

void cs_rcm_remove_initiator_connection (const uint8_t conn_handle)
Parameters
TypeDirectionArgument NameDescription
const uint8_t[in]conn_handle

the connection handle to remove

Remove an initiator connection with the provided handle.


cs_rcm_can_accept_new_connection#

bool cs_rcm_can_accept_new_connection (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Tell whether an additional connection can be accepted.

Returns

  • true if an additional connection can be accepted, false otherwise


cs_rcm_get_number_of_connections#

uint8_t cs_rcm_get_number_of_connections (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Show the number of active connections.

Returns

  • the number of active connections


Macro Definition Documentation#

CS_REFLECTOR_CS_EVENT_BUF_SIZE#

#define CS_REFLECTOR_CS_EVENT_BUF_SIZE
Value:
(16)

CS_REFLECTOR_MAX_CONNECTIONS#

#define CS_REFLECTOR_MAX_CONNECTIONS
Value:
SL_BT_CONFIG_MAX_CONNECTIONS

CS_REFLECTOR_MIN_TX_POWER_DBM#

#define CS_REFLECTOR_MIN_TX_POWER_DBM
Value:
(-3)

CS_REFLECTOR_MAX_TX_POWER_DBM#

#define CS_REFLECTOR_MAX_TX_POWER_DBM
Value:
(20)

CS_REFLECTOR_ANTENNA_OFFSET#

#define CS_REFLECTOR_ANTENNA_OFFSET
Value:
0

CS_REFLECTOR_CS_SYNC_ANTENNA#

#define CS_REFLECTOR_CS_SYNC_ANTENNA
Value:
CS_SYNC_SWITCHING

CS_REFLECTOR_LOG#

#define CS_REFLECTOR_LOG
Value:
1

CS_REFLECTOR_LOG_PREFIX#

#define CS_REFLECTOR_LOG_PREFIX
Value:
"[Reflector]"

REFLECTOR_CONFIG_DEFAULT#

#define REFLECTOR_CONFIG_DEFAULT
Value:
{ \
.max_tx_power_dbm = CS_REFLECTOR_MAX_TX_POWER_DBM, \
.cs_sync_antenna = CS_REFLECTOR_CS_SYNC_ANTENNA \
}