BT Event System Event Masks#

Event Mask values used with Event System.

When the component bluetooth_event_system_ipc is included in the application, the Bluetooth host stack events are published using the Event System provided by the event_system component. The constants in this group define the event masks used for Bluetooth host stack events.

Macros#

#define
SL_BT_EVENT_MASK_PUBLIC ((uint32_t) 0x01)

Event mask bit set in all public Bluetooth host events.

Macro Definition Documentation#

SL_BT_EVENT_MASK_PUBLIC#

#define SL_BT_EVENT_MASK_PUBLIC
Value:
((uint32_t) 0x01)

Event mask bit set in all public Bluetooth host events.