sl_bt_evt_gatt_server_notification_tx_completed#
Indicates that one or more GATT notifications have been transmitted.
By default, this event is not enabled on Bluetooth connections due to additional resource usages
Following enablers are required to enable the Bluetooth stack's functionality for supporting this event,
Include feature bluetooth_feature_resource_report in the application project.
Use command sl_bt_resource_enable_connection_tx_report to enable data packet TX status reports before this Bluetooth connection is established.
Modules#
sl_bt_evt_gatt_server_notification_tx_completed_s
Typedefs#
Macros#
#define
Identifier of the notification_tx_completed event.