Testing Commands#

Testing Commands.

Modules#

sl_bt_evt_test_dtm_completed

Enumerations#

enum
sl_bt_test_pkt_prbs9 = 0x0
sl_bt_test_pkt_11110000 = 0x1
sl_bt_test_pkt_10101010 = 0x2
sl_bt_test_pkt_11111111 = 0x4
sl_bt_test_pkt_00000000 = 0x5
sl_bt_test_pkt_00001111 = 0x6
sl_bt_test_pkt_01010101 = 0x7
sl_bt_test_pkt_pn9 = 0xfd
sl_bt_test_pkt_carrier = 0xfe
}

Test packet types supported by the stack.

enum
sl_bt_test_phy_1m = 0x1
sl_bt_test_phy_2m = 0x2
sl_bt_test_phy_125k = 0x3
sl_bt_test_phy_500k = 0x4
}

Test PHY types.

Functions#

sl_status_t
sl_bt_test_dtm_tx_v4(uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy, int8_t power_level)
sl_status_t
sl_bt_test_dtm_tx_cw(uint8_t packet_type, uint8_t channel, uint8_t phy, int16_t power_level)
sl_status_t
sl_bt_test_dtm_rx(uint8_t channel, uint8_t phy)
sl_status_t

Macros#

#define
sl_bt_cmd_test_dtm_tx_v4_id 0x030e0020
#define
sl_bt_cmd_test_dtm_tx_cw_id 0x040e0020
#define
sl_bt_cmd_test_dtm_rx_id 0x010e0020
#define
sl_bt_cmd_test_dtm_end_id 0x020e0020
#define
sl_bt_rsp_test_dtm_tx_v4_id 0x030e0020
#define
sl_bt_rsp_test_dtm_tx_cw_id 0x040e0020
#define
sl_bt_rsp_test_dtm_rx_id 0x010e0020
#define
sl_bt_rsp_test_dtm_end_id 0x020e0020

Enumeration Documentation#

sl_bt_test_packet_type_t#

sl_bt_test_packet_type_t

Test packet types supported by the stack.

Enumerator
sl_bt_test_pkt_prbs9

(0x0) PRBS9 packet payload

sl_bt_test_pkt_11110000

(0x1) 11110000 packet payload

sl_bt_test_pkt_10101010

(0x2) 10101010 packet payload

sl_bt_test_pkt_11111111

(0x4) 11111111 packet payload

sl_bt_test_pkt_00000000

(0x5) 00000000 packet payload

sl_bt_test_pkt_00001111

(0x6) 00001111 packet payload

sl_bt_test_pkt_01010101

(0x7) 01010101 packet payload

sl_bt_test_pkt_pn9

(0xfd) PN9 continuously modulated output

sl_bt_test_pkt_carrier

(0xfe) Unmodulated carrier


sl_bt_test_phy_t#

sl_bt_test_phy_t

Test PHY types.

Enumerator
sl_bt_test_phy_1m

(0x1) 1M PHY

sl_bt_test_phy_2m

(0x2) 2M PHY

sl_bt_test_phy_125k

(0x3) 125k Coded PHY

sl_bt_test_phy_500k

(0x4) 500k Coded PHY


Function Documentation#

sl_bt_test_dtm_tx_v4#

sl_status_t sl_bt_test_dtm_tx_v4 (uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy, int8_t power_level)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]packet_type

Enum sl_bt_test_packet_type_t. Packet type to transmit. Values:

  • sl_bt_test_pkt_prbs9 (0x0): PRBS9 packet payload

  • sl_bt_test_pkt_11110000 (0x1): 11110000 packet payload

  • sl_bt_test_pkt_10101010 (0x2): 10101010 packet payload

  • sl_bt_test_pkt_11111111 (0x4): 11111111 packet payload

  • sl_bt_test_pkt_00000000 (0x5): 00000000 packet payload

  • sl_bt_test_pkt_00001111 (0x6): 00001111 packet payload

  • sl_bt_test_pkt_01010101 (0x7): 01010101 packet payload

uint8_t[in]length

Packet length in bytes

  • Range: 0 to 255

uint8_t[in]channel

Bluetooth channel. Channel is (F - 2402) / 2, where F is frequency in MHz.

  • Range: 0 (2402 MHz) to 39 (2480 MHz)

uint8_t[in]phy

Enum sl_bt_test_phy_t. PHY to use. Values:

  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

int8_t[in]power_level

TX power level in unit dBm. Use specified or the nearest TX power level. The minimum -127 dBm is specified in the Bluetooth specification. However, a device may not support this low TX power. In addition, only some devices support 20 dBm TX power. Effective TX power will be limited by the global system TX power that can be set with the sl_bt_system_set_tx_power command. Values:

  • Range: -127 to +20

  • 0x7E: Use minimum TX power level the device supports.

  • 0x7F: Use the smallest of the maximum TX power level the device supports and the global maximum TX power setting in stack.

Start a transmitter test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

In the transmitter test, the device sends packets continuously with a fixed interval. The type and length of each packet is set by packet_type and length parameters. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY.

Stop the test using the sl_bt_test_dtm_end command.

For transmitter test with packet type sl_bt_test_pkt_pn9 or sl_bt_test_pkt_carrier, use the sl_bt_test_dtm_tx_cw command.

Starting a transmitter test while other Bluetooth activities are active will either result in an error response or cause functionality issues, hence make sure other Bluetooth activities are stopped when performing the test.

Returns

  • Command result

Events


sl_bt_test_dtm_tx_cw#

sl_status_t sl_bt_test_dtm_tx_cw (uint8_t packet_type, uint8_t channel, uint8_t phy, int16_t power_level)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]packet_type

Enum sl_bt_test_packet_type_t. Packet type to transmit. Values:

  • sl_bt_test_pkt_pn9 (0xfd): PN9 continuously modulated output

  • sl_bt_test_pkt_carrier (0xfe): Unmodulated carrier

uint8_t[in]channel

Bluetooth channel. Channel is (F - 2402) / 2,where F is frequency in MHz.

  • Range: 0 to 39

uint8_t[in]phy

Enum sl_bt_test_phy_t. PHY to use. Values:

  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

int16_t[in]power_level

TX power level. Unit: 0.1 dBm.

If the value exceeds the range of power level value, allowed by the device, the command will adjust the power level to the closest minimum or maximum value.

Start a transmitter test for a custom wave. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

In the custom wave transmitter test, the device continuously transmits the career. The parameter packet_type specifies the packet type. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY.

Stop the test using the sl_bt_test_dtm_end command.

Starting a transmitter test while other Bluetooth activities are active will either result in an error response or cause functionality issues, hence make sure other Bluetooth activities are stopped when performing the test.

Returns

  • Command result

Events


sl_bt_test_dtm_rx#

sl_status_t sl_bt_test_dtm_rx (uint8_t channel, uint8_t phy)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel

Bluetooth channel. Channel is (F - 2402) / 2, where F is frequency in MHz.

  • Range: 0 to 39

uint8_t[in]phy

Enum sl_bt_test_phy_t. PHY to use. Values:

  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

Start a receiver test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

Parameter phy specifies which PHY is used to receive the packets. All devices support at least 1M PHY.

The test may be stopped using sl_bt_test_dtm_end command. This will trigger another sl_bt_evt_test_dtm_completed event, which carries the number of packets received during the test.

Starting a receiver test while other Bluetooth activities are active will either result in an error response or cause functionality issues, hence make sure other Bluetooth activities are stopped when performing the test.

Returns

  • Command result

Events


sl_bt_test_dtm_end#

sl_status_t sl_bt_test_dtm_end (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

End a transmitter or a receiver test. When the command is processed by the radio and the test has ended, a sl_bt_evt_test_dtm_completed event is triggered.

Returns

  • Command result

Events