Sl_bt_peer_manager_filter#

Functions#

sl_status_t
sl_status_t
sl_status_t
sl_bt_peer_manager_set_filter_address_type(sl_bt_gap_address_type_t filter_addr_type)
sl_status_t
sl_bt_peer_manager_set_filter_device_name(const char *device_name, uint8_t device_name_len, bool full_match)
sl_status_t
sl_bt_peer_manager_set_filter_service_uuid16(sl_bt_uuid_16_t *service_uuid16)
sl_status_t
sl_status_t
sl_bt_peer_manager_set_filter_service_data(uint8_t *service_data, uint8_t service_data_offset, uint8_t service_data_len)
sl_status_t
sl_bt_peer_manager_set_filter_manufacturer_data(uint8_t *manufacturer_data, uint8_t manufacturer_data_offset, uint8_t manufacturer_data_len)
sl_status_t
bool
sl_bt_peer_manager_find_match(bd_addr *address, sl_bt_gap_address_type_t address_type, int8_t rssi, const uint8array *adv_data)
sl_status_t
sl_bt_peer_manager_str_to_address(const char *str, bd_addr *address)

Macros#

#define
SL_BT_PEER_MANAGER_FILTER_LOG 0

Function Documentation#

sl_bt_peer_manager_filter_init#

void sl_bt_peer_manager_filter_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize filtering.


sl_bt_peer_manager_set_filter_bt_address#

void sl_bt_peer_manager_set_filter_bt_address (bool enabled)
Parameters
TypeDirectionArgument NameDescription
bool[in]enabled

Enable or disable BT address filtering.

Enable/disable BT address filtering.


sl_bt_peer_manager_add_allowed_bt_address#

sl_status_t sl_bt_peer_manager_add_allowed_bt_address (bd_addr * filter_addr)
Parameters
TypeDirectionArgument NameDescription
bd_addr *[in]filter_addr

BT address to allow

Add a new allowed BT address.


sl_bt_peer_manager_remove_allowed_bt_address#

sl_status_t sl_bt_peer_manager_remove_allowed_bt_address (bd_addr * filter_addr)
Parameters
TypeDirectionArgument NameDescription
bd_addr *N/Afilter_addr

Remove a BT address from the allowed list.


sl_bt_peer_manager_set_filter_address_type#

sl_status_t sl_bt_peer_manager_set_filter_address_type (sl_bt_gap_address_type_t filter_addr_type)
Parameters
TypeDirectionArgument NameDescription
sl_bt_gap_address_type_t[in]filter_addr_type

Address type to set the filter to.

Set filter address type.


sl_bt_peer_manager_set_filter_device_name#

sl_status_t sl_bt_peer_manager_set_filter_device_name (const char * device_name, uint8_t device_name_len, bool full_match)
Parameters
TypeDirectionArgument NameDescription
const char *[in]device_name

Device name to set the filter to.

uint8_t[in]device_name_len

Length of the device name.

bool[in]full_match

If true, only full matches are accepted in the scan response.

Set filter device name.

Set the filter device name to the specified device name. The device name in the scan response will only be checked if the advertisement type is Shortened Local Name (0x08) or Complete Local Name (0x09).


sl_bt_peer_manager_set_filter_service_uuid16#

sl_status_t sl_bt_peer_manager_set_filter_service_uuid16 (sl_bt_uuid_16_t * service_uuid16)
Parameters
TypeDirectionArgument NameDescription
sl_bt_uuid_16_t *[in]service_uuid16

Service UUID16 to set the filter to.

Set filter service UUID16.

Set the filter service UUID16 to the specified service UUID16. The service UUID in the scan response will only be checked if the advertisement type is Incomplete List of 16-bit Service Class UUIDs or Complete List of 16-bit Service Class UUIDs.


sl_bt_peer_manager_set_filter_service_uuid128#

sl_status_t sl_bt_peer_manager_set_filter_service_uuid128 (uuid_128 * service_uuid128)
Parameters
TypeDirectionArgument NameDescription
uuid_128 *[in]service_uuid128

Service UUID128 to set the filter to.

Set filter service UUID128.

Set the filter service UUID128 to the specified service UUID128. The service UUID in the scan response will only be checked if the advertisement type is Incomplete List of 32-bit Service Class UUIDs or Complete List of 16-bit Service Class UUIDs.


sl_bt_peer_manager_set_filter_service_data#

sl_status_t sl_bt_peer_manager_set_filter_service_data (uint8_t * service_data, uint8_t service_data_offset, uint8_t service_data_len)
Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]service_data

Service data to set the filter to.

uint8_t[in]service_data_offset

Offset of the service data.

uint8_t[in]service_data_len

Length of the service data.

Set filter service data.

Set the filter service data to the specified service data. When processing the scan response, the search will start from the given offset until the given length using memcmp(). The service data in the scan response will only be checked if the advertisement type is Service Data - 128-bit UUID.


sl_bt_peer_manager_set_filter_manufacturer_data#

sl_status_t sl_bt_peer_manager_set_filter_manufacturer_data (uint8_t * manufacturer_data, uint8_t manufacturer_data_offset, uint8_t manufacturer_data_len)
Parameters
TypeDirectionArgument NameDescription
uint8_t *[in]manufacturer_data

Manufacturer data to set the filter to.

uint8_t[in]manufacturer_data_offset

Offset of the manufacturer data.

uint8_t[in]manufacturer_data_len

Length of the manufacturer data.

Set filter manufacturer data.

Set the filter manufacturer data to the specified manufacturer data. When processing the scan response, the search will start from the given offset until the given length using memcmp(). The manufacturer data in the scan response will only be checked if the advertisement type is Manufacturer Specific Data.


sl_bt_peer_manager_set_filter_rssi#

sl_status_t sl_bt_peer_manager_set_filter_rssi (int8_t rssi)
Parameters
TypeDirectionArgument NameDescription
int8_t[in]rssi

RSSI to set the filter to.

Set filter RSSI.

Set the filter RSSI (Signal strength indicator in the last received packet) to the specified RSSI. The RSSI in the scan response has to be greater than the set value. Units: dBm Range: -127 to +20


sl_bt_peer_manager_is_filter_set#

bool sl_bt_peer_manager_is_filter_set (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Check if there are any filters set.


sl_bt_peer_manager_reset_filter#

sl_status_t sl_bt_peer_manager_reset_filter (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Reset filters.

Reset all filters to default values.


sl_bt_peer_manager_find_match#

bool sl_bt_peer_manager_find_match (bd_addr * address, sl_bt_gap_address_type_t address_type, int8_t rssi, const uint8array * adv_data)
Parameters
TypeDirectionArgument NameDescription
bd_addr *[in]address

Address of the device.

sl_bt_gap_address_type_t[in]address_type

Address type of the device.

int8_t[in]rssi

RSSI of the device.

const uint8array *[in]adv_data

Advertising data of the device.

Find a match for the filters.

Check if the scan response matches the filters. There is an AND relationship between the filters, meaning that all filters must match for the function to return true.


sl_bt_peer_manager_is_filter_set_allowed#

bool sl_bt_peer_manager_is_filter_set_allowed (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_bt_peer_manager_str_to_address#

sl_status_t sl_bt_peer_manager_str_to_address (const char * str, bd_addr * address)
Parameters
TypeDirectionArgument NameDescription
const char *[in]str

Hexadecimal representation of the Bluetooth LE address with optional separator characters ':' or ' ', e.g. "AA:BB:CC:DD:EE:FF".

bd_addr *[out]address

Output.

Parse BT address from string.

Returns

  • Status of the operation.