Channel Sounding Test#
Channel Sounding Test.
This class provides optional test commands and events for CS between Bluetooth devices.
Modules#
sl_bt_evt_cs_test_end_completed
Enumerations#
Defines tone extension for CS test.
This defines sounding sequence marker for CS test.
Functions#
Macros#
Enumeration Documentation#
sl_bt_cs_test_tone_extension_t#
sl_bt_cs_test_tone_extension_t
Defines tone extension for CS test.
| Enumerator | |
|---|---|
| sl_bt_cs_test_tone_extension_both_without | (0x0) Initiator and Reflector tones sent without tone extension |
| sl_bt_cs_test_tone_extension_reflector_without | (0x1) Initiator tone sent with extension; Reflector tone sent without extension |
| sl_bt_cs_test_tone_extension_initiator_without | (0x2) Initiator tone sent without extension; Reflector tone sent with extension |
| sl_bt_cs_test_tone_extension_both_with | (0x3) Initiator and Reflector tones sent with extension |
| sl_bt_cs_test_tone_extension_round_robin | (0x4) Loop through values 0x00 to 0x03 |
sl_bt_cs_test_sounding_sequence_marker_t#
sl_bt_cs_test_sounding_sequence_marker_t
This defines sounding sequence marker for CS test.
| Enumerator | |
|---|---|
| sl_bt_cs_test_sounding_sequence_marker_1 | (0x0) Use 0b0011 as the Sounding Sequence marker |
| sl_bt_cs_test_sounding_sequence_marker_2 | (0x1) Use 0b1100 as the Sounding Sequence marker |
| sl_bt_cs_test_sounding_sequence_marker_round_robin | (0x2) Loop through 0b0011 and 0b1100 |
Function Documentation#
sl_bt_cs_test_start#
sl_status_t sl_bt_cs_test_start (uint8_t main_mode_type, uint8_t sub_mode_type, uint8_t main_mode_repetition, uint8_t mode_calibration_steps, uint8_t role, uint8_t rtt_type, uint8_t cs_sync_phy, uint8_t antenna_selection, const sl_bt_cs_subevent_length_t * subevent_len, uint16_t subevent_interval, uint8_t max_num_subevents, int8_t tx_power, uint8_t t_ip1_time, uint8_t t_ip2_time, uint8_t t_fcs_time, uint8_t t_pm_time, uint8_t t_sw_time, uint8_t tone_antenna_config, uint8_t reserved, uint8_t snr_control_initiator, uint8_t snr_control_reflector, uint16_t drbg_nonce, uint8_t channel_map_repetition, uint16_t override_config, size_t override_parameters_len, const uint8_t * override_parameters)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | main_mode_type | Enum sl_bt_cs_mode_t. Main mode type. Values :
|
| uint8_t | [in] | sub_mode_type | Enum sl_bt_cs_mode_t. Sub mode type. Values:
|
| uint8_t | [in] | main_mode_repetition | Number of main mode steps taken from the end of the last CS subevent to be repeated at the beginning of the current CS subevent directly after the last Mode 0 step of that event.
|
| uint8_t | [in] | mode_calibration_steps | Number of calibration mode steps to be included at the beginning of the test CS subevent
|
| uint8_t | [in] | role | Enum sl_bt_cs_role_t. Role during CS procedure Values:
|
| uint8_t | [in] | rtt_type | Enum sl_bt_cs_rtt_type_t. RTT payload type used in the CS procedure Values:
|
| uint8_t | [in] | cs_sync_phy | Enum sl_bt_gap_phy_t. Used PHY for CS_SYNC exchanges during a procedure Values:
|
| uint8_t | [in] | antenna_selection | Antenna identifier to be used for CS_SYNC packets, including mode-0 packets
|
| const sl_bt_cs_subevent_length_t * | [in] | subevent_len | CS subevent length in units of microseconds.
|
| uint16_t | [in] | subevent_interval | Interval between the start of two consecutive CS events. Units: 0.625 ms.
|
| uint8_t | [in] | max_num_subevents | The maximum allowed number of subevents in the procedure.
|
| int8_t | [in] | tx_power | Transmit power level for the transmission. Units: dBm.
|
| uint8_t | [in] | t_ip1_time | Idle time in microseconds between the RTT packets
|
| uint8_t | [in] | t_ip2_time | Interlude time in microseconds between the CS tones
|
| uint8_t | [in] | t_fcs_time | Time in microseconds for frequency changes
|
| uint8_t | [in] | t_pm_time | Time in microseconds for the phase measurement period of the CS tones
|
| uint8_t | [in] | t_sw_time | Time in microseconds for the antenna switch period of the CS tones
|
| uint8_t | [in] | tone_antenna_config | Antenna Configuration Index used during antenna switching
|
| uint8_t | [in] | reserved | Reserved for future use. |
| uint8_t | [in] | snr_control_initiator | Enum sl_bt_cs_snr_control_adjustment_t. The Signal Noise Ratio (SNR) control adjustment for the CS_SYNC transmissions of the initiator. Values:
|
| uint8_t | [in] | snr_control_reflector | Enum sl_bt_cs_snr_control_adjustment_t. The Signal Noise Ratio (SNR) control adjustment for the CS_SYNC transmissions of the reflector. Values:
|
| uint16_t | [in] | drbg_nonce | The DRBG_Nonce value determines octets 14 and 15 of the initial value of the DRBG nonce. |
| uint8_t | [in] | channel_map_repetition | Number of times the channel_map field will be cycled through for non-Mode 0 steps within an CS procedure.
|
| uint16_t | [in] | override_config | Configuration of the parameters in override_parameters. Please refer to the Bluetooth Specification document on the HCI_CS_Test comamnd for more information on the override configuration details. |
| size_t | [in] | override_parameters_len | Length of data in |
| const uint8_t * | [in] | override_parameters | Variable set of parameters. Please refer to the Bluetooth Specification document on the HCI_CS_Test comamnd for more information on the override parameters details. |
Start a single CS procedure using the given configuration. The reflector must be initialized before starting the initiator. To stop an ongoing test, use the sl_bt_test_dtm_end command.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_result - Triggered when local controller has results to report for every CS subevent within the CS procedure
sl_bt_cs_test_end#
sl_status_t sl_bt_cs_test_end (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Stops any ongoing CS test. When the local controller has sent all the remaining subevents for the ongoing procedure it will generate an sl_bt_evt_cs_test_end_completed event.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_test_end_completed - Triggered when local controller has stopped the CS procedure started with the sl_bt_cs_test_start command.