NCP Event Filter Interface#

Component that provides the Bluetooth Network Co-Processor (NCP) Event Filter interface. This is a No-Code component if used together with NCP Interface component.

Modules#

user_cmd_manage_event_filter

user_cmd_manage_event_filter.hdr

Functions#

void
sl_ncp_evt_filter_handler(user_cmd_manage_event_filter_t *cmd)
bool

Typedef Documentation#

evt_filter_t#

typedef uint32_t evt_filter_t

user_cmd_manage_event_filter_t#

typedef struct user_cmd_manage_event_filter user_cmd_manage_event_filter_t

Function Documentation#

sl_ncp_evt_filter_handler#

void sl_ncp_evt_filter_handler (user_cmd_manage_event_filter_t * cmd)
Parameters
TypeDirectionArgument NameDescription
user_cmd_manage_event_filter_t *[in]cmd

payload of manage event filter

User command (manage_event_filter) handler. This function processes the event filter command which is in the cmd parameter and according to it adds/removes/resets the events in the event filter array.


sl_ncp_evt_filter_is_filtered#

bool sl_ncp_evt_filter_is_filtered (uint32_t header)
Parameters
TypeDirectionArgument NameDescription
uint32_t[in]header

incoming Bluetooth stack event header

Checks if the given event is filtered or not.

Returns

  • Returns true if filtered, false otherwise.


Macro Definition Documentation#

SL_NCP_EVT_FILTER_ARRAY_LENGTH#

#define SL_NCP_EVT_FILTER_ARRAY_LENGTH
Value:
8

SL_NCP_EVT_FILTER_CMD_ADD_ID#

#define SL_NCP_EVT_FILTER_CMD_ADD_ID
Value:
0

SL_NCP_EVT_FILTER_CMD_REMOVE_ID#

#define SL_NCP_EVT_FILTER_CMD_REMOVE_ID
Value:
1

SL_NCP_EVT_FILTER_CMD_RESET_ID#

#define SL_NCP_EVT_FILTER_CMD_RESET_ID
Value:
2

SL_NCP_EVT_FILTER_CMD_ADD_LEN#

#define SL_NCP_EVT_FILTER_CMD_ADD_LEN
Value:
5

SL_NCP_EVT_FILTER_CMD_REMOVE_LEN#

#define SL_NCP_EVT_FILTER_CMD_REMOVE_LEN
Value:
5

SL_NCP_EVT_FILTER_CMD_RESET_LEN#

#define SL_NCP_EVT_FILTER_CMD_RESET_LEN
Value:
1